This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have a customer asking if CCS can be licensed with a dongle rather than a MAC address. THe customer wants to use CCS on different computers, but not simultaneously. Everything I have read indicates that dongles are not supported. I want to confirm this before getting back to the customer.
Regards,
John Wiemeyer
Hi John,
that I am aware of that is not supported. Some options might be
- the node locked license can be registered to 2 MAC addresses
- note that it is actual debug requiring a license. In other words editing and writing can be done without a license
- note that depending on the hardware, they may be able to use one of the two free license types (ie ccs is free to use with the xds100 for example)
- if it is an option for them and they have connectivity ... another option although not the easiest perhaps would be a singe seat floating license
Please let us know whether these help
Best Regards,
Lisa
John,
Maybe someone else had done it, but I personally don't know if this is possible. However, would be a possibility to use a Wi-Fi USB adapter and use its MAC address to license CCS? I recall that some even allowed disabling the radio but still kept the MAC address visible to the Operating system (if radio waves are a problem at the lab).
Hope this helps,
Rafael
Hi Rafael,
The USB WiFi adapter seems like a good idea. It would be great if we knew it worked.
Regards,
John
Hi Rafael
Do we have any documentation to support this for the customer?
Thank you
Elush Shirazpour
Have there been any reports of success using the MAC address from a USB connected device?
R. Harkins