This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have a customer asking if CCS can be licensed with a dongle rather than a MAC address. THe customer wants to use CCS on different computers, but not simultaneously. Everything I have read indicates that dongles are not supported. I want to confirm this before getting back to the customer.
Regards,
John Wiemeyer
Hi John,
that I am aware of that is not supported. Some options might be
- the node locked license can be registered to 2 MAC addresses
- note that it is actual debug requiring a license. In other words editing and writing can be done without a license
- note that depending on the hardware, they may be able to use one of the two free license types (ie ccs is free to use with the xds100 for example)
- if it is an option for them and they have connectivity ... another option although not the easiest perhaps would be a singe seat floating license
Please let us know whether these help
Best Regards,
Lisa
John,
Maybe someone else had done it, but I personally don't know if this is possible. However, would be a possibility to use a Wi-Fi USB adapter and use its MAC address to license CCS? I recall that some even allowed disabling the radio but still kept the MAC address visible to the Operating system (if radio waves are a problem at the lab).
Hope this helps,
Rafael
Hi Rafael
Do we have any documentation to support this for the customer?
Thank you
Elush Shirazpour