Part Number: PSPICE-FOR-TI
This FAQ covers various topics related to obtaining and using PSpice for TI.
Licensing
Does PSpice for TI need a license to run?
Will my PSpice for TI license expire?
Are there limitations to the number of licenses I can hold for the PSpice for TI tool?
What is the process to migrate my Pspice for TI license to a new computer?
I get license expiration warning in the middle of my session using PSpice for TI. What should I do?
I was able to use PSpice for TI for the past couple of months. Suddenly I restarted my application and I cannot use it anymore? Why?
How long can I be offline while running the PSpice for TI application?
Do I need to be connected to Internet when I launch PSpice for TI for the first time?
Installation
How do I get PSpice for TI?
How long will my download link be valid? How do I get a new download link?
What is an access key?
What happens if I lose my PSpice for TI Access Key?
Can I use the same Access Key to install PSpice for TI on multiple machines?
When I use the Access Key with PSpice for TI Installer, it gives me an error?
Does my Access Key have an expiration date? Do I have to renew it periodically?
My PSpice for TI software download failed in middle of downloading software? What do I do?
I cannot install PSpice for TI. The error message says "An Internal error occurred" with (-8) or (-12)
I cannot install PSpice for TI. The error message says "the required files cannot be read from the server".
Can I get the PSpice for TI package for installing offline?
I am getting User Max Hosts exceeded message while trying to register. What does that mean?
Do I need to be connected to internet while installing the PSpice for TI software?
I already have the full commercial version of Cadence SPB/PSpice/OrCAD/Allegro. Can I still run PSpice for TI?
Simulating Your Design
Why can't I plot more than three signals in PSpice for TI?
Share Your Design
How do I share PSpice for TI projects?
TI Model Library
How to get the latest TI models?
How can I add all the PSpice for TI model libraries to the commercial version of PSpice/SPB/Orcad?
Use 3-party Models
How do I import a 3rd-party model into PSpice for TI?
How do I use my own diode (BJT, MOSFET ...) model for the breakout part in PSpice for TI?
Can I define my own model in PSpice for TI?
When something goes wrong