Browse By Tags

  • INA132: change of gain

    Part Number: INA132
    Other Parts Discussed in Thread: INA827, INA331, INA145, INA122, INA126, INA321, , INA500, RES11A, INA597, OPA317

    Hi,
    is it possible (even not recommended) to change the gain?

    Regards, Holger

  • OPA317-Q1: Max offset voltage Question & schematic review

    Part Number: OPA317-Q1
    Other Parts Discussed in Thread: OPA317, TLV333, LM7705

    Hi,

    The customer reviews the OPA317 to measure the IGBT current.

    However, the offset voltage is high compared to the competitor, so the customer does not want to use OPA317…

  • OPA196: Spice Simulation Models

    Part Number: OPA196
    Other Parts Discussed in Thread: OPA4317, OPA317

    I can't get the Spice Models for OPA196 and OPA4317 from the website, Where I can get it?

  • DAC8564: Suit amp with DAC8564 For 4-20mA

    Part Number: DAC8564
    Other Parts Discussed in Thread: OPA333, OPA317, OPA391, OPA191, XTR111, XTR300

    HI SIR

    I want to design a 4-20mA Function which use the DAC8564,

    Did you have suggestion AMP for this?

    thanks

  • INA317: INA317 output oscillation

    Part Number: INA317
    Other Parts Discussed in Thread: OPA317

    Hello,

              For the moment, I am debugging the board with INA 317 . I found the INA317 output has some oscillation with 80KHz/80mVpp, see attached:

    Test condition is: short VO- and VO+ and connect…

  • OPA317IDBVR

    Hello Team, I am unable to access the PSpice model for the mentioned manufacture part number OPA317IDBVR (Zero-Drift Amplifier 1 Circuit Rail-to-Rail SOT-23-5), it would be appreciated if the model is available let me know the location or site from where…

  • OPA317: OPA317IDBVR

    Part Number: OPA317

    The PSpice for OPA317IDBVR is not available or if in case it is there I am unable to get access to that particular file... It is needed for simulation purpose, could you please provide me with the PSpice model...

  • OPA317-Q1: Voltage drop due to OPA317

    Part Number: OPA317-Q1
    Other Parts Discussed in Thread: OPA317, TINA-TI

    Hello TI,

    We are using a current source to test a current sense circuit. The given input DC current range is 1mA to 75mA.

    We are facing a voltage drop across R3 ranging from 3mV to…

  • RE: OPA317: Voltage inversion using Single supply Op amp Circuits

    Thank you Marek for the detailed analysis and Simulation results.

    Margin on both side voltage railing is OK for my application.  

    In first circuit, resistor was missed when I did some edit in the original circuit to post here.  Will  keep that resistor.

  • RE: OPA317: Voltage inversion using Single supply Op amp Circuits

    Anil,

    Your top circuit will not work - you need to add an input resistor to place the amplifier in an inverting configuration - see below.

    Keep in mind that since the linear output range of OPA317is defined within 100mV of either rail (see table below…

  • OPA317: Voltage inversion using Single supply Op amp Circuits

    Part Number: OPA317
    Other Parts Discussed in Thread: TINA-TI

    Hi,

    I am using OPA317 for

         *  Negative to positive voltage conversion (using 5V supply for opamp)

         * Positive to Negative voltage conversion (using -5V supply for opamp)

    Attached is the circuit…

  • RE: OPA2333A-EP: CA3420 Replacement

    Ambroise.

    The closest to CA3420 would be OPA196 with min +/-2.25V supplies or OPA170 with min +/-1.35V supplies.  But if you must operate on +/-1V supplies, you may consider OPA317 or OPA313.

  • RE: ADS114S08: Low input offset voltage opamp

    Hi Arumugam,

    I see that you have also been discussing the op amp circuit with Luis in the amplifier E2E.  Similar to what Luis has done I created a TINA simulation of the circuit you are using along with the 1k/100nF input filter and I don't see any oscillation…

  • RE: OPA2317: replace instead of LMC6082IMX

    Hi Arumugam,

    The OPA317 or LMC6082 should work in the RTD measurement application; however, I have questions about the amplifier used in the inverting configuration and the RTD connections.

    1)      The schematic does not clearly show a DC path connection of…

  • RE: OPA2317: replace instead of LMC6082IMX

    Hi Arumugam,

    Yes, the OPAx317 amplifiers offer very low offset and near zero offset drift without flicker noise due to the internal offset auto-calibration correction. Since your RTD signal of interest is very low frequency, and the ADS124S08 has relative…

  • RE: OPA820: Design Methodology for MFB Filters

    hey Joe, I did a little more work on this with your OPA820 gain of 1 design, The attached spreadsheet breaks the calculation into pieces and step by step works towards the result - I get 76 ohms now.

    I tried that in sim for the OPA820, and the output…

  • RE: OPA2317-Q1: Input range question

    Hi Marek,

    Yes, the input range is 0 to -200V, and I want t o covert to 0 to 4V. And the OPA317 is powered form a single supply(0,5V).

    And the simulation shows that the circuit can achieve this function, right?

    Thanks & Best Regards,

    Sherry

  • RE: OPA2317-Q1: Input range question

    Sherry,

    There are several ways to implement such function but we need to know what is the exact range of the input/output signall you need?  Is it 0 to -200V input that you want to convert to 0 to 4V output or something else?   Also, OPA317 may be powered…

  • RE: OPA317 Overdriven

    Meng

    We haven't heard back from you so we assume this answered your questions. If not, just post another reply below.

    Thanks
    Dennis
  • RE: OPA317 Overdriven

    Hi Meng,

    figure 20 shows the internal protection against high differential input voltages. But if the input signal exceeds the rails you need additional current limiting, as mentioned in sections 6.1 and 8.3.2 of datasheet. I see that you already have…

  • OPA317 Overdriven

    Other Parts Discussed in Thread: OPA317

    OPA317 is used in small signal amplification circuit. In the process of using OPA317, there will be Overdriven, IN + 5V.

    1. Can the structure of the following pictures be understood as self protection of IC? Is there…

  • RE: LMC6484: looking for single channel alternative part.

    LMC6448 is a general purpose quad and we have many much higher precision parts that you could use in your application. OPA317 is one of them but depending on the other considerations you should also check TLV333, OPA376, or our low voltage highest precision…
  • LMC6484: looking for single channel alternative part.

    Part Number: LMC6484
    Other Parts Discussed in Thread: LM35, ADS1100, LMC6061, OPA317, OPA388, TLV333, OPA376

    Hello,

    I'm using LMC6484 to convert a LM35 temperature signal (about 0 - 70° C) into a 0-5 V range which is then fed into an ADS1100.…

  • RE: OPA317: Differential circuit analysis

    Hi Keith,

    You hit the nail on the head - stability. If the differential filter capacitor is connected directly across the OPA317 inputs the circuit will become unstable. It comes about from the pole introduced into the feedback loop by the 1.02 Meg feedback…
  • RE: OPA317: Differential circuit analysis

    Hi Keith,

    it's difficult to say something useful without knowing the full schematic...

    When omitting the two 4R99 resistors you won't have any low pass filtering in this circuit, unless the unshown source on the left provides some source impedance…
1 2