Tool/software:
Is there a way to parse the TLV sequence from the MRR demo provided in the SDK. Currently, the board is being used in tandem with MRR demo to detect objects to implement a Driver Assistance warning system. Upon…
Tool/software:
Is there a way to parse the TLV sequence from the MRR demo provided in the SDK. Currently, the board is being used in tandem with MRR demo to detect objects to implement a Driver Assistance warning system. Upon…
Tool/software:
I have built the demo for the latest SDK, 4701. The demo seems only to handle out-of-the-box detections. We would like to implement tracking with the latest SDK for our use case. Would it be possible to run the HECR…
Tool/software:
Hi Ti,
Referring to MMWAVE_L_SDK_05_05_02_00, I performed the following tests on the sensorPosition parameter:
Test scenario:
Man riding a bicycle along the white line towards the radar
test 1 :
The normal…
Tool/software:
Hi Ti,
Referring to MMWAVE_L_SDK_05_05_02_00, I performed the following tests on the sensorPosition parameter:
Test scenario:
Man riding a bicycle along the white line towards the radar
test 1 :
The normal…
Tool/software:
Hi team,
I want to include clustering to the Demo Application and export Cluster information through UART. How can I do it ? Any suggestions would be appreciated.
Thank you…
Tool/software:
I am Pablo Crego from GMV, Aerospace and Defence. I am writing because we are interested in buying one radar from Texas Instruments. Specifically, we have chosen…
Tool/software:
Hello,
I'm writing you regarding a question about the FFT that is implemented on the function MmwDemo_computeVitalSignProcessing() of the vitalsign.c code (vital signs open source lab). My concern is about the…
Tool/software: Code Composer Studio 12.8.0
Hello Sir,
I installed SDK https://www.ti.com/tool/MMWAVE-SDK but in which I am not able to find source code of binary (e.g. 3D people counting…
Tool/software:
Hello, we are using the MMWCAS-DSP-EVM and Vision SDK for radar application development.
Currently our software is based on the example application "tda2xx_cascade_linux_radar", it includes the linux usecases…
Tool/software:
Hello,
I have a question regarding the implementation of the FFTs in the code of the vital signs lab. For what I'm seeing in the code, the dpc.c file implements functions like DoaProc_configParser to send data…
Part Number: AWRL6432AOPEVM
Tool/software:
I am developing a product using xWRL6432AOPEVM. There is an angle offset at the output position, so I need help in proceeding with receiving channel calibration.
The development environment analyzes the output…
Tool/software:
Hi,
I am using the "automated_parking_18xx" code to retrieve data from the AWR1843BOOST.
The code outputs the following structures:
Header Structure (MmwDemo_output_message_header): Description:…
Tool/software:
I am using iwr6843aopevm 3d people counting demo. I want to add a new task that uses generated point cloud. I searched google but got nothing. How can I do this?
Tool/software:
Is there any way to use hard coded cfg for iwr6843aopevm projects? Currently I am sending the cfg file over cli port.
Hi everyone,
For our project to detect humans, we used IWRL6432 radar sensor, and for the antenna design, we used 2D Antenna Variant, which promises us a very long distance to detect human (10 meters).
However, the range of the demo…
Hi,
We have DCA1000EVM and AWR1843BOOST devices. I want to program the AWR but when I try to set up DCA1000 at "Connect, Reset and Configure" step, I am getting the…
Hi,
I'm encountering an issue with the AWR1843BOOST Radar.
When I use the 18xx_mrr code and flash it onto the chip, it begins transmitting data automatically, but the…
Hello,
I am trying to find out what the minimum frequency slope (i.e., maximum chirp time) is that the AWR2243 can support for a chirp. The ICD states that PF_FREQ_ SLOPE_CONST has 1 LSB equivalent to 48.279 kHz/us, so I assume this…
Dear Team,
I am writing to you regarding an issue I am facing with the IWR6843EVM board and the radar toolbox. I have been using CCS version 11.1 on Windows 10 without any problem, but when I upgraded to Windows 11, I encountered an error while…
In the radar toolbox download options, there are only the release notes selectable for download. How can I download the radar toolbox from the web?
Can you share a direct download link?
Thanks!
Good afternoon, all. I am part of a design group looking into the feasibility of low-cost radar for space applications in Low-Earth Orbit. While there has been some work in placing similar chips into orbit as a means of detecting…
Hi All
For AWR2944 OF our radar board, we use DCA1000 to transmit raw ADC data, the Rx1 and Rx3 have bit error, but Rx2 and Rx4 do not have bit error.
I have three questions:
1. Why only RX1 AND 3 have bit error, Do Rx1 and 3…