Texas Instruments (TI) Processors support forum is an extensive online knowledge base where millions of technical questions and solutions are available 24/7. You can search processors content or ask technical support questions on Sitara™ processors, digital signal processors (DSP) and automotive processors. Find the right solution for your circuit design challenges by using our TI E2E™ support forums that are supported by thousands of contributing TI experts.
Part Number: TDA4VH-Q1
The high speed interfaces on the TDA4x share the SerDes lanes. The lanes can be muxed for different interfaces, but how can I configure them within Linux?
Part Number: AM2754-Q1 Other Parts Discussed in Thread: SYSCONFIG
In the MCU+ SDK 11.02 offering, the examples of OSPI and Flash are configured to work at the highest protocol that is 8D-8D-8D.
In case for profiling purpose, an engineer wants to run…
Part Number: TDA4VH-Q1
Hi,
After reset of C7x, i am trying to load newer C7x binary, but the second load takes a lot of time.
Could you please help me to solve this issue.
Part Number: AM6442 Other Parts Discussed in Thread: UNIFLASH
I am trying to flash an image for AM64/AM243 device by loading SBL JTAG UNIFLASH from CCS version 20. *.* , after following the steps mentioned in the MCU+SDK documentation: https://software…
Part Number: AM62A7-Q1
Hi,
I am trying to do CPU reset for C7x core on AM62Ax device and facing a page fault error.
Below is the error message.
"(Error -1351 - (0:0:0)) Register or Memory request has timed out. The CPU is executing a High Priority…
Part Number: AM62D-Q1
When implementing audio input/output systems using MCASP (Multichannel Audio Serial Port), there is inherent latency in the audio pipeline(SW) due to buffer priming and the DMA queuing mechanism. This FAQ explains the fundamental…
Part Number: AM62D-Q1
By default, The AWE SDK uses the AWE Designer to load any signal processing chain. However, once the signal chain is finalised, how to load the signal chain on startup without the use of AWE Designer?
Other Parts Discussed in Thread: AM2431 Hello Randy
AM2431: MCU design: PCIe differential impedance value
Since the 2 queries are 2 different topics, i will split the thread.
For PCIe interface traces impedance control, I get different information…
Part Number: AM620-Q1
There are more than 30 ECC aggregators in each of AM62x, AM62Ax, AM62Px and AM62Dx devices. How do we find the ESM events corresponding to each of the ECC Aggregators?