Texas Instruments (TI) Processors support forum is an extensive online knowledge base where millions of technical questions and solutions are available 24/7. You can search processors content or ask technical support questions on Sitara™ processors, digital signal processors (DSP) and automotive processors. Find the right solution for your circuit design challenges by using our TI E2E™ support forums that are supported by thousands of contributing TI experts.
Part Number: AM625 Other Parts Discussed in Thread: AM623 , AM6442 , AM2434 , TDA4VM , AM2431 , AM6548 , AM62P5-Q1 , AM62A3-Q1 , TDA4AL-Q1 , TDA4VM-Q1 , TDA4AH-Q1 , MCU-PLUS-SDK-AM243X , SK-AM62A-LP , AM62A7 , TDA4VH-Q1
Tool/software:
Hi TI Experts,
I have the below…
Part Number: PROCESSOR-SDK-AM64X Other Parts Discussed in Thread: TMDS243EVM
Tool/software:
Hi TI Expert,
How can we use AM64x/ AM243x - MCU+SDK to enable PCIE based Precision Time Measurement (PTM) ?
Regards
Part Number: TDA4VM Tool/software: The IgH EtherCAT stack is an open source EtherCAT stack.
It comes with a generic driver that uses generic Linux ethernet API calls, but is not optimized for specific platforms, and therefore comes with latency.
How…
Part Number: TDA4VM Other Parts Discussed in Thread: J721EXCPXEVM , Tool/software: How to run ETHFW without connecting GESI card to J721EXCPXEVM for TDA4VM/J721E? When using TI SDK ETHFW was failed to load.
Part Number: TLV62585
Tool/software:
Hi Experts,
I am reviewing a customer schematic.
Customer is using TLV62585DRLR
the input is 4.2V and could be switched to 3V.
The output is 3.3V.
Do you have any concern with the TLV62585DRLR providing output or 3…
Part Number: AM3358
Tool/software:
AM335x GPMC-NAND boot issue was observed with AM335x Linux SDK 9.1 [1]. The FAQ lists the u-boot and kernel patches to support flashing and booting u-boot/kernel/root_fs with AM335x Linux SDK 9.1 from GPMC-NAND on AM335x…
Part Number: AM6442
Tool/software:
In AM64X/AM243/AM62X there are many Resets.
So, what is the difference between each type of Reset?
What is the boot flow for each Reset ?
What are the Registers/Peripherals affected for each Reset ?
How different Resets…
Part Number: J784S4XEVM Tool/software: UFS is present on the J784S4EVM. How can one use it instead of eMMC to host rootfs and use that to boot to Linux command prompt.
Part Number: AM6442 Other Parts Discussed in Thread: TMDS64EVM
Tool/software:
AM64x boot ROM supports booting from parallel GPMC NAND. From "4.4.10 GPMC NAND Boot" in AM64x TRM "AM64x ROM only supports boot from ONFI 1.0 compatible 8 bit parallel…
Other Parts Discussed in Thread: SYSCONFIG The DDR Controller and PHY in Sitara processors is a flexible interface which can be used with LPDDR4 or DDR4. There are many settings available to fine-tune the signal timing on this interface. These settings…