• Part III: Get CerTIfied, not certi-FRIED! Electromagnetic compatibility testing explained

    Other Parts Discussed in Post: STRIKE

    Welcome to part three of this blog series discussing electromagnetic compatibility (EMC) testing. In parts one and two we discussed the background of certification testing and the specifications for ESD and radiated EMI immunity tests. This time, we’ll continue with the details of electrical fast transient (EFT) and surge testing.

    IEC 61000-4-4: EFT (Electrical Fast Transients…

  • “X” marks the spot as “2” “Y” supply splitters can start-up quickly

    Other Parts Discussed in Post: TINA-TI

    **Click on images to enlarge.

    Just about every single-supply application uses a “supply splitter” to create a mid-point reference that is ½*Vcc. Texas Instruments makes an IC dedicated to that purpose called the TLE2426.  Now, before you quit reading because you think I am trying to sell you something, hear me out. The below information is valid for the TLE2426

  • Perils of using op amps outside the specified conditions

    I regularly respond to questions on the Precision Amplifiers forum attempting to clarify misunderstanding of differences between the specified and operating conditions used in our product datasheet (PDS) for defining various op amp parameters. These differences have great technical implications since PDS limits apply only to specified ranges. Therefore, it is paramount for designers not to use operating conditions as…

  • The case for isolated delta-sigma modulators: Is my system fast enough for short-circuit detection?

    Other Parts Discussed in Post: TIPD165

    Galvanic isolation is a key requirement in many industrial applications. Isolation provides technical advantages such as breaking noisy ground loops, and it also protects the end user and sensitive equipment from potentially dangerous high voltage and transients.

    An isolated current-monitoring acquisition system can be constructed as shown in Figure 1: the input current is transformed…

  • Why correct voltage matters for op-amp PowerPads™

    The PowerPad™ is a great package feature that allows operational amplifiers and other linear circuits to deliver otherwise unattainable output power from a device packaged in a small outline (SO) package. The PowerPad™ provides a highly conductive thermal path from the back of the integrated circuit die to an external heat sink, or to a copper PC board plane acting like one. The product datasheet is specific about the…

  • 2-Wire 4-20 mA Sensor Transmitters: Background and Compliance Voltage (Part 1)

    Part 1:

    2-wire 4-20 mA sensor transmitters are very common in industrial control and automation. They are popular because they allow a remote process to be monitored with only two analog signal wires. The two wires carry both the power for the sensor/monitoring circuitry and the analog output signal. Common applications for 2-wire sensor transmitters are pressure sensors, gas sensors, chemical sensors, level sensors,…

  • SAR ADC response times: A marketing analogy

    This is the second post in our SAR ADC series.

    Part 2: A marketing analogy

    When a response time of 1 µs is required from the SAR ADC (tRESP-ADC = 1 µs), many engineers would search for a SAR ADC with throughput of 1 Msps (tTHROUGHPUT = 1 us). In reality, the two parameters are actually different. To demonstrate the difference, let’s look at the following analogy:

    You are the marketing manager of a major…

  • The importance of proper termination

    I recently performed some tests in the lab and noticed a strange ringing on the output signal. After troubleshooting the problem, I managed to trace the ringing back to the input signal. Figure 1 shows the input signal of my circuit with the ringing boxed in red. I needed to find the cause of the ringing since a clean step response was expected. It turns out that my lab equipment was not properly terminated. This blog…

  • SPICE-ing up Precision DACs

    Other Parts Discussed in Post: TINA-TI, DAC8411

    This post was co-written by Kunal Gandhi and Rahul Prakash.

    Engineers may agree that one of the most anxious and stressful moments they face is when his or her design is back from fabrication and ready to be tested. While it is thrilling to see our concept or design work for the first time in the lab, sometimes we have to accept catastrophic failures, too.

    In this blog post…

  • Understanding total harmonic distortion and noise curves

    Other Parts Discussed in Post: OPA316

    Noise and distortion are two common enemies for engineers designing precision analog systems. But when looking at total harmonic distortion and noise (THD+N) figures in an op amp datasheet, it may not be immediately clear which enemy you’re battling: noise or distortion?

    “Noise” describes the random electrical signals produced by the amplifier. “Distortion” refers to unwanted…

  • SAR ADC Response Times: Respond quickly, control quickly

    This technical article was updated on July 23, 2020.

    Part 1:

    The objective of many typical control system applications is to effect a control action based on the status of input control variables. Some of these include position, speed, angle, level, temperature and pressure.

    And for each of these control variables, you may need to optimize the design for ‘precise’ measurements, ‘precise’ control actions, and/or a fast…

  • ADC Accuracy Part 2: Total unadjusted error explained

    This technical article was updated on July 23, 2020.

    In the first ADC Accuracy post, we established the differences between the resolution and accuracy for an analog-to-digital converter (ADC). Now we can dig into the factors that contribute toward total accuracy of the ADC, often referred to as Total Unadjusted Error (TUE).

    Ever wondered what “Total” stands for in the TUE specification of ADC? Is it as simple as adding…

  • INAs: Offset voltage vs. gain

    Other Parts Discussed in Post: INA333

    Have you ever wondered why a traditional 3-op amp instrumentation amplifier’s offset voltage changes with gain? Figure 1 is an excerpt from the INA333 datasheet that shows an example of the dependence of the offset voltage on device gain. Today, let's walk through how the equation is determined.

    Figure 1: INA333 offset voltage specification

    Traditional 3-op amp instrumentation…

  • ADC Accuracy Part 1: Is accuracy different from resolution?

    This technical article was updated on July 23, 2020.

    In talking to system designers using analog-to-digital converters (ADCs), one of the most common questions that I hear is:

    “Is your 16-bit ADC also 16-bit accurate?”

    The answer to this question lies in the fundamental understanding of the difference between the concept of resolution and accuracy. Despite being two completely different concepts, these two…

  • Performance comparison between SAR ADC input types – Part 2

    This technical article was updated on July 23, 2020.

    Today, we continue our series on successive approximation register (SAR) analog-to-digital converters (ADCs) input types. Previously, I reviewed input considerations and pnoise performance comparisons between SAR ADCs. In this post, we will look at the source for Total Harmonic Distortion (THD) in a SAR ADC and how it differs between various input types.

    THD Impact

  • To simulate or not to simulate, that is the question

    To simulate, or not to simulate, that is the question-
    Whether it is wiser in the Engineer’s mind to suffer
    The ridicules of colleagues and wrath of management,
    Or to hasten accuracy and time to market,
    And by using SPICE, end all doubt?

    The use, or overuse, of SPICE simulation is an age old controversy. Many engineers rely heavily on simulation and do relatively little hand calculation. Other engineers have distain…

  • Industrial DACs: How to design universal analog outputs

    In the last two posts in this series I talked about how to build 3-wire analog outputs and how to protect them from transient overstress. This post will finish off the discussion of 3-wire analog outputs with some solutions to one more application-specific problem.

    A growing trend in the industrial application space is for analog output modules to provide both voltage and current outputs on a single terminal block. This…

  • Part 3 - A voltage reference duel of duals

    In this three-part series, I discussed the solutions for generating two well-matched, low-drift voltage references. We started with three topologies in Part 1, we compared and contrasted the differences in terms of performance in Part 2. Now, let’s take a look at other design considerations of these solutions: space consumption and cost.

    Space Consumption and Cost

    Apart from system performance, PCB real estate…

  • Performance comparison between SAR ADC input types – Part 1

    This technical article was updated on July 23, 2020.

    My previous blog Input considerations for SAR ADC's, introduced various input types for Successive Approximation Register (SAR) analog-to-digital converters (ADCs): single-ended, pseudo-differential, fully differential input and true differential input.

    Some of the key specifications considered when selecting a SAR ADC include resolution, channel count, sampling…

  • Part 2 - A voltage reference duel of duals

    In my previous post, we talked about three topologies for generating two high-accuracy voltage reference outputs. Today, we’ll compare the performance of these solutions from three perspectives: total error, drift tracking and matching between outputs.

    Total error  

    Equation (1) converts specifications given as a percentage (%) to parts per million (ppm).

      

    (Equation 1)

    The Total Error performance metric of each…

  • Part 1- A voltage reference duel of duals

    Developing a low-drift system can be very difficult, especially with a bipolar input signal. Applications such as bidirectional current sensing shown in Figure 1, require the use of two well-matched, low-drift reference voltages. The first voltage, VREF, defines the full-scale range of the ADC. A bias voltage, VBIAS, is necessary in order to level shift the bipolar signal. It is desirable to have VBIAS = VREF/2 so that…

  • Part II – Get CerTIfied, not certi-FRIED! Electromagnetic compatibility testing explained.

    Welcome to part two of this blog series discussing electromagnetic compatibility (EMC) testing. In part one, we discussed the need for certification testing, who performs the tests, and what constitutes a pass or fail condition. This time, we’re going to dive right into the technical specifications of some of the most common tests.


    IEC 61000-4-2: ESD (Electrostatic discharge)

    ESD (Electrostatic discharge) is one…

  • How to combine error terms

    Other Parts Discussed in Post: INA826

    Calculating the total error of a system can be tricky, especially when the specifications units vary widely. When calculating the total error, all specifications must be converted into a common unit before combining. This blog will show you how to convert between units of volt, percentage and parts per million (ppm) to ensure proper calculation of total system error.

    Most errors…

  • Industrial DACs: Protecting 3-wire analog outputs

    In my last post, I talked about how integration has simplified 3-wire analog output design. In this post, I’ll show you one way to protect these designs against dangerous industrial transients that can cause electrical overstress.

      
    Let’s start with a few examples of what we’re trying to protect the system against:
    • Some systems are installed or calibrated in environments that are not ESD-safe, which…
  • Top questions on op amp power dissipation – Part 2

    Other Parts Discussed in Post: OPA316

    Part 2 of 2:

    Two commonly asked questions when designing an operational amplifier into a new application are:

    1.     What is its “typical” power dissipation? Covered in my first post.

    2.     What is its “maximum” power dissipation?

    The op amp’s maximum power should be evaluated in the intended circuit. Let’s assume the first case where the amplifier is being operated…