Part Number: CD4050B Other Parts Discussed in Thread: UCC27527 , CD40106B
Hi
I had asked a Q reg UCC27527 Input characteristics .
This is a related Q
We want to create a Short Pulse Suppression Ckt for our 0-15 V Signals from the DSP
Typical value would…
Part Number: CD4050B Other Parts Discussed in Thread: CD4504B , Hi team.
I'd like to know About the relationship between input and output voltage.
We will use the input voltage of 10Vpeak when Vcc is 15V.
According to datasheet,
Vin seems to depend…
Part Number: CD4050B Dear Specialists,
My customer is considering to adopt CD4050BPWR and has a question.
I would be grateful if you could advise.
---
We'd like to CD4050PWR, but we have a concern about mount condition.
Because we will need to process…
Part Number: CD4050B Dear Specialists,
My customer is considering CD4050 and has questions about device function test.
I would be grateful if you could advise.
---
We'd like to conduct a kind of stress test(thermal, shock and etc) and confirm deterioration…
Part Number: CD4050B Other Parts Discussed in Thread: CD40106B Dear all,
I am trying to properly understand the datasheet of the CD4050B Hex Buffer IC. It is supplied with 15V and decoupled with a 100nF (not shown in the schematic). Input D (pin 9) is…
Part Number: CD4050B Hello, We have a customer who pointed out a possible datasheet discrepancy. The device is the CD4050BE. Reviewing the present day datasheet, back to September, 2016, lists the Ioh output high current at measure voltage is listed at…
Part Number: CD4050B Other Parts Discussed in Thread: CD4504B Hi, I need to convert 15V logic to 5V logic for my application. I saw two ICs CD4050B and CD4504B that seemingly can do this, looking at the datasheets. Is it correct that both can do the logic…
Other Parts Discussed in Thread: AM26C31 , AM26C32 , CD4050B , SN74HCS125 , THVD2450V Hello Community,
We're working on a project that involves transmitting a 32kHz clock signal from a MEMS TXO (SIT1552AC-JE-DCC-32.768E) to a remote MEMS Accelerometer via…
Today I tried to use the CD4050B. This is what I got.
Channel 1 is input (0 to 5 V), channel 2 is output (-5 to +5 V)
CD4050B seems to convert the voltage level as I desire. The threshold is not very critical for me. However, the fall time is too slow…
Other Parts Discussed in Thread: CD4050B , LM393 I am designing a board using a 5V microcontroller that must send control signals to some CD4000 family logic. I have designed in four CD4050B hex logic level converters to convert the 0~5V signals to 0~12V…