Part Number: PGA309 Hi team,
A customer at the E2EChina Forum also needs this Multi-Cal PGA309 Software Source Code, but the download link in the Original question is no longer valid, where can he download it?
https://e2e.ti.com/support/amplifiers-group…
Part Number: BQ25750 Other Parts Discussed in Thread: TPS2121 , BQ25756 , BQ25756E Hi all,
I need to build a system than can be powered by 4 smart batteries or from a DC power supply if the batteries are not present.
When both the DC supply and the batteries…
Hi Arijeet,
Please try with this configuration: LMK5B33216_XO=48MHz_REF=2kHz_OUTs=13.824MHz, ZDM.tcs
ZDM feedback output to DPLL2 is OUT0. All outputs are set to 13.824 MHz and sourced from APLL2. Both IN0 and IN1 are configured for a 2 kHz frequency. …
Part Number: PGA305 Other Parts Discussed in Thread: PGA309 Hello,
Is there a multi-cal software available to configure multiple PGA305? Can the multi-cal software for PGA309 be modified to support PGA305?
Thanks in advance,
Edwin
Part Number: TDA4VM HI TI
Running Cam for a long time may cause the system to restart. Please help analyze the cause.
1641.log.txt log has been uploaded
Part Number: MULTI-CAL-SYSTEM To whom it may concern,
I am having a similar communication error with the HP34401-A. The display shows the same error on the screen and is beeping when queried but no valid data is being displayed on the software GUI. I…
Part Number: PGA308 Other Parts Discussed in Thread: MULTI-CAL-SYSTEM Hello,
There is a problem with the multi-cal-system of PGA308 in use. Please check whether you can repair it or guide my customer to do some tests to find the problem. thank you!
A…
Part Number: MULTI-CAL-SYSTEM Other Parts Discussed in Thread: PGA309 I am in need of the source code for the Multi-Cal-PGA309 program. I have REV A as downloaded from the website. I will need the REV A source code.
Hoping someone can help quickly!
Part Number: MULTI-CAL-SYSTEM Other Parts Discussed in Thread: PGA309 Does the temperature calibration for the PGA309, using the multi-cal-system, have to be in order? For example, if I want to compensate the sensor at -40°F, 23°F, and 85°F, do i need…
Part Number: TDA4VM Hi TI expert:
We use SDK 0703, QNX.
We can keep multi-cam graph running when I unplug the camera for one channel, and channel can capture error frame which is registerd by tivxCaptureRegisterErrorFrame.
I have refer to the follow e2e…