Part Number: EK-TM4C129EXL Other Parts Discussed in Thread: EK-TM4C1294XL SW-TM4C-BOOTLDR-UG-2.2.0.295 states:
When the user application is running, it can still invoke the ROM boot loader to force an update of the firmware through a chosen interface…
Hi, Mani,
Have you ever read https://www.ti.com/lit/an/slaa721e/slaa721e.pdf?
It had been answered very clearly that you can make your own customized boot loader for the sw upgrade. You could bypass the standard BSL and use your own application as a BSL…
Part Number: TMS320F28377D Other Parts Discussed in Thread: UNIFLASH , C2000WARE , CONTROLSUITE Hello,
We are facing the same issue as the thread below, where the Flash cannot be programmed (see full provided log).
https://e2e.ti.com/support/microcontrollers…
Master-FAQ List – C6678 and C6678-EVM
Introduction :
This Master-FAQ document will help to explore the functions and features of C6678 Processor device using the C6678-Evaluation Module(EVM) with SDK. Going through these FAQ-list will help the customer…
Hi Derek,
thanks for my conclusion confirmation. I attached the screen of my computer. I downgraded USB2ANY firmware to the required 2.7.0 version and it seems, that the device control will be OK. Tomorrow I will start the device measurement. Thank to…
Hello,
Does the issue happen only after running from flash with secondary boot loader? Is it working properly if using CCS?
If you connect a JTAG emulator, do you see where the SW hangs at? Re-program pinmux may cause glitch, and you may have to do a…
Hello Ramesh,
There is CAN boot loader capability as part of our Flash boot loader. You can use the Flash boot loader with the boot_serial project, and just change the bl_config.h file to use CAN over UART (a number of lines have to be commented/uncommented…
Other Parts Discussed in Thread: TPS65185 , USB2GPIO-LOADER-SW , USB2ANY , TPS65185EVM , IPG-UI Hi All,
I'm trying to get my TPS65185 EVM kit working, which includes a USB-to-GPIO adapter (also known as "USB Interface Driver" and "HPA172")…
Hello Yao,
I am attaching a Flash Boot loader project for the EK-TM4C123GXL LaunchPad here: 2402.boot_serial.zip
And here is a demonstration program to go with it that includes instructions on how to use: boot_demo1.zip
You can find further details in the…
Voici mon ami,
TivaWARE\docs\ SW-TM4C-BOOTLDR-UG-2.1.4.178
It may be wise to mention that boot-loaders demand:
great attention to (even) fine detail
some indirection
solid testing to confirm that your implementation has succeeded
My tech group believes…