This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [H] High-Speed Amplifier Circuit Design Considerations



Frequently Asked Questions: Amplifiers >> High Speed Amplifiers >> Circuit Design Considerations
Circuit Design Considerations Transimpedance Amplifier Circuits Fully Differential Amplifier Circuits ADC Driver Circuits Other Op Amp Circuits
Stability Input/Output Limitations PCB Layout Guidelines Simulation & Modeling Power, Thermal, Quality, & Manufacturing

  

    


Circuit Design Considerations


Related Content:

3 common questions when designing with high-speed amplifiers

What you need to know about input bias current – and why

How to determine power gain and voltage gain in RF systems

How to determine if a CFA or a VFA is better for your design

High-gain, high-bandwidth… how can I get it all?

The decoupling capacitor…is it really necessary?

Achieving high-DC precision and wide large signal bandwidth with Hi-Z buffers

When to use an amplifier with rail-to-rail inputs – and what to watch out for

Correcting DC errors in high-speed amplifier circuits

Voltage-reference impact on total harmonic distortion

Dual Bipolar Power-Supply Considerations for Amplifiers

What are the advantages of using JFET-input amplifiers in high-speed applications?

Large-Signal Specifications for High-Voltage Line Drivers

Considerations for High-Gain Multistage Designs

Easily improve the performance of analog circuits with decompensated amplifiers

How to reduce distortion in high-voltage, high-frequency signal generation for AWGs

Preventing output polarity inversion in high-speed amplifiers

 

Top E2E FAQs and Posts:

OPA810: How is the input protection designed?

SLVA662 – July 2014 Demystifying Type II and Type III Compensators Using OpAmp and OTA for DC/DC Converters

THS3491: Impedance matching to drive a 50 ohm transmission line

THS4551: Does the simulation file provided from the datasheet on the THS4551 have an error?