Other Parts Discussed in Thread: TLV3601, LMH34400, OPA856
Tool/software:
Issues for TIA and Comparaot with LMH34400 and TLV3601.pptx
This is Youngjoon Cho, trying to develop a TIA and comparator circuit using the LMH34400 and TLV3601.
Our objective is to find a single peak in a highly reflected signal.
The TIA I built using the LMH34400 works fine, but when I connect the comparator I built using the TLV3601, there is an issue.
I have attached a document that summarizes the issue.
Belows are specified summary
- Designing the TIA(LMH34400) and comparator(TVL3601) for measuring high reflective target
- We want to measure only single peak signal at the comparator
- TIA amplifies pulse signal well when it operates without connecting comparator
- However, there are DC offset, ringings and oscillation when comparator is cascaded, especially when the measured is signals are saturated (having long pulse width).