Part Number: INA849
Tool/software:
hi
i need support for the above part
the requirement is we need to measure transient current of 10A/us
Is it possible to measure this transient current with this INA?
Load transient testing with high slew rates
as per the above link it is stated difficult to measure transient current if it is onboard slammer while it is difficult but not impossible right?
if so need support in reference design with TI part
we use high side sensing resistor 0.2mohms. the sense resistor is chosen keeping in mind to measure 1A - 20A static current with 2-3% accuracy at lower end and 1% accuracy at higher end