This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all, I am using MPY634 as divider circuit. I would like to create a simple offset adjust circuit permanently in the circuit board, adjust the offset at pin Y1 and X2 is ground with the pot and leave the pot undisturbed. I want to ask what values of resistance shall I use. How to make a test circuit for this and what should be the DC input for this. After balancing I would then connect input from the preamplifier circuit. Please help.
Ronnie,
See:
http://e2e.ti.com/support/amplifiers/etc_amplifiers__other_linear/f/18/p/333160/1161732.aspx#1161732
Regards, Thomas
PA - Linear Applications Engineering