• TLV320DAC3203: DSP to Headphone output

    Part Number: TLV320DAC3203

    Tool/software:

    Hello everyone,

    I'm trying to implement the following application.
    DSP --> Audio Interface --> DAC --> Headphone

    However, I encountered a strange problem.
    When I powered on for the first time and initialized…

  • TLV320AIC32X4SW-LINUX: Writing page 46 register in linux driver

    Part Number: TLV320AIC32X4SW-LINUX
    Other Parts Discussed in Thread: TLV320DAC3203

    Tool/software:

    Hi,

    I intend to write a value into the register of page 46 inside the Linux driver (tlv320aic32x4.c) itself.

    I have tried to write it by having a new macro…

  • TLV320DAC3203: Line-In (MIC) to I2S

    Part Number: TLV320DAC3203

    Tool/software:

    Hi,

    we need an audio codec to convert analog audio data comming from/to a Smartphone headset jack to digital (I2S) data.

    Therefore we have planed to use the TLV320DAC3203.

    The speaker output of the Smartphone…

  • TLV320DAC3203: TLV320DAC3203 LDOIN range with internal A-LDO enabled

    Part Number: TLV320DAC3203

    Tool/software:

    Hi Ti,

    As per we are using TLV320DAC3203 with internally A-LDO enabled to have 1.8V at AVDD without any external regulator on this pin. Our LDOIN and IOVDD is at 3.1V and we have DVDD via separate 1.8V regulator…

  • TLV320DAC3203: IOVDD and DVDD voltages

    Part Number: TLV320DAC3203

    Tool/software:

    Hi TI support,

    We are using going to add TLV320DAC3203 as a Audio DAC with its going to the headphone. Our MCU is at 3.1V so all the IOs are at same voltage. As per TLV320DAC3203 datasheet there are LDOIN, Avdd…

  • TLV320DAC3203: TLV320DAC3203 direct interfacing with Headphone

    Part Number: TLV320DAC3203
    Other Parts Discussed in Thread: TAD5212

    Tool/software:

    Hi Ti Support, 

    We are going to integrate TLV320DAC3203IRGER with ESP32-S3 via I2S as a single chip without its output connected directly to the ear/headphone via Audio…

  • TLV320DAC3203: Loopback control register setting

    Part Number: TLV320DAC3203
    Other Parts Discussed in Thread: MSP430FR2633

    Tool/software:

    Hi dear people,

    I encounter a discrepancy between the recommended setting for Page 0 / Register 29: Audio Interface Setting Register 3 - 0x00 / 0x1D and that what…

  • TLV320DAC3203: need to understand Page 1 / Register 2: LDO Control Register

    Part Number: TLV320DAC3203

    Tool/software:

    Hi Ivan,

    I am sorry, I still have difficultys to get my board working propperly.

    Some things are still not clear for me. I have a working code on the EVAL board and as far as I can see, this is also working on…

  • TLV320DAC3203EVM-K: Is it possible to use the USB-MODEVM Interface board alone, to test an own prototype?

    Part Number: TLV320DAC3203EVM-K
    Other Parts Discussed in Thread: TLV320DAC3203

    Tool/software:

    Dear people,

    I am aware, the TLV320DAC3203EVM-K can be used with external signals like one can read on the user's guide:
    2.4 Digital Signal Connections
    The…

  • TLV320DAC3203: How to resume from the over current protection

    Part Number: TLV320DAC3203

    Tool/software:

    Hi,

    Is my understanding correct that the over current protection in headphone outputs is non-latching error and TLV320DAC3203 can automatically resume the normal operation if the HPL or HPR short to GND is removed…

  • [FAQ] Low Power Audio DAC FAQs

  • TLV320DAC3203: Beep Generator

    Part Number: TLV320DAC3203

    Hi,

    During sleep mode, our clock (MCLK ) will stop providing DAC3203 .. 

    But during this condition , we wish to produce the beep by DAC3203 from its beep generator .

     

    In order for the beep generator to be able to produce the 

  • TLV320DAC3203: Audio Interface Inquiry

    Part Number: TLV320DAC3203

    Hi,

    I have an inquiry on TLV320DAC3203.

    Beside I2S format, do DSP, RJF and LJF support master / slave mode? 

    Rgds
    Kelvin

  • TLV320DAC3203: power supply turned off sequence

    Part Number: TLV320DAC3203

    Hello Experts,

    Would you tell a turned off sequence of power supply, please? There are some  turned on sequence of power supply on E2E, but I don't find turned off sequence. Is there any recommended sequence?

    Best Regards,

  • TLV320DAC3203: Logic levels

    Part Number: TLV320DAC3203

    I am using DVDD = 1.8V and IOVDD, LDOIN = 3.3V.  Am I correct in assuming the maximum logic levels on Reset, MCLK, SCL, and SDA = 3.6V with this setup?

  • TLV320DAC3203: Need to know about the internal protection of the HP outputs

    Part Number: TLV320DAC3203
    Other Parts Discussed in Thread: PGA2500

    Hi dear people,

    I am considering to power my design via a Phantom Power Supply.

    From the 48V from the supply I get my System-Vcc using DC/DC and LDO converters. My calculations show,…

  • TLV320ADC6120: TLV320ADC6120 clock issue using internal LDO

    Part Number: TLV320ADC6120
    Other Parts Discussed in Thread: TLV320ADC3120, TLV320DAC3203

    Hi, I am having a clock issue with TLV320ADC6120

    I am using internal LDO.

    here is my setup code. I am trying to configure the ADC as MASTER with 12.288mhz mclk as…

  • TLV320DAC3203: About supply voltages

    Part Number: TLV320DAC3203
    Other Parts Discussed in Thread: MSP430FR2633, , TPS62840

    Hi dear people,

    I want to check if I have understand this thread correctly (https://e2e.ti.com/support/audio-group/audio/f/audio-forum/752176/tlv320dac3203-supply-voltage…

  • TLV320DAC3203EVM-K: PLL powered on while not needed?

    Part Number: TLV320DAC3203EVM-K
    Other Parts Discussed in Thread: TLV320DAC3203

    Hi Ivan,

    going on with the settings of the TLV320DAC3203, I am now testing with a higher MCLK.


    I read in the Reference Guide (slau434a), by the settings for Fast Startup:
    "The…

  • TLV320DAC3203: SW driver and Volume control

    Part Number: TLV320DAC3203

    Hi TI team

    When checking for the Linux driver of TLV320DAC3203, I found that can use TLV320AIC32x4 driver, since it is compatible with.
    For more details, I'd like to check how exactly it is compatible, and what need to do in SW…

  • TLV320DAC3203EVM-K: about shut-down of the TLV320DAC3203

    Part Number: TLV320DAC3203EVM-K
    Other Parts Discussed in Thread: TLV320DAC3203

    Hi Ivan,

    I am back here with the question about shut-down of the TLV320DAC3203.

    It is said in SLAU434A:

    The DAC Modulator is clocked by DAC_MOD_CLK. For proper power-up of the…

  • TLV320DAC3203EVM-K: Register settings for MICBIAS

    Part Number: TLV320DAC3203EVM-K
    Other Parts Discussed in Thread: TLV320DAC3203

    Hi dear people,

    continuing with my project using the TLV320DAC3203, I have some questions related to MICBIAS settings:

    On the TLV320DAC3203 Applications Reference Guide I can…

  • TLV320DAC3203EVM-K: Fs 48KHz setting

    Part Number: TLV320DAC3203EVM-K
    Other Parts Discussed in Thread: TLV320DAC3203

    Hello,

    Our customer is running TLV320DAC3203EVM-K.

    It works fine with Fs 44.1KHz USB audio source, but if change FW setting for Fs 48KHz as following the procedure on GUI then…

  • TLV320DAC3203: Dynamic volume control on the fly with digital mics

    Part Number: TLV320DAC3203

    Hy dear people,

    I have again a silly question to which I cannot find an Answer.

    How  can I dynamically control the output volume on a TLV320DAC3203 (HPL HPR) with digital mics as input?

    The datasheet says:
    "The level of the…

  • TLV320DAC3203:TLV320DAC3203 can use STM32F103RBT6?

    Part Number: TLV320DAC3203

    Hello, I want to use Sound source files such as mp3 or wmv in memory to output.

    I use MCU STM32F103RBT6.

    1. Is it possible to output a sound source from an MP3 or WMV sound source through TLV320DAC3203?

    2. Is STM32F103RBT6 compatible…

1 2 3 4 5 »