Part Number: LMK05318BEVM
Other Parts Discussed in Thread: LMK05318B
Tool/software:
Hello,
I have LMK05318BEVM und it works very well.
I have been able to synchronise a 100 MHz output frequency to 1 KHz input frequency (phase and frequency) with the following thresholds paramters set in TICS Pro:
- For DPLL Phase Lock Detect:
- Lock thresh 7.59 ns
- Unlk thresh 484.45 ns
- For DPLL frequency Lock Detect:
- Accurcy 1 ppm
These thresholds are the maximum I could set depending on the input frequency. I found this out by simply testing several values. For example, when i set Unlk thresh under 484.45 ns the phase is no more locked. I check this using flags with the status0 led.
The thing is, according to the oscilloscope I get a phase offset between input and output within 5 ns max. But according to the parameters of the DPLL Phase Lock Detecter, the phase offset is almost 400 ns. The DPLL is considered to be phase locked if the phase difference between the two inputs of the TDC (divided reference and divided VCO1) is within the lock threshold. TDC frequency is 1 kHz because R devider is set to 1
I am confused. Who can help?
BR
Zain