Other Parts Discussed in Thread: TINA-TI
I am attempting to use the LM555 in monostable mode but the output doesn't generate a pulse. It simple follows the state of the trigger. I captured the attached waveform and it shows that the capacitor voltage (pin 6/7) doesn't disappear (CH3). Therefore, we see that the pulse "works" for the expected period of time but instead of going low, it enters this astable mode. It only goes low when trigger goes back to 1. I am using a digital IO PC card for the trigger manually so I am triggering much slower than the desired length of the pulse.
Note: Output has voltage divider so that measured pulse (CH4) is half the out value.
Datasheet examples always show trigger being a shorter pulse than the output pulse. Is this why? Does the trigger need to be shorter or it will otherwise keep the output on like I am seeing.