Other Parts Discussed in Thread: CDCE6214
Tool/software:
When using REFP/N as the reference, I'm seeing that the phase between the output clocks and the input reference appears to depend on the reference frequency.
I think I…
Tool/software:
Hi expert,
Hardware platform:J721EXSOMG01EVM + J721EXCP01EVM
Software:ti-processor-sdk-linux-adas-j721e-evm-09_02_00_05
1. The hardware schematic show EEPROMSEL…
Tool/software:
Hello expert,
May I know the programming times limitation for CDCE6214? For other solution from other product line, we can only program device twice. So we would like to know how many times we can program CDCE6214…
Hi,
I wish to replace the CDCI6214 to CDCE6214.
In TICS Pro. The CDCI6214 can set the LVCMOS output to CMOSP, CMOSN, and CMOSPN. Then it alos can set to P+ N+, P+ N…
Hi ,
we are using the CDCI6214 clock generator for creating a 100 MHz differential AC coupled LVDS clock.
We have programmed the EEPROM page 1 with the necessary configurations for the required clock and the clock output is properly…
Hi ,
we are using the CDCI6214 clock generator for creating a 100 MHz differential AC coupled LVDS clock. The device was configured as shown in the attached schematics.
At first, the SDA line of the connected configuration I2C was…
I am using the CDC16214 EVM along with the TI CS Pro software tool. When I bring up the software, it says Connection Mode: Disconnected. I have tried various USB cables and still no luck…
Hello,
My customer is looking for a suitable replacement part for IDT ICS841604AGI-01LF.
Could you please recommend a suitable TI part for IDT ICS841604AGI-01LF?
Thank you.
JH
Hi TI team,
CDCE6214TWRGETQ1 is used for one of our design. We have observed some difference between datasheet and EVK user guide.
Hi,
I am using the LMK03318 to generate several differential outputs. But the output7 peak to peak swing is always larger than other output. The swing is almost about 2V that…
Dear Team,
The CDCI6214 chip can work using the PAGE0 mode of the EEPROM after burning the EEPROM through the PC. Currently, I hope to use i2cget -y -f 19 0x76 0x1 w to dynamically read and write registers for debugging in this…
Hi Team,
This is technical support request for CDCI624. When CDCI6214 PLL unlock occurs, except for powering off and restarting, no matter how you configure the chip or RESET, it cannot return to normal. After merging the i2c of the…
Hi,
I'm trying to load my TICS Pro file onto my CDCI6214EVM board, the "USB2ANY" is connected and green, but when toggling the "PWR on/off" button, I get the "No Device Found!" pop-up.…
Dear Team,
We modify the board.
Output Y1 and Y2 will change the original output signal of R0A from LVDS to LVPECL output. Could you help to generate R0B clock gen code?
Please find the R0A code for your reference. Thanks.
Dear Team,
We change the original output signal of R0A from LVDS to LVPECL output, could you please help to generate a 24MP clock gen code ?
Thanks a lot.
Many Thanks,
Jimmy