• LMX2572EVM: lmx2572evm

    Part Number: LMX2572EVM
    Other Parts Discussed in Thread: LMX2572, LMX2594EVM

    Tool/software:

    Hi

    i would kike to use the part lmx2572 in my design . so required pcb design files of lmx2572evm to speed up the  design.

  • LMX2594EVM: Is it possible to use this evaluation board to modulate a laser

    Part Number: LMX2594EVM
    Other Parts Discussed in Thread: LMX2594

    Tool/software:

    Hello,  I am by no means an electrical engineer.  I see that this evaluation board can emit a signal up to 15GHz.  

    Here is a Lithium Niobate (LiNbO3) Mach-Zehnder Interferometer…

  • LMX2594EVM: Technical Inquiries

    Part Number: LMX2594EVM

    Tool/software:

    Hello E2E Experts,

    Good day.

    I would like to make sure that the component is compatible with my project.
    In my project, I would like to apply a very fast sweeper across two channels: 2.4 GHz and 5.8 GHz.
    I need to…

  • LMX2594EVM: Sweeping capabilities

    Part Number: LMX2594EVM
    Other Parts Discussed in Thread: LMX2594, LMX2492, LMX2491

    Tool/software:

    I would like to make sure that the component is compatible with my project.
    in my project, I would like to apply a very fast sweeper across two channels:…

  • LMX2594EVM: Is it possible to achieve 1 GHz bandwidth on a FMCW signal with the LMX2594 EVM evaluation board?

    Part Number: LMX2594EVM
    Other Parts Discussed in Thread: LMX2594, LMX2492

    Tool/software:

    I am doing a FMCW project and I would like to know if, to get a chirp at 10GHz and with a bandwidth of 1GHz, it is enough only with the LMX2594 EVM evaluation board…

  • LMX2594: Noisy output signal across frequency range of device

    Part Number: LMX2594
    Other Parts Discussed in Thread: LMX2572EVM, , LMX2572

    Tool/software:

    For a design I am currently debugging the LMX2594 and throughout the entire frequency range of the device the output signal is very noisy and not clean. Previously…

  • LMX2594EVM: Reference Pro Part number and SW required

    Part Number: LMX2594EVM
    Other Parts Discussed in Thread: LMX2594, USB2ANY,

    Tool/software:

    What is the orderable part number for the Reference Pro board referred to in the EVM User Manual?

    What SW needs to be downloaded as well?

    Thank you

  • LMX2594EVM: spurious

    Part Number: LMX2594EVM
    Other Parts Discussed in Thread: LMX2594, LMX2572, LMX2582

    Tool/software:

    Could you please give me some advias?
    I have checked Fpd and Fout in Figure 1 (Figure 2) with LMX2594.
    As a result, we confirmed the waveforms in Figure 3…

  • LMX2594EVM: LMX2492EVM & LMX2594EVM

    Part Number: LMX2594EVM
    Other Parts Discussed in Thread: LMX2492EVM, , LMX2594, PLLATINUMSIM-SW, LMX2492

    Tool/software:

    Hi Texas team,

    I am using LMX2492EVM and LMX2594EVM board for our application where we need Ramp signal which bandwidth will be 1.5…

  • TSW3065EVM: PLL modules standalone capabilities

    Part Number: TSW3065EVM
    Other Parts Discussed in Thread: TRF3765, LMX2594EVM, LMX2594, LMX2592, USB2ANY, LMX2592EVM

    Tool/software:

    Dear TI,

    We have 2 inquiries regarding TI PLLs:

    First inquiry

    We have acquired a module, the TSW3065EVM, which generates…

  • LMX2615-SP: LMX2615

    Part Number: LMX2615-SP
    Other Parts Discussed in Thread: LMX2594EVM

    Tool/software:

    Hello 

    Now I am testing LMX2615-SP.

    I use TICS Pro to obtain Register MAP.

    For the datasheet, the division value is equivalent to 72.

    However, there is no value for TICS…

  • LMX2594EVM: How to set up the SYNC function of the LMX2594EVM using the LMK04828B as a signal source

    Part Number: LMX2594EVM
    Other Parts Discussed in Thread: LMX2594

    Tool/software:

    Hello.

    I want to synchronize using the SYNC function with LMX2594EVM.

    The OSCin and SYNC signals are generated by LMK04828B, and the settings are as shown in the image below…

  • LMX2594EVM: LMX2594

    Part Number: LMX2594EVM

    Tool/software:

    How is the phase noise power spectral density of VCO and OSC calculated from the given values for 1/f^3 noise and 1/f2 noise and noise floor of VCO and OSC
    they are given as dBc/Hz values for 1/f^3 and 1/f^2 and…

  • LMX2594EVM: LMX2594EVM SPI configuration

    Part Number: LMX2594EVM
    Other Parts Discussed in Thread: USB2ANY, LMX2492EVM, LMX2492

    Tool/software:

    Hi Texas team,

    We want to use LMX2594EVM board for our application. We have some enquiry about it which is given below,

    1. Is it needed to buy separate…

  • LMX2594EVM: Intermittent Locking

    Part Number: LMX2594EVM
    Other Parts Discussed in Thread: LMX2594

    I am not able to get the LMX2594 to consistently lock with the following settings in TICS Pro:

     

    When I change the CAL_CLK_DIV from Div1 to Div8 it locks every time.  Any idea why this is the…

  • LMX2594: Inconsistent VTUNE for output freq.

    Part Number: LMX2594

    Hi, 

    I'm mesuring VTUNE pin of the eval-board LMX2594EVM and I found the VTUNE voltage mesured on scope is inconsistent to the expected values.

    In fact, I would like to generate a linear sawtooth ramp from 5GHz to 5.025GHz (so…

  • LMX2572LPEVM: Design files

    Part Number: LMX2572LPEVM
    Other Parts Discussed in Thread: LMX2594, LMX2594EVM, LMX2572LP

    Hi,

    Are the design files or step model of LMX2572LPEVM available for download anywhere?

  • LMX2594EVM: VCC not drawing enough voltage

    Part Number: LMX2594EVM

    Hello,

    I am using the LMX2594EVM. I set the power supply that I am using to 3.3V and 600mA. However, upon power up I see that the power supply reads only ~800mV with 600mA output.

    What could be causing this? The EVM looks to not…

  • LMX2594: LMX2594 Spurs when toggling output

    Part Number: LMX2594

    I am using the LMX2594EVM right now and I am trying to replicate frequency hopping, however I have noticed that when I change frequencies (N, NUM, DEN) I need to disable the output otherwise I get weird products while the registers…

  • LMX2594EVM: LMX2594EVM boards (SV601308)

    Dear Mr.Derek Payne, good morning. Could you please indicate the tool/instrument used to create the graphs presented in Figures 2-2 to 2-27, and in Figures 3-1 and 3-2,

    included within the Application Report "Streamline RF Synthesizer VCO Calibration…

  • LMX2595:ramp

    Part Number: LMX2595
    Other Parts Discussed in Thread: LMX2572EVM, LMX2594EVM

    我想使用 lmx2595 芯片生成 4 到 4.1GHz 斜坡信号,如何配置我的 TICS pro,我已经生成了 4GHz 静态信号,请告诉我过程并附上图片,非常感谢

  • LMX2594EVM: Lower output power near 13.5GHz

    Part Number: LMX2594EVM
    Other Parts Discussed in Thread: LMX2594

    Hi,

    I accidently observed a much lower output power near 13,5GHz by using inductor pull-up method, see picture below:

    I'm wondering where it comes from. The first reflection is the resonance…

  • LMX2594EVM: Require the information on frequency capability and output power as well as phase noise

    Part Number: LMX2594EVM
    Other Parts Discussed in Thread: LMX2594

    Hello Sir,

    I am reaching out to inquire about the frequency output capabilities of the LMX2924 synthesizer, as well as the availability of its measured phase noise graph.

    We are looking for…

  • LMX2594: Not Responding to SPI Commands

    Part Number: LMX2594
    Other Parts Discussed in Thread: LMK61PD0A2, USB2ANY,

    I am using an Arty-A7 FPGA dev board to send SPI Commands into the LMX2594. When I send my commands I get no response from the device, I have verified the boards operation by programming…

  • LMX2594EVM: Reference Pro board drawing

    Part Number: LMX2594EVM

    The EVM kit comes with a Reference Pro board. 

    Is a mechanical drawing showing the size and hole locations of the Reference Pro available?

1 2 3 4 5 »