This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
// config SER ub941 0x0c 0x1E 0x03 // Select FPD-Link III Port 0 and Port1 0x0c 0x66 0x1A 0x0c 0x67 0x03 // M = 3 0x0c 0x66 0x03 0x0c 0x67 0x19 // N = 25, set CLK= 800*3/25 = 96M 0x0c 0x01 0x08 // Disable DSI 0x0c 0x1E 0x01 // Select FPD-Link III Port 0 0x0c 0x4F 0x8C // Set DSI_CONTINUOUS_CLOCK, 4 lanes, DSI Port 0 0x0c 0x5b 0x07 // Force split mode 0x0c 0x56 0x80 // port0 dsi continue clock 0x0c 0x32 0x80 // Set the line size to 1920(LSB) 0x0c 0x33 0x07 // Set the line size to 1920 (MSB) 0x0c 0x1E 0x01 // Select FPD-Link III Port 0 0x0c 0x36 0x00 // Set crop start X position to 0 (LSB) 0x0c 0x37 0x80 // Set crop start X position to 0 (MSB) and enable cropping 0x0c 0x38 0x7F // Set crop stop X position to 1919 (LSB) 0x0c 0x39 0x07 // Set crop stop X position to 1919 (MSB) 0x0c 0x3A 0x00 // Set crop start Y position to 0 (LSB) 0x0c 0x3B 0x00 // Set crop start Y position to 0 (MSB) 0x0c 0x3C 0xCF // Set crop stop Y position to 719 (LSB) 0x0c 0x3D 0x02 // Set crop stop Y position to 719 (MSB) 0x0c 0x1E 0x02 // Select FPD-Link III Port 1 0x0c 0x36 0x00 // Set crop start X position to 0 (LSB) 0x0c 0x37 0x80 // Set crop start X position to 0 (MSB) and enable cropping 0x0c 0x38 0x7F // Set crop stop X position to 1919 (LSB) 0x0c 0x39 0x07 // Set crop stop X position to 1919 (MSB) 0x0c 0x3A 0x00 // Set crop start Y position to 0 (LSB) 0x0c 0x3B 0x00 // Set crop start Y position to 0 (MSB) 0x0c 0x3C 0xCF // Set crop stop Y position to 719 (LSB) 0x0c 0x3D 0x02 // Set crop stop Y position to 719 (MSB) 0x0c 0x40 0x04 // Select DSI Port 0 digital registers 0x0c 0x41 0x05 // Select DPHY_SKIP_TIMING register 0x0c 0x42 0x42 // Write TSKIP_CNT value for 577 MHz DSI clock frequency 0x0c 0x40 0x10 // Init DSI clock settings (section 10.2 of the datasheet) 0x0c 0x41 0x86 0x0c 0x42 0x0A 0x0c 0x41 0x94 0x0c 0x42 0x0A 0x0c 0x1e 0x01 // passthrough all i2c dev to soc side 0x0c 0x17 0x9e 0x0c 0x1e 0x02 // passthrough all i2c dev to soc side 0x0c 0x17 0x9e 0x0c 0x1e 0x04 0x0c 0x17 0x9e delay(50ms) // config DES1 ub948 0x34 0x01 0xff delay(5ms) 0x34 0x1d 0x13 0x34 0x26 0x15 0x34 0x27 0x15 0x34 0x41 0x1f 0x34 0x4b 0x0a // config DES1 ub948 0x0c 0x01 0xff delay(5ms) 0x0c 0x56 0x80 0x0c 0x01 0x00 0x0c 0x64 0x00 0x0c 0x65 0x00 // config BL1 0x15 0x03 0xff // set brightness value 0x15 0x04 0x01 // enable backlight 1 // config BL1 0x6B 0x03 0xff // set brightness value 0x6B 0x04 0x01 // enable backlight 2 // SER ub941 0x0c 0x01 0x00 //enable DSI
Mode Info:1. Host SoC: Qcom SA8155
2. Backlight1 and Backlight 2 is on
3. DSI clock is continues
4. Host config image size is 3840x720@60fps
5. Host config timing:
Hello,
I will look over this script to make sure it is correct. In the meantime can you confirm a few things:
Regards,
Ben
/* Panel Timing: H-width :1920, HFP:32 HBP:64 HVsync:32 V-height:720, VFP:36 VBP:18 VSync :8 */ 0x0c 0x1E 0x03 // Select FPD-Link III Port 0 and Port1 0x0c 0x66 0x04 // Set H-Total 0x800, 2048(1920+32+64+32); V-Total 0x30E, 782(720+36+18+8); 0x0c 0x67 0x00 0x0c 0x66 0x05 0x0c 0x67 0xE8 0x0c 0x66 0x06 0x0c 0x67 0x30 0x0c 0x66 0x07 // Set H-Width 0x780, 1920; V-Height 0x2d0, 720; 0x0c 0x67 0x80 0x0c 0x66 0x08 0x0c 0x67 0x07 0x0c 0x66 0x09 0x0c 0x67 0x2D 0x0c 0x66 0x0A // Set HSync 32, VSync 8 0x0c 0x67 0x20 0x0c 0x66 0x0B 0x0c 0x67 0x08 0x0c 0x66 0x0C // Set HBP 64, VBP 18 0x0c 0x67 0x40 0x0c 0x66 0x0D 0x0c 0x67 0x12 0x0c 0x66 0x0E 0x0c 0x67 0x03 0x0c 0x65 0x0C // set external clock and internal PATGEN timing 0x0c 0x64 0x05 // enable PG, corlor bar
Hi Ben:
use above patgen code, panel1 and panel2 can display color bars;
Pattern Generator Timing as above, Horizonta timing is 1/2 of host.
SA8155 config full Timing:
3840x720@60fps,
H-width :3840, HFP:64 HBP:128 HVsync:64
V-height:720, VFP:36 VBP:18 VSync :8
Hello,
I regenerated a script for you. Please try this script to see if there is any improvement:
# 941AS Superframe config # Python script : Superframe_Crop_3840x720 import time UH941AS = 4 board.WriteI2C(UH941AS,0x01,0x08) #Disable DSI # set split mode, left/right 3D image, non-continuous clock mode board.WriteI2C(UH941AS,0x1E,0x01) #Select Port0 board.WriteI2C(UH941AS,0x5B,0x07) #Force Splitter Mode board.WriteI2C(UH941AS,0x56,0x80) #Enable conversion of L/R image into alternating pixel image board.WriteI2C(UH941AS, 0x4F, 0x8C) #Set 4 lane DSI ##### Register 4F code configuration limited to use case of single DSI mode (RX Port 0) and no Altnerate line mode. If you would like to change the mode, please see register 0x4F [6:4] in D/S board.WriteI2C(UH941AS,0x1E,0x02) #Select Port1 board.WriteI2C(UH941AS,0x5B,0x07) #Force Splitter Mode board.WriteI2C(UH941AS,0x56,0x80) #Enable conversion of L/R image into alternating pixel image board.WriteI2C(UH941AS, 0x4F, 0x8C) #Set 4 lane DSI ##### Register 4F code configuration limited to use case of single DSI mode (RX Port 0) and no Altnerate line mode. If you would like to change the mode, please see register 0x4F [6:4] in D/S board.WriteI2C(UH941AS, 0x1E, 0x01) # Select Port0 board.WriteI2C(UH941AS, 0x32, 0x80) #Set IMG_LINE_SIZE board.WriteI2C(UH941AS, 0x33, 0x07) #Set IMG_LINE_SIZE board.WriteI2C(UH941AS, 0x36, 0x00) #Set crop start X position (LSB) board.WriteI2C(UH941AS, 0x37, 0x80) #Set crop start X position (MSB) board.WriteI2C(UH941AS, 0x38, 0x7F) #Set crop stop X position (LSB) board.WriteI2C(UH941AS, 0x39, 0x07) #Set crop stop X position (MSB) board.WriteI2C(UH941AS, 0x3A, 0x00) #Set crop start Y position (LSB) board.WriteI2C(UH941AS, 0x3B, 0x00) #Set crop start Y position (MSB) board.WriteI2C(UH941AS, 0x3C, 0xCF) #Set crop stop Y position (MSB) board.WriteI2C(UH941AS, 0x3D, 0x02) #Set crop start Y position (LSB) board.WriteI2C(UH941AS, 0x1E, 0x02) # Select Port1 board.WriteI2C(UH941AS, 0x36, 0x00) #Set crop start X position (LSB) board.WriteI2C(UH941AS, 0x37, 0x80) #Set crop start X position (MSB) board.WriteI2C(UH941AS, 0x38, 0x7F) #Set crop stop X position (LSB) board.WriteI2C(UH941AS, 0x39, 0x07) #Set crop stop X position (MSB) board.WriteI2C(UH941AS, 0x3A, 0x00) #Set crop start Y position (LSB) board.WriteI2C(UH941AS, 0x3B, 0x00) #Set crop start Y position (MSB) board.WriteI2C(UH941AS, 0x3C, 0xCF) #Set crop stop Y position (MSB) board.WriteI2C(UH941AS, 0x3D, 0x02) #Set crop start Y position (LSB) board.WriteI2C(UH941AS,0x1E,0x01) # Select Port0 board.WriteI2C(UH941AS, 0x40, 0x04) # Select DSI digital page board.WriteI2C(UH941AS, 0x41, 0x05) # To reg 0x05 (TSKIP CNT) board.WriteI2C(UH941AS, 0x42, 0x1C) # Set value for DSI+CLK board.WriteI2C(UH941AS,0x40,0x08) # Select DSI digital page board.WriteI2C(UH941AS,0x41,0x05) # To reg 0x05 (TSKIP CNT) board.WriteI2C(UH941AS, 0x42, 0x1C) # Set value for DSI+CLK board.WriteI2C(UH941AS,0x01,0x00) #Enable DSI
Regards,
Ben
// config patgen 0c 1E 03 0c 66 04 0c 67 00 0c 66 05 0c 67 E8 0c 66 06 0c 67 30 0c 66 07 0c 67 80 0c 66 08 0c 67 07 0c 66 09 0c 67 2D 0c 66 0A 0c 67 20 0c 66 0B 0c 67 08 0c 66 0C 0c 67 40 0c 66 0D 0c 67 12 0c 66 0E 0c 67 03 0c 65 0C 0c 64 05 // copy form Superframe_Crop_3840x720.py 0C 01 08 0C 1E 01 0C 5B 07 0C 56 80 0C 4F 8C 0C 1E 02 0C 5B 07 0C 56 80 0C 4F 8C 0C 1E 01 0C 32 80 0C 33 07 0C 36 00 0C 37 80 0C 38 7F 0C 39 07 0C 3A 00 0C 3B 00 0C 3C CF 0C 3D 02 0C 1E 02 0C 36 00 0C 37 80 0C 38 7F 0C 39 07 0C 3A 00 0C 3B 00 0C 3C CF 0C 3D 02 0C 1E 01 0C 40 04 0C 41 05 0C 42 1C 0C 40 08 0C 41 05 0C 42 1C // config i2c 0c 1e 01 0c 17 9e 0c 1e 02 0c 17 9e 0c 1e 04 0c 17 9e // set remote slave FF 50 // delay(50ms) 34 01 ff FF 5 34 1d 13 34 26 15 34 27 15 34 41 1f 34 4b 0a 2c 01 ff FF 5 2c 1d 13 2c 26 15 2c 27 15 2c 41 1f 2c 4b 0a FF 2 6B 04 01 15 04 01 FF 2 6B 03 FF 15 03 FF // disable patgen 0c 1e 03 0c 65 00 0c 64 00 0c 1e 04 // enable dsi 0c 01 00
Hi ben;
I try the setting of Superframe_Crop_3840x720.py, The phenomenon is the same as before(backlight is on, but panel not display image);
setting as above.
I try config SA8155 output 1920x720 size image ,and config ub941 work in single-link-mode, Panel1 can display image;
I have a question, what is the difference between split-mode and sing-link mode input formats? I understand it's just the size is different. so, I configure the host side output just to increase the image size and h-porch for split-mode;is or right?
Hi,
The PCLK and the horizontal timing needs to be twice the size of a single image, yes.
Can you confirm a couple more things?
Regards,
Ben
Hi Ben:
How to confirm lock established with 948s? measure lock pin level of 948s? or read which register of 948s? what's the meaning of lock status ?
I try patgen with external timing and external clock(change reg 0x64=0x08), panel is not display.
Hi Ben:
There are new phenomena:
I try config non_burst_sync_pulse for dsi hs-mode,
Hi,
Thank you for the updates, this narrows down the issue significantly. Can you ensure that the DSI source follows the MIPI DSI standard closely, and enables LP-11 during at least one of the BLLP periods of the video frame?
Can you also check the indirect register 0x2A to confirm the DSI_DTYPE is reported correctly?
If the DSI source is correctly implementing LP-11 transitions, and the DSI_DTYPE is correct, you may need to check the DSI source with a protocol analyzer. Instructions on how to check these things are described in the DS90UB941AS-Q1 DSI Bringup Guide.
Regards,
Ben
Hi Ben:
1. readback register 0x2A (DSI_DTYPE ), value is 0x3E;
2. indirect register 0x05(TSKIP_CNT) config value is 0x42, (Other values have also been tried).
3. Measured by oscilloscope, LP11 per frame, continuous clock, fps 60HZ
4. Check items as described in the documentation DS90UB941AS-Q1 DSI Bringup Guide,No obvious abnormality found .
Which reasons may cause the following phenomena?
Phenomena:
Using the line interleaved source image to test, Panel1 displays odd lines of content,Panel2 shows even lines;but the right half of the source image is not displayed.
sourceimage:
Hi,
It seems that Alternate line splitting is occurring while Left/Right (Side by Side) Splitting is what is needed. Can you provide a register dump? I would like to check to make sure the device programming reflects the script, as well as check register 0x58 VIDEO_3D_STS to see if video processing errors have been detected.
Regards,
Ben
UB941S main registers dump: reg_addr 0x0 = 0x18 reg_addr 0x1 = 0x0 reg_addr 0x2 = 0x0 reg_addr 0x3 = 0x92 reg_addr 0x4 = 0x0 reg_addr 0x5 = 0x0 reg_addr 0x6 = 0x68 reg_addr 0x7 = 0x0 reg_addr 0x8 = 0x0 reg_addr 0x9 = 0x1 reg_addr 0xA = 0xAE reg_addr 0xB = 0x0 reg_addr 0xC = 0x57 reg_addr 0xD = 0x30 reg_addr 0xE = 0x0 reg_addr 0xF = 0x0 reg_addr 0x10 = 0x0 reg_addr 0x11 = 0x0 reg_addr 0x12 = 0x0 reg_addr 0x13 = 0x8F reg_addr 0x14 = 0x0 reg_addr 0x15 = 0x0 reg_addr 0x16 = 0xFE reg_addr 0x17 = 0x9E reg_addr 0x18 = 0x7F reg_addr 0x19 = 0x7F reg_addr 0x1A = 0x1 reg_addr 0x1B = 0x0 reg_addr 0x1C = 0x0 reg_addr 0x1D = 0x0 reg_addr 0x1E = 0x4 reg_addr 0x1F = 0x0 reg_addr 0x20 = 0xB reg_addr 0x21 = 0x0 reg_addr 0x22 = 0x25 reg_addr 0x23 = 0x0 reg_addr 0x24 = 0x0 reg_addr 0x25 = 0x0 reg_addr 0x26 = 0x0 reg_addr 0x27 = 0x0 reg_addr 0x28 = 0x1 reg_addr 0x29 = 0x20 reg_addr 0x2A = 0x20 reg_addr 0x2B = 0xA0 reg_addr 0x2C = 0x0 reg_addr 0x2D = 0x0 reg_addr 0x2E = 0xA5 reg_addr 0x2F = 0x5A reg_addr 0x30 = 0x0 reg_addr 0x31 = 0x9 reg_addr 0x32 = 0x80 reg_addr 0x33 = 0x7 reg_addr 0x34 = 0xC reg_addr 0x35 = 0x0 reg_addr 0x36 = 0x0 reg_addr 0x37 = 0x80 reg_addr 0x38 = 0x7F reg_addr 0x39 = 0x7 reg_addr 0x3A = 0x0 reg_addr 0x3B = 0x0 reg_addr 0x3C = 0xCF reg_addr 0x3D = 0x2 reg_addr 0x3E = 0x81 reg_addr 0x3F = 0x2 reg_addr 0x40 = 0x8 reg_addr 0x41 = 0x20 reg_addr 0x42 = 0xF reg_addr 0x43 = 0x0 reg_addr 0x44 = 0x0 reg_addr 0x45 = 0x0 reg_addr 0x46 = 0x0 reg_addr 0x47 = 0x0 reg_addr 0x48 = 0x0 reg_addr 0x49 = 0x0 reg_addr 0x4A = 0x0 reg_addr 0x4B = 0x0 reg_addr 0x4C = 0x0 reg_addr 0x4D = 0x0 reg_addr 0x4E = 0x0 reg_addr 0x4F = 0x8C reg_addr 0x50 = 0x16 reg_addr 0x51 = 0x0 reg_addr 0x52 = 0x0 reg_addr 0x53 = 0x0 reg_addr 0x54 = 0x2 reg_addr 0x55 = 0x10 reg_addr 0x56 = 0x80 reg_addr 0x57 = 0x2 reg_addr 0x58 = 0x3 reg_addr 0x59 = 0x0 reg_addr 0x5A = 0xF9 reg_addr 0x5B = 0x7 reg_addr 0x5C = 0x7 reg_addr 0x5D = 0x6 reg_addr 0x5E = 0x44 reg_addr 0x5F = 0x61 reg_addr 0x60 = 0x22 reg_addr 0x61 = 0x2 reg_addr 0x62 = 0x0 reg_addr 0x63 = 0x0 reg_addr 0x64 = 0x0 reg_addr 0x65 = 0x0 reg_addr 0x66 = 0xE reg_addr 0x67 = 0x3 reg_addr 0x68 = 0x0 reg_addr 0x69 = 0x0 reg_addr 0x6A = 0x0 reg_addr 0x6B = 0x0 reg_addr 0x6C = 0x0 reg_addr 0x6D = 0x2 reg_addr 0x6E = 0x20 reg_addr 0x6F = 0x0 reg_addr 0x70 = 0x0 reg_addr 0x71 = 0x0 reg_addr 0x72 = 0x0 reg_addr 0x73 = 0x0 reg_addr 0x74 = 0x0 reg_addr 0x75 = 0x0 reg_addr 0x76 = 0x0 reg_addr 0x77 = 0x0 reg_addr 0x78 = 0x0 reg_addr 0x79 = 0x0 reg_addr 0x7A = 0x0 reg_addr 0x7B = 0x0 reg_addr 0x7C = 0x0 reg_addr 0x7D = 0x0 reg_addr 0x7E = 0x7F reg_addr 0x7F = 0x0 reg_addr 0x80 = 0x0 reg_addr 0x81 = 0x0 reg_addr 0x82 = 0x0 reg_addr 0x83 = 0x0 reg_addr 0x84 = 0x0 reg_addr 0x85 = 0x0 reg_addr 0x86 = 0x0 reg_addr 0x87 = 0x0 reg_addr 0x88 = 0x0 reg_addr 0x89 = 0x0 reg_addr 0x8A = 0x0 reg_addr 0x8B = 0x0 reg_addr 0x8C = 0x0 reg_addr 0x8D = 0x0 reg_addr 0x8E = 0x0 reg_addr 0x8F = 0x0 reg_addr 0x90 = 0x0 reg_addr 0x91 = 0x0 reg_addr 0x92 = 0x0 reg_addr 0x93 = 0x0 reg_addr 0x94 = 0x0 reg_addr 0x95 = 0x0 reg_addr 0x96 = 0x0 reg_addr 0x97 = 0x0 reg_addr 0x98 = 0x0 reg_addr 0x99 = 0x0 reg_addr 0x9A = 0x0 reg_addr 0x9B = 0x0 reg_addr 0x9C = 0x0 reg_addr 0x9D = 0x0 reg_addr 0x9E = 0x0 reg_addr 0x9F = 0x0 reg_addr 0xA0 = 0x0 reg_addr 0xA1 = 0x0 reg_addr 0xA2 = 0x0 reg_addr 0xA3 = 0x0 reg_addr 0xA4 = 0x0 reg_addr 0xA5 = 0x0 reg_addr 0xA6 = 0x0 reg_addr 0xA7 = 0x0 reg_addr 0xA8 = 0x0 reg_addr 0xA9 = 0x0 reg_addr 0xAA = 0x0 reg_addr 0xAB = 0x0 reg_addr 0xAC = 0x0 reg_addr 0xAD = 0x0 reg_addr 0xAE = 0x0 reg_addr 0xAF = 0x0 reg_addr 0xB0 = 0x0 reg_addr 0xB1 = 0x0 reg_addr 0xB2 = 0x0 reg_addr 0xB3 = 0x0 reg_addr 0xB4 = 0x0 reg_addr 0xB5 = 0x0 reg_addr 0xB6 = 0x0 reg_addr 0xB7 = 0x0 reg_addr 0xB8 = 0x0 reg_addr 0xB9 = 0x0 reg_addr 0xBA = 0x0 reg_addr 0xBB = 0x0 reg_addr 0xBC = 0x0 reg_addr 0xBD = 0x0 reg_addr 0xBE = 0x0 reg_addr 0xBF = 0x0 reg_addr 0xC0 = 0x0 reg_addr 0xC1 = 0x0 reg_addr 0xC2 = 0x82 reg_addr 0xC3 = 0x0 reg_addr 0xC4 = 0x38 reg_addr 0xC5 = 0x0 reg_addr 0xC6 = 0x0 reg_addr 0xC7 = 0x64 reg_addr 0xC8 = 0x40 reg_addr 0xC9 = 0x0 reg_addr 0xCA = 0x0 reg_addr 0xCB = 0x0 reg_addr 0xCC = 0x0 reg_addr 0xCD = 0x2 reg_addr 0xCE = 0xFF reg_addr 0xCF = 0x0 reg_addr 0xD0 = 0x0 reg_addr 0xD1 = 0x0 reg_addr 0xD2 = 0x0 reg_addr 0xD3 = 0x0 reg_addr 0xD4 = 0x0 reg_addr 0xD5 = 0x0 reg_addr 0xD6 = 0x0 reg_addr 0xD7 = 0x0 reg_addr 0xD8 = 0x0 reg_addr 0xD9 = 0x0 reg_addr 0xDA = 0x0 reg_addr 0xDB = 0x0 reg_addr 0xDC = 0x0 reg_addr 0xDD = 0x0 reg_addr 0xDE = 0x0 reg_addr 0xDF = 0x0 reg_addr 0xE0 = 0x0 reg_addr 0xE1 = 0x0 reg_addr 0xE2 = 0x82 reg_addr 0xE3 = 0x0 reg_addr 0xE4 = 0x28 reg_addr 0xE5 = 0x8 reg_addr 0xE6 = 0x0 reg_addr 0xE7 = 0x0 reg_addr 0xE8 = 0x0 reg_addr 0xE9 = 0x0 reg_addr 0xEA = 0x0 reg_addr 0xEB = 0x0 reg_addr 0xEC = 0x0 reg_addr 0xED = 0x2 reg_addr 0xEE = 0x0 reg_addr 0xEF = 0x0 reg_addr 0xF0 = 0x5F reg_addr 0xF1 = 0x55 reg_addr 0xF2 = 0x42 reg_addr 0xF3 = 0x39 reg_addr 0xF4 = 0x34 reg_addr 0xF5 = 0x31 reg_addr 0xF6 = 0x0 reg_addr 0xF7 = 0x0 reg_addr 0xF8 = 0x0 reg_addr 0xF9 = 0x0 reg_addr 0xFA = 0x0 reg_addr 0xFB = 0x0 reg_addr 0xFC = 0x0 reg_addr 0xFD = 0x0 reg_addr 0xFE = 0x0 UB941S DSI Port 0 indirect registers dump: offset_addr 0x0 = 0x0 offset_addr 0x1 = 0x0 offset_addr 0x2 = 0x0 offset_addr 0x3 = 0x1D offset_addr 0x4 = 0x14 offset_addr 0x5 = 0x40 offset_addr 0x6 = 0x0 offset_addr 0x7 = 0x0 offset_addr 0x8 = 0x0 offset_addr 0x9 = 0x0 offset_addr 0xA = 0x0 offset_addr 0xB = 0x0 offset_addr 0xC = 0x0 offset_addr 0xD = 0x0 offset_addr 0xE = 0x0 offset_addr 0xF = 0x1F offset_addr 0x10 = 0x0 offset_addr 0x11 = 0x0 offset_addr 0x12 = 0x0 offset_addr 0x13 = 0x0 offset_addr 0x14 = 0x0 offset_addr 0x15 = 0x0 offset_addr 0x16 = 0x0 offset_addr 0x17 = 0x0 offset_addr 0x18 = 0x0 offset_addr 0x19 = 0x0 offset_addr 0x1A = 0x0 offset_addr 0x1B = 0x0 offset_addr 0x1C = 0x0 offset_addr 0x1D = 0x0 offset_addr 0x1E = 0x0 offset_addr 0x1F = 0x0 offset_addr 0x20 = 0x0 offset_addr 0x21 = 0x0 offset_addr 0x22 = 0xFF offset_addr 0x23 = 0x7F offset_addr 0x24 = 0x0 offset_addr 0x25 = 0x0 offset_addr 0x26 = 0x0 offset_addr 0x27 = 0x0 offset_addr 0x28 = 0x1 offset_addr 0x29 = 0xFF offset_addr 0x2A = 0x3E offset_addr 0x2B = 0x18 offset_addr 0x2C = 0x0 offset_addr 0x2D = 0x0 offset_addr 0x2E = 0x0 offset_addr 0x2F = 0x0 offset_addr 0x30 = 0x0 offset_addr 0x31 = 0x40 offset_addr 0x32 = 0x0 offset_addr 0x33 = 0x8 offset_addr 0x34 = 0x0 offset_addr 0x35 = 0x20 offset_addr 0x36 = 0x0 offset_addr 0x37 = 0x0 offset_addr 0x38 = 0x0 offset_addr 0x39 = 0x0 offset_addr 0x3A = 0x2 offset_addr 0x3B = 0x3
0c 1E 03 0c 66 04 0c 67 00 0c 66 05 0c 67 E8 0c 66 06 0c 67 30 0c 66 07 0c 67 80 0c 66 08 0c 67 07 0c 66 09 0c 67 2D 0c 66 0A 0c 67 20 0c 66 0B 0c 67 08 0c 66 0C 0c 67 40 0c 66 0D 0c 67 12 0c 66 0E 0c 67 03 0c 65 0C 0c 64 05 0C 01 08 0C 1E 01 0C 5B 07 0C 56 80 0C 4F 8C 0C 1E 02 0C 5B 07 0C 56 80 0C 4F 8C 0C 1E 01 0C 32 80 0C 33 07 0C 36 00 0C 37 80 0C 38 7F 0C 39 07 0C 3A 00 0C 3B 00 0C 3C CF 0C 3D 02 0C 1E 02 0C 36 00 0C 37 80 0C 38 7F 0C 39 07 0C 3A 00 0C 3B 00 0C 3C CF 0C 3D 02 0C 1E 01 0C 40 04 0C 41 05 0C 42 40 0C 41 20 0C 42 00 0C 41 30 0C 42 00 0C 41 31 0C 42 40 0C 41 32 0C 42 00 0C 41 33 0C 42 08 0C 40 08 0C 41 05 0C 42 40 0C 41 20 0C 42 0F 0c 1e 01 0c 17 9e 0c 1e 02 0c 17 9e 0c 1e 04 0c 17 9e FF 64 34 01 ff FF 5 34 1d 13 34 26 15 34 27 15 34 41 1f 34 4b 0a 2c 01 ff FF 5 2c 1d 13 2c 26 15 2c 27 15 2c 41 1f 2c 4b 0a FF 2 6B 04 01 15 04 01 FF 2 6B 03 FF 15 03 FF 0c 1e 03 0c 65 00 0c 64 00 0c 1e 04 0c 01 00
Hi Ben:
Please check the above dump file and setting file; Restart the machine, the value of register 0x58(VIDEO_3D_STS ) is different, there are one of the following values: 0x03, 0x02, 0x01, 0x00;
Found a new problem, when the machine is completely powered off and restarted, i2c write backlight2 will fail probabilistically and backlight2 not on, what is the possible reason?
Hello,
Based on the VIDEO_3D_STS errors, it seems that the DSI source is not transmitting the correct timing to the 941AS. Do you have the capability to check the DSI source with protocol analyzer?
Regards,
Ben
Hi,
Okay, I believe I can assist in giving instructions on how to extract the timing parameters, but I will need to give these instructions over private message since this is a public thread.
Regards,
Ben
Hello,
I am closing this thread for now as we have taken this discussion to private message. Please post here again if additional support is needed.
Please be noted that the E2E support forums will undergo maintenance from Sept. 28 to Oct. 2, hence it will not be available during this time. If you need design support during this time, please contact your TI representative
Normal E2E support should be back by Monday, Oct. 3.
Regards,
Ben
Hi Ben:
Thank you very much for your support;Now, Split-Mode display can display correctly;
Because the dsi source is abnormal; when the configuration width is greater than 2560, the SA8155 display module will separate the image buffer and use two LMs to process the image buffer, which will eventually cause the dsi output to be non-surperframe source.