Other Parts Discussed in Thread: DP83867E
Hi Team,
When we ran a 10Base-Te Peak Differential Voltage compliance test on his DP83867CS board,
the compliance test results were as follows:
We would appreciate any advice regarding the results of the compliance test.
<10Base-Te Peak Differential Voltage Results>
1.Test Board
(1)No.1_Board
①First time :1.55[V] ---- PASS
②second time:1.56[V] ---- PASS
(2)No.2_Board
①First time :1.528[V] ---- FAIL
②second time:1.518[V] ---- FAIL
The above No.1_Board and No.2_Board differ only in PHY parts.
2.Procedure of test
Based on the e2e results below, we used a pseudo-random signal using the PHY BIST (0x16) function as the test signal.
<Referenced e2e>
e2e.ti.com/.../dp83867ir-10base-te-100base-tx-1000base-t-compliance-test
As the test signal, we used a pseudorandom signal generated by the PHY BIST (0x16) function.
Below, register settings
0x1f 0x8000, PHY RESET
0x00 0x0100, 10Base-T / Te mode
0x10 0x5008, Forced MDI mode
0x16 0xd80
Please tell me about the following.
[Question 1]
We use P83867CSRGZ as PHY component.
When I checked the description of VOD (Vpeak Differential) for 10BASE-Te in the data sheet,
I found that the MIN/MAX values for ERGZ/ISRGZ were listed, but the MIN/MAX values for CSRGZ were not listed.
Does the lack of CSRGZ specification mean that 10BASE-Te VOD (Vpeak Differential) is not guaranteed?
Please let me know if there are any regulations for the MIN and MAX values of CSRGZ.
[Question 2]
I think the output of Peak Differential Voltage varies depending on the PHY parts.
Is it possible to adjust the differential voltage output of 10BASE-Te?
Best Regards,