Tool/software:
Hi, I am using TXB0108DQSR for my design. I noticed that there are differences between the pinout reported in the datasheet and the symbol and footprint I found on the Texas Instruments website.
For better understanding…
Tool/software:
Hi, I am using TXB0108DQSR for my design. I noticed that there are differences between the pinout reported in the datasheet and the symbol and footprint I found on the Texas Instruments website.
For better understanding…
Tool/software:
Hi,
My customer is using this device to translate from 1.8V to 3.3V
What is the minimum pull up resistance required to guarantee correct direction? (for both directions?) Thank you!
Tool/software:
Tool/software:
ご協力いただきありがとうございます。
5V自動方向検出バストランシーバをご存知の場合は、お知らせください。
理想的には、自動方向検出が追加されたCD74ACT245Eのようなものです。
よろしくお願いいたします。
Tool/software:
Hi there
Our customer wants to use a channel as both a digital input and a digital output. The digital input side should be 5V tolerant, while the digital output…
Tool/software:
Hi all,
Planning to use a TXB0108 level shifter for converting 5 V to 3.3 V to interface with my Zynq 7000 FPGA. Schematic photos as attached.
The inputs…
Tool/software:
Dears,
The customer uses a level conversion chip, and the specific application is to realize PBI bus communication between DSP F28377D and a communication board. Now I want to choose a bidirectional level conversion…
Tool/software:
Hello,
I see no ramp time specification related to the OE port.
Can I drive this with an RC ramp of 2ms/V without any issues?
Thank You,
Tool/software:
Greetings Everyone,
How are you all doing? Just a few questions for you
1) Where to download IBIS models for the TXB0108, TXU0304BQAR, SN74LXC2T45DTTR, SN74LXC8T245PWR, SN74AVC4T245RSV
2) Need to speak with someone about…
Tool/software:
Hello support team,
My customer would like to use buffer/driver at SPI signal and eSPI signal. (1.8V, open-drain preferred.)
It seems that there would be the need…
Tool/software:
Hello Team,
My customer has been using two devices below and currently requires more channels.
- LSF0102DQER (I2C Only)
- TXB0108YZPR
Requirement is as…
Tool/software:
Hi,
Greetings...
We are planning to use TXB0108 in our application.
We would like to know whether the unused pins in Port A & Port B can be left open. Kindly provide your comments on the same.
Also, we would like…
Tool/software:
1.TXB0108PWR level conversion chip, the device manual states that "external pull-up or pull-down resistors are not recommended. If it must be used, it is recommended that this value be greater than 50kΩ "(page P17…
Tool/software:
Hi Team,
Anyone can suggest an alternative for SN74LVC8T245 with auto-direction control feature.
Regards,
P. Sam Durai.
Tool/software:
Hi there,
We bought 2 SN74AXC8T245 Evaluation Modules, but unfortunately the channel 1 of the 8 channels does not work for both EVMs.
We…
FAQ: Logic and Voltage Translation > Auto-Bidirectional Level-Shifters >> Current FAQ
To mitigate oscillation concerns with devices with edge rate accelerators / one-shots such as TXB / TXS devices, consider below:
FAQ: Logic and Voltage Translation > Auto-Bidirectional Level-Shifters > Fixed DIR / DIR CNTRL Level-Shifters >> Current FAQ
Do not use auto-bidirectional level-shifters if the below is applicable. Use fixed or direction control level-shifters instead…