This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
Our product will use RTI watchdog triggering warm reset. First I tested the watchdog example in SDK 08.02.00.12, but I found warm reset doesn't work correctly.
I set syscfg as below, and called watchdog_reset_mode_main() from main(). I can see only "Prints will be stopped after reset " is repeated without stop in CCS console.
Could you clarify the reason why the SDK example is not working?
fyi, the interrupt mode example of the watchdog is working well.
Regards,
Moonil
Hi Moonil,
I am still working on it. Will get back to you soon.
Best regards,
Ming
Hi Moonil,
I juts found out the reset is not supported in this family of device. See the snapshot from TRM bellow:
Best regards,
Ming