[FAQ] AM625 / AM623 / AM620-Q1 / AM625-Q1 / AM625SIP / AM62A7 / AM62A3 / AM62A1-Q1 / AM62D-Q1 / AM62P / AM62P-Q1 / AM62L Custom board hardware design – Queries regarding Crystal selection and clock specifications

Other Parts Discussed in Thread: SK-AM62, SK-AM62-LP, AM62P, AM62D-Q1, AM62A3, AM62A7-Q1, AM62A3-Q1, AM62A7, AM62P-Q1, AM62L, AM620-Q1, AM625, AM623, AM625-Q1, AM625SIP, AM6442, AM3352, OMAP-L138

Hi TI Experts,

I have the below queries regarding the crystal selection.

1. Recommended crystal frequency for MCU_OSC0

2. Do you have recommended part numbers for Crystal? 

3. Can you help check if NX2016SA-25MHZ-EXS00A-CS10694, CRYSTAL 25.0000MHZ 8PF SMD could be used?

4. Do you have recommendations for MCU_OSC0 crystal selection.

5. Could you share the crystal part number used on the SK-AM62 and SK-AM62-LP?

6. Is it required to always connect the WKUP_LFOSC0?

7. Do you have recommendations for WKUP_LFOSC0 crystal selection.

8. Can i use an oscillator as the clock source?

9. Is there a real max value for crystal ESR?

10. Is there some guidelines for the crystal circuit layout?

11. Is there a delay requirement for the MCU_PORz after all the power supplies ramp and does the delay depend on the clock source

12.Recommended value for Rbias and Rd  R

13. MCU_OSC0_XI/MCU_OSC0_OUT starts before VDD_CORE voltage pull high, is this a concern

14. Does it have any side effect when MCU_OSC0_XI clock starts  before VDD_CORE voltage pull high?  What kind of conditions let MCU_OSC0_XI doesn't start until after VDD_CORE is applied?

 15. I would like to check the specifications of the 32kHz XTAL connected to the AM62P.

The following are the specifications of the 25MHz XTAL.

Isn't there a specification for the tolerance range drawn by the green line in the 32kHz XTAL?

Let me know your thoughts.

  • Hi Board designers, 

    The FAQ is generic and can also be used for

    AM62A7 / AM62A3 / AM62A7-Q1 / AM62A3-Q1 and AM62D-Q1 processor families.

    AM62P, AM62P-Q1 processor families

    AM62L processor families

    Refer below inputs for the queries related to the MCU_OSC0 crystal selection. 

    1.Recommended crystal frequency for MCU_OSC0

    Recommended Crystal Parallel Resonance Frequency for MCU_OSC0 Fxtal is 25 MHz

    2. Do you have recommended part numbers for Crystal? 

    Note that we do not provide part number recommendations.

    The system requirements of a customer’s product needs to be considered when selecting a crystal.  We do not know the operating conditions or frequency tolerance of all attached devices within their system.  The crystal requirements defined in our datasheet only address the processor requirements, but the crystal characteristics may also influence clocks that are sourced to attached devices which have their own requirements. In some cases, the attached devices may have frequency requirements that are tighter than the processor frequency requirements.

    3. Can you help check below specs and confirm this crystal specifications meets the requirements for the MCU_OSC0 Internal Oscillator Clock Source.

    The device expert and oscillator designer reviewed the crystal requirements and agree this crystal specifications meets the requirements for the HF oscillator implemented on our AM64x, AM62x, AM62Ax, AM62P, AM62P-Q1 Sitara processors.

    4. Do you have recommendations for MCU_OSC0 crystal selection.

    Refer below sections of the device datasheet.

    https://www.ti.com/lit/gpn/am625

    Figure 7-16. MCU_OSC0 Crystal Implementation
    The crystal must be in the fundamental mode of operation and parallel resonant.


    Table 7-19. MCU_OSC0 Crystal Circuit Requirements summarizes the required electrical constraints.

    5. Could you share the crystal part number used on the SK-AM62 and SK-AM62-LP?

    SK-AM62 and SK-AM62-LP

    XRCGB25M000F3M00R0

    25 MHz ±30ppm Crystal 6pF 150 Ohms 4-SMD, No Lead

    Do consider parasitic capacitance introduced by the PCB when determining the crystal load cap value.

    6. Is it required to always connect the WKUP_LFOSC0?

    Use of WKUP_LFOSC0 is application dependent.

    When WKUP_LFOSC0 is not used refer below section of the datasheet for oscillator connections 

    7.11.4.1.5 WKUP_LFOSC0 Not Used
    Figure 7-25. WKUP_LFOSC0 Not Used - 
    shows the recommended oscillator connections when WKUP_LFOSC0 is not used.

    7.  Do you have recommendations for WKUP_LFOSC0 crystal selection.

    Refer the below section of the device data sheet.

    7.11.4.1.2 MCU_OSC0 LVCMOS Digital Clock Source

    7.11.4.1.4 WKUP_LFOSC0 LVCMOS Digital Clock Source

    Note: Take care of the XO connection as per the data sheet recommendation.

    8. Can i use an oscillator as the clock source?

    Refer 7.11.4.1.2 MCU_OSC0 LVCMOS Digital Clock Source of the data sheet. Follow the recommended XO termination.

    7.11.4.1.4 WKUP_LFOSC0 LVCMOS Digital Clock Source

    9. Is there a real max value for crystal ESR?

    The maximum ESR recommended is 50 ohms regardless of shunt capacitance.

    10. Is there some guidelines for the crystal circuit layout?

    We currently have the below guidelines for the AM62A7.

    9.3 Clock Routing Guidelines
    9.3.1 Oscillator Routing

    The Same guidelines can be followed for the AM625 / AM623 / AM625SIP / AM625-Q1 / AM620-Q1

    The guidelines will be updated in the next data sheet revision for AM625 / AM623 / AM625SIP / AM625-Q1 / AM620-Q1

    11. Is there a delay requirement for the MCU_PORz after all the power supplies ramp and does the delay depend on the clock source

    Refer to MCU_PORz Timing Requirements in the device-specific data sheet

    RST1 Hold time, MCU_PORz active (low) at Power-up after supplies valid (using external crystal circuit) is 9500000 ns
    RST2 Hold time, MCU_PORz active (low) at Power-up after supplies valid and external clock stable (using external LVCMOS clock source) 1200 ns. (This does not include the external oscillator start-up time)

    12. Recommended value for Rbias and Rd

    WKUP_LFOSC0 Internal Oscillator Clock Source

    WKUP_LFOSC0 Crystal Implementation figure shows the recommended crystal circuit. It is recommended that preproduction printed-circuit board
    (PCB) designs include the two optional resistors Rbias (500k to 2M ohm) and Rd (0 ohm) in case they are required for proper oscillator operation when combined with production crystal circuit components. In most cases, Rbias is not required and Rd is a 0-Ω resistor. These resistors may be removed from production PCB designs after evaluating oscillator performance with production crystal circuit components installed on preproduction PCBs.

    Note: TI does not expect customers to install a Rbias resistor or use any value other than 0 ohms for Rd without contacting TI to discuss any issue they may have with the oscillator.  

    13. MCU_OSC0_XI/MCU_OSC0_OUT starts before VDD_CORE voltage ramps up, is this a concern

    The oscillator is working as expected. It most cases the oscillation will start shortly after its 1.8V power rail is applied, but there may be conditions where it doesn't start until after VDD_CORE is applied.

    14. Does it have any side effect when MCU_OSC0_XI clock starts  before VDD_CORE voltage ramps up?  What kind of conditions let MCU_OSC0_XI doesn't start until after VDD_CORE is applied?

    No side effects.

    The oscillator has registers in the VDD_CORE power domain that controls some of its operating functions. It is very unlikely the start-up will be delayed until VDD_CORE is valid, but we are being conservative by saying the oscillation will not begin until VDD_CORE is valid to ensure the product designer provides adequate time for the oscillator to start before reset is released.

    (+) [FAQ] AM6442: question about MCU_OSC0 Start-up - Processors forum - Processors - TI E2E support forums

    [FAQ] AM6442: question about MCU_OSC0 Start-up

    I have a question about "Figure 7-16. MCU_OSC0 Start-up Time" from the datasheet. Here it looks like that MCU_OSC0 is only allowed to start when VDD_MCU is ramping. In reality the osciallation starts already with VDDS_OSC0, while VDD_MCU is still disabled. 

    I assume that this is OK and not causing any problems?! But if this is the case, why is the Start-up Time ts shown relatative to VDD_MCU stable? Shouldn't it be related to VDDS_OSC0 stable?

     

    The oscillator is powered from VDDS_OSC0. So it may power-up and begin oscillation as soon as VDDS_OSC0 is applied. However, the oscillator has a few control registers which are powered by the VDD_CORE domain. So there is a chance the oscillator may not start until the VDD_CORE is valid. 

    The supply shown in the upper waveform should be named VDD_CORE rather than VDD_MCU. AM64x does not even have a power rail named VDD_MCU. Therefore, I need to get this figure updated in the datasheet. Thanks for asking the question, which highlighted the error in the figure. 

    15. I would like to check the specifications of the 32kHz XTAL.

    The following are the specifications of the 25MHz XTAL.

    The following are the specifications of the 32KHz XTAL

    Isn't there a specification for the tolerance range drawn by the green line in the 32kHz XTAL?

    The accuracy of this clock source is primarily a function of your system requirements.

    We plan to define a max limit of +/-100PPM for the AM62Px device. However, your specific application may require a more accurate source.

    Regards,

    Sreenivasa

  • Hi TI Experts,

    I have the below additional queries regarding the crystal selection.

    16. It is assumed that when a crystal connected externally has a large change in frequency due to some factor, there will be an effect on the PLL.

    I would like to know the effect on the PLL when the frequency changes and how each function will operate. The factors that may cause the frequency to change include initial failure, environment, and manufacturing defects.

    17. Does the 25MHz and 32kHz XTAL have an oscillation margin switching function and is there need to configure registers.

    18. Do you have some recommendations on the crystal load and load capacitance matching

    Let me know your thoughts.

  • Hi Board designers, 

    Refer below inputs for the queries related to the MCU_OSC0 crystal selection. 

    16. It is assumed that when a crystal connected externally has a large change in frequency due to some factor, there will be an effect on the PLL.

    I would like to know the effect on the PLL when the frequency changes and how each function will operate. The factors that may cause the frequency to change include initial failure, environment, and manufacturing defects.

    Ans: It is not possible for crystals to have a large change in frequency. They have a very high-Q impedance response. The impedance drops dramatically with a very small shift in frequency, which would cause the gain in the oscillator feedback path to drop such that it is not possible to maintain oscillation. So, they are either oscillating at their designed frequency are not oscillating.

    17. Does the 25MHz and 32kHz XTAL have an oscillation margin switching function and is there need to configure registers.

    No HFOSC0 registers are required to be changed. These registers should remain in their default state.
    Select the appropriate crystal circuit components that are compliant to the values defined in the MCU_OSC0 Crystal Circuit Requirements table.
    Read the Load Capacitance and Shunt Capacitance sections to select the appropriate crystal circuit components.


    The only LFOSC0 register bits that should be changed by the customer are BP_C, PD_C, and CTRLMMR_WKUP_LFXOSC_TRIM[18:16],
    where PD_C is reset (0) to enable the oscillator and the BP_C bit is only set (1) to place the oscillator in bypass mode when
    using an LVCMOS clock source. The CTRLMMR_WKUP_LFXOSC_TRIM[18:16] bits are set based on the actual capacitance load applied to the crystal,
    as defined by the Load Capacitance Equation. The load capacitance range of the crystal will be half of the recommended capacitor value range
    since there are connected in series with the crystals resonate circuit.

    18. Do you have some recommendations on the crystal load and load capacitance matching 

    It is recommended to match the crystal load and the load capacitance as per the data sheet recommendations. Any difference in the crystal load and the load cap capacitance selected could result in PPM variation of the clock frequency Choose crystal load as per the standard capacitance availability to ensure matching of the capacitance.

    References

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1115457/am6411-is-it-needed-to-input-the-synchronized-clock-between-am64x-and-ethernet-phy

    Regards,

    Sreenivasa

  • Hi Board designers, 


    Refer below inputs for AM62A3-Q1: Oscillator Clock Loss Detection. This should be same for all the AM62x devices. 

    If MCU_PLL_CLKSEL_CLKLOSS_SWTCH_EN is set, when HFOSC0 stops, will it automatically switch to CLK_12M_RC and output to the MCU_ERRORn pin at the same time?
    [TI] >> Yes.


    Which register can be used to determine that it has been automatically switched to CLK_12M_RC?
    [TI] >> You can read ESM event register WKUP_ESM0_ESM_LVL_EVENT_IN_13


    Does the oscillator return to HFOSC0 when a warm reset?
    [TI] >> I am not sure if I understand this question. When HFOSC0 starts switching again the reference clock will be automatically switched to HFOSC0 clock.


    Will it switch to CLK_12M_RC even if HFOSC0 is not oscillating at cold start?
    [TI] >> By default MCU_PLL_CLKSEL_CLKLOSS_SWTCH_EN is set to ‘0’. So at cold start, if HFOSC0 is not switching then the mux will not switch to CLK_12M_RC. If HFOSC0 is not switching during cold start, the device will not boot-up.

    Accuracy of the MCU_RC_OSC_12M

    https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1431627/am2431-accuracy-of-the-mcu_rc_osc_12m

    (+) [FAQ] AM6422: How to Switch Back to External Clock After Clock Loss Detection - Processors forum - Processors - TI E2E support forums

    We tried the power cycle of AM64x and observe 2 cases:
    1. Ocsilator Disabled: AM64x doesn't boot up.
    2. Ocsilator Enabled: AM64x runs on 25MHz clock.

    We modified the config to enable clock loss detection as mentioned in above post. Then we did the warm reset of AM64x and observe the following scenarios: 
    1. Ocsilator Disabled. Clock losss detected and after watchdog reset / warm rest AM64x runs on 12.5 MHz.
    2. Ocsilator Enabled: AM64x continued running on 12.5MHz not switched to 25MHz.

    We monitored MCU_SAFETY_ERRORn pin, during clock loss detection pin status changed from HIGH->LOW. However, there is no transition detected when 25MHz clock available again.

    I added the inputs from out reset expert:

    The expectation is that the fault is routed to the ESM, and some external circuit would generate a power cycle or cold reset so the system can recover.  I think this is the only way the clock loss detection circuit would reset the detection.  Also, MCU_PORz is the only way CLKLOSS_SWITCH_EN bit gets reset.  So a warm reset will not help here, and that is why they observe the 12MHz_RC still clocking the processor after a warm reset

     

    The RC clock backup is not available immediately after PORz because of the default value of CLKLOSS_SWITCH_EN.  There is some setup that needs to happen anyway, in that the error needs to be routed to the ESM to trigger the ERROR signal, so that an external can do something about it (power cycle the device, for example).  When all that is setup, the RC clock will clock the device after a fault, but it is only intended to keep the ESM alive to generate the appropriate ERROR signal.  It is not expected that the device will operate fully.

     

    On a cold reset, if the 25MHz is not available, the device will not boot.  Even if the clock loss detection circuitry works at that point, the CLKLOSS_SWITCH_EN defaults to 0 as mentioned previously, so the mux will never switch to the RC clock.  Even if it would be able to switch, the ROM does not support booting with that input frequency.

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Query regarding Spread Spectrum input:

    Does MCU_OSC(25MHz) support spread spectrum clock oscillators?

    Please refer to the device specific data sheet for the crystal requirement or for using external LVCMOS clock input.

    SS clock input is not supported.

    (+) AM625: external and internal spread spectrum oscillator support - Processors forum - Processors - TI E2E support forums

    1. Do AM62x processors support external clock generator or do they support ONLY crystal oscillator?

    2. If external clock generator is supported, does it support SS oscillator also? I have a problem with USB Device mode communication when I use SiT9005AC-13-18NH25.000000 as oscillator. Other peripherals like LPDDR4, SD card interface and eMMC flash work in general.

    3.  Based on this link (https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1358154/am625-pll-spread-spectrum-modulation), internal SS feature is not supported in AM62x devices. Is it still correct or is it supported now?

    1) Yes. You can use a 1.8V LVCMOS clock source rather than a crystal circuit. However, the current datasheet does not define the MCU_OSC0 LVCMOS Digital Clock Source Requirements. We will be adding these requirements to the next revision of the datasheet. For now, please refer to the "MCU_OSC0 LVCMOS Digital Clock Source" section of the AM62Dx or AM62Px datasheets. The requirements for AM62x will be the same.

    2) An external 1.8V LVCMOS source is supported, but not a Spread Spectrum source. As mentioned above, please follow the requirements defined in the "MCU_OSC0 LVCMOS Digital Clock Source" section of the AM62Dx or AM62Px datasheets.

    3) That is correct. SSC is not currently supported on AM62x. We may support SSC on the PLL that sources the DSS peripheral in the future, but there are no plans to support SSC for any other PLLs.

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Additional references for crystal selection

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1038770/am3358-frequency-tolerance-and-frequency-stability-of-24mhz-crystal/3841749

    The accuracy of the AM335x reference clock source should be based on system level requirements. For example, you may need a 30 PPM reference clock if an AM335x timer is being used to operate something that needs this level of accuracy. 

    The 50 PPM limit was defined for AM335x because the RMII Ethernet standard requires this accuracy. The other Ethernet standards only require 100 PPM, so you may be able to back-off on this 50 PPM requirement if not using RMII. However, this depends if you have other system function that require an accuracy of 50 PPM. I would not recommend going above 100 PPM as this may begin to effect other peripheral interfaces.

    Keep in mind, a crystal has three contributions to accuracy. There is a parameter that defines initial accuracy, another parameter that defines accuracy over operating temperature, and aging parameter that defines how much the resonate frequency changes over time due to aging effects. When selecting a crystal, you must combine all of these to determine frequency accuracy across all operating conditions for the life of the product.

    Reliable start-up is also a concern with crystal selection. The max ESR of the crystal is one of the primary concerns. The AM335x oscillator may not have enough gain to reliably start oscillation if the crystal ESR is too low. Many crystal datasheets define a worst case max ESR value for the entire family of crystals rather than a specific max ESR for the crystal being selected. In most cases the higher frequency crystals in the family will have a much lower max ESR value that what is found in the datasheet. Therefore, you may need to contact the crystal manufacture and request a device specific datasheet for the crystal part number you plan to use.

    One way to confirm you have start-up margin, is by inserting a resistor in series with the selected crystal and checking for reliable start-up across all operating conditions. I suggest you begin with a resistor value that is about 5x the max ESR of the crystal. If you have start-up issues with this value you can reduce it to 3x. There is not enough gain margin if oscillation will not reliably start with a 3x resistor. You would need to select a crystal with lower ESR if you find it will not reliably start with a 3X series resistor.

    You neve said if you were using RMII and needed 50 PPM system performance. Therefore, I cannot comment how were these options align with your system requirements.

    I noticed the Digi-key description for your existing crystal, which they are selling under part number 7A-24.000MAAJ-T was cut for an 18pF load, so it must not be one of the standard options shown in the datasheet. What load did you apply to this crystal in your product? Are you willing to change load capacitor values in your product when you change crystals? How much capacitive load does you signals apply to the crystal circuit?

    I do not think a crystal cut for 18pF load was ever appropriate for AM335x. Each load capacitor would need to be approximately 33 - 36 pF to achieve a 18pF load for the crystal and the AM335x datasheet only allows load capacitors in the range of 12 - 24 pF. 

    The highest load capacitance crystal you would be able to use is 12pF to remain in the ranged defined by the AM335x datasheet.

    The AA-24.000MAHJ-T datasheet shows their standard offering is a crystal cut for a 8pF load. However, they provide an option to specify a load capacitance. I did not see an aging parameter in this datasheet, so not sure how PPM will change over time on this crystal.  It may be a viable option as long as you apply the correct load capacitance for the crystal your purchase while remaining compliant with AM335x datasheet. However, you should validate startup reliability using the method described previously to ensure ESR in not going to be a problem.

    The ECS-240-18-30-JGN-TR datasheet does not clearly show an option for buying a crystal cut for a lower capacitive load and 20 pF is too high. You may be able to use this as a viable option if they would sell you one that was cut for 10 pF.

    AM3352: Crystal OSC0 - Parameters - ESR and Behaviors

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/998892/am3352-crystal-osc0---parameters---esr-and-behaviors/3690471

    The biggest concern is not having enough gain margin to reliably start oscillation when the higher ESR crystal is combined with the other crystal circuit components and internal oscillator.

    There is a good chance you have enough gain margin if this combination of components has been used for a while without receiving any reports of the oscillator not starting.

    In most cases the actual ESR of a crystal is much smaller than the published value. This is especially true when the ESR value you are using is taken from a data sheet that covers an entire family of crystals. The max ESR value published in a crystal family data sheet is typically inflated to cover the entire range of crystals. You may be able to reach out to the crystal manufacture and request a part number specific datasheet to confirm the max ESR of your crystal.

    You can test the gain margin by placing a resistor in series with the crystal, which increases the ESR seen my the entire circuit. We typically recommend confirming reliable start of oscillation across operating conditions when the series resistor inserted increases the ESR to at least 3x the expected ESR of the crystal. 

    Load capacitor values should be selected based on the load expected by the crystal. Crystal are cut to oscillate at the specified frequency with a specific capacitive load. The frequency of oscillation will be pulled a few PPM from the specified frequency if the load you apply is not correct. Most crystal manufactures provide a service where they evaluate your product with their crystal and make recommendations if your initial component selection is not optimum. I think the fee they charge is reasonable for any high volume product where you want to be confident that you clock solution is robust.

    Regards,

    Sreenivasa

  • Hi Board designers, 

    AM62A3-Q1: HW : crystal failure


    It is assumed that when a crystal connected externally has a large change in frequency due to some factor, there will be an effect on the PLL.

    I would like to know the effect on the PLL when the frequency changes and how each function will operate.

    The factors that may cause the frequency to change include initial failure, environment, and manufacturing defects.

    It is not possible for crystals to have a large change in frequency. They have a very high-Q impedance response. The impedance drops dramatically with a very small shift in frequency, which would cause the gain in the oscillator feedback path to drop such that it is not possible to maintain oscillation. So, they are either oscillating at their designed frequency are not oscillating.

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Refer below FAQ for information related to Oscillator specifications being added to all the processor family data sheets and use of BAQ oscillator:

    (+) CDC6C: BAW oscillator use for AM6442 - Clock & timing forum - Clock & timing - TI E2E support forums

    LMK6CE02500DDLFT

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Information related to clock source (oscillator) placed on carrier board:

    Q. The oscillator is placed on the carrier board and the clock is connected through a connector to the processor.
    My question was on the clock length and related concerns.
    Checking if there are any concern or care-abouts for customer to take care while placing the oscillator on the carrier board or should customer place the oscillator on the processor board and is there a recommendation or requirement to place oscillator close to processor like the crystal.

    A.

    The digital output of the LVCMOS clock source with fast rise/fall times will be more tolerant to noise than the near sinusoid signal that is produced by the crystal circuit, so placing it near the processor is not as important as the crystal circuit. They need to follow the recommendations in the following notes and confirm the Rise/Fall Time (10%-90% rise, 90%-10% fall) is less than 4ns at the MCU_OSC0_XI pin.
    Note
    1. A DC steady-state condition is not allowed on MCU_OSC0_XI when the oscillator is powered up. This is not allowed because MCU_OSC0_XI is internally AC coupled to a comparator that can enter an unknown state when DC is applied to the input. Therefore, application software must power down MCU_OSC0 any time MCU_OSC0_XI is not toggling between logic states. 2. The LVCMOS clock signal sourcing the MCU_OSC0_XI input must have monotonic transitions.
    The clock source should be connected to MCU_OSC0_XI with a point-to-point connection, via a series termination resistor placed near the clock source. The series termination resistor value should match the clock source output impedance to the transmission line impedance. For example, the series termination resistor value needs to be 20 ohms if the clock source has an output impedance of 30 ohms and the PCB signal trace has a characteristic impedance of 50 ohms. This allows the reflection that returns from the far end of the un-terminated transmission line to be completely absorbed such that is does not introduce any non-monotonic events on the signal.
    3. The PCB trace length connecting the LVCMOS clock source to MCU_OSC0_XI should be minimized. This reduces capacitive loading and decreases probability of external noise sources coupling into the clock signal. Reduced capacitive loading improves rise/fall times of the clock signal which reduces the probability of jitter being introduced in the system.

    My biggest concern is related to ground noise introduced by the two PCB implementation. Any ground noise (high frequency potential difference between the grounds of each PCB) will appears as noise on any signal that is sourced from a device on the carrier PCB to our device on the processor PCB. They need to have a lot of ground pins on the connectors that connect the two PCBs. I would say at least one ground for every two or three signals that transition from one board to the other.

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Queries related to SOC start-up with crystal not operating

    Will it switch to CLK_12M_RC even if HFOSC0 is not oscillating at cold start?
    [TI] >> By default MCU_PLL_CLKSEL_CLKLOSS_SWTCH_EN is set to ‘0’. So at cold start, if HFOSC0 is not switching then the mux will not switch to CLK_12M_RC. If HFOSC0 is not switching during cold start, the device will not boot-up.

    Did you have a chance to power cycle the board and see the behavior with the oscillator disabled.

    5.4.4 Device Oscillators
    The device has the possibility to source clocks of an external high-frequency oscillator - MCU_HFOSC0. The
    device has also one internal RC oscillator - MCU_RC_OSC_12M.

    Oscillator Clock Loss Detection

    Observation clocks

    One more observation we had capture, we monitored the OBSCLK0 output using an oscilloscope. We mapped the OBSCLK0 pin to output MCU_HFOSC0_CLKOUT:

    • When the 25 MHz external clock is active, we observe 25 MHz on the oscilloscope.
    • After the fallback, the output changes to 12.5 MHz.
    • However, when the external 25 MHz clock is re-enabled, the oscilloscope again shows 25 MHz, but the processor continues to run on the internal 12.5 MHz clock.

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Inputs related to IBIS model for Xi

    NC is the expected connection for the AM64x, AM62x, AM62Ax, AM62Px and AM62L family of processors. This is the crystal or oscillator input. We do not provide any IBIS models for the clocking section IP of the processor.

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/752136/tms320c6746-ibis-model-for-l19-oscin-pin/2782761

    I checked a couple of other IBIS files available on TI.com, and they also do not provide model data for the oscillator inputs (even if used as an clock input from some LVCMOS oscillator source instead of a crystal).

    I suspect the reason is because these clock/crystal inputs are analog in nature, but I will follow up with our IBIS expert. IBIS files are meant for IO buffers.

    This NC for OSCIN/CLKIN pins is consistent with other devices.

    https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/274626/f2812-pgf-ibis-model-clk-is-nc-signals

    We checked with our Design team on this and got the following reply:

    "We do not provide IBIS models for power/ground/Oscillator pins.  Usually SI simulations are significant for drivers.  X1 being a receiver may be modeled as a simple cap".  

    Just to clarify further, SI simulations are significant primarily for drivers. i.e. Signal integrity simulations are useful only for I/O pins and not for input-only, clocking pins like X1.  

    OMAP-L138: OSCIN (pin L19) missing in IBIS model?

    OSCIN input (pin L19) is missing in OMAP-L138 IBIS model. Do we have updated IBIS file?
     
    Or is OSCIN not required for IBIS? Having said this should customer try to find an option on his compilation tools to ignore these pins…

    Generally speaking, OSC inputs are not simulated, especially if an actual crystal is used.  IBIS does not simulate analog inputs.

    Regards,

    Sreenivasa