Other Parts Discussed in Thread: TMCS1133, LAUNCHXL-F28P65X, TMCS1123, AMC3302, ADS127L18
Tool/software:
Hi!
I design 600VDC EV HVAC driver for 3phase sensorless motor 30A/phase max.
We try to create some evaluation design, and…
Tool/software:
Hi!
I design 600VDC EV HVAC driver for 3phase sensorless motor 30A/phase max.
We try to create some evaluation design, and…
Tool/software:
Hi
I want to know TMCS1126-Q1 lifetime (available period)
I looked up the data sheet, but I couldn't find an answer
I want to check all the temperature conditions…
Tool/software:
hello.
I am writing to ask a question about current sensing.
As shown in the current photo, I increased the input dc voltage to 500v.
I can see that the B-phase current…
Tool/software:
Hi Sir:
Can we use the TMCS1123 part to design it to sense voltages from 6900 to 11400V(AC)?
BR
SH
Tool/software:
Hello experts,
I got a few questions from a customer regarding TMCS1123 maximum current.
1.The Ambient Temperature in Figure 7-4 excludes self-heating effect, that is, the ambient temperature is case temerature without…
Tool/software:
Hi Team,
Based on Pre-compliance testing consideration - could you please check that listed parts are compliance for the USA, Canada, Mexico market?
P/N: TMCS1123A1AQDVGR
Also please share UL certificate and its details…
Tool/software:
What is the best hall-effect current sensor for measuring DC current, ranging from 1A to 85A with Vs=3.3V. Thank you
Tool/software:
Hi,
Customer wants to know our accuracy in low current application.
For 500mA input current, Could TMCS112X support error less than 3%?
Thank you,
Yishan Chen
Tool/software:
Can I get the step file for 3D model for this part TMCS1123C1AQDVGR.
Thanks.
Tool/software:
Hi team,
In D/S, TMCS1123 and 1126 is planning to get IEC62368 certification.
How about IEC60950?
Best regards,
Goto
Tool/software:
Hi
i need the maximum current supply details. that i can apply for the Vs pin for this TMCS1123C1AQDVGR current sensor.
Hello Team,
We are planning to use the current sensor TMCS1108 in one of our products to measure the DC current flowing to a motor.
The maximum current to…
Other than voltage isolation, are there any issues with routing copper planes carrying current beneath the TMCS1123 part? We are looking at expanding the copper flood beneath the part (connected to IN+/IN-) to reduce voltage loss…