産業用機器のコントローラを設計している人なら、おそらく次のような課題に頭を悩ませたことがあるでしょう。
- 「どのレベルの電圧が必要だろうか?」
- 「電流レベルに注意しているか?」
- 「コントローラの動作に必要な周波数は?」
- 「このデバイスには高温や磁気に対する耐性が必要になるだろうか?」
中にはより問題になりそうなものとそうでもないものがあり、設計するものがストリング・インバータ、モーター・ドライブ、Eメーターかでも重要性が変わります…
産業用機器のコントローラを設計している人なら、おそらく次のような課題に頭を悩ませたことがあるでしょう。
中にはより問題になりそうなものとそうでもないものがあり、設計するものがストリング・インバータ、モーター・ドライブ、Eメーターかでも重要性が変わります…
Medical ultrasound is a noninvasive method of imaging the body’s internal structures (like organs) by transmitting high-frequency waves and measuring the reflections that occur at various boundaries within, such…
As battery-powered systems become more common, quickly identifying a failing battery so that it can be replaced is becoming increasingly important. From an individual battery powering a mobile phone to a bank of…
In this post, I’ll show how to design a cost-optimized, discrete, wide-bandwidth instrumentation amplifier using the TLV3544. Instrumentation amplifiers are used for their high input impedance and ability to…
The digital multimeter (DMM) is a centerpiece in any electronics lab, but as the precision of electronics continues to increase, so does the need for DMMs that can quickly and accurately measure current, voltage…
In my previous post, I discussed the proper way to layout a printed circuit board (PCB) for an operational amplifier (op amp) and provided a list of good layout practices to follow. In this post, I will discuss common mistakes when laying out a PCB for…
This technical article was updated on July 23, 2020.
High-precision data-acquisition systems are designed to minimize errors from various system components, like those introduced by switching transients on the reference input of a data converter. In the…
伝送媒体を通して流れる信号は、ノイズ、歪み、および信号損失の影響を受けます。通常、低いビット・レートではシグナル・インテグリティ(完全性)やフィデリティ(忠実度)を保つことができ、長距離の伝送が可能ですが、DisplayPortやHDMI®(高精細度マルチメディア・インターフェイス)を介した何ギガビット/秒もの高速信号の場合、信号がコネクタを結ぶ長い配線や長いケーブルを流れる際に、通常はシグナル・インテグリティが大きく低下します。このような長い配線により、受信端で信号強度が下がり、歪みまたはノイズの多い信号になったり…
In my last post, I talked about the different types of digital filters commonly used in delta-sigma analog-to-digital converters (ADCs). In this post, let’s focus on the most common type of digital filter used in…
The world is a hazardous place, and electronic systems are just as susceptible to mechanical failures as they are to unseen electromagnetic radiation. Let’s take a look at how to protect circuit designs…
In my last post, I discussed two important characteristics of delta-sigma analog-to-digital converters (ADCs) that simplify the design of your anti-aliasing filter: an oversampling architecture and a supplemental digital decimation filter. The oversampling…
President Ronald Reagan frequently said “trust but verify” when discussing U.S. relations with the Soviet Union. Some say it comes from a Russian proverb, “doveryai no proveryai.”
Trust but…