Browse By Tags

  • AM62P-Q1: mipi csi data verification

    Part Number: AM62P-Q1
    Other Parts Discussed in Thread: AM62P

    Tool/software:

    At present, we adapt the radar ads6311, and find that the probability of pcm gray image will appear light spots at 600FPS frame rate, and the probability of problems at 200FPS…

  • IWRL6432: IWRL6432AOP product page is missing

    Part Number: IWRL6432

    Tool/software:

    Hi,

    We were thinking about using IWRL6432AOP part for a new project, but we've found that the product page is missing.

    Is this part going to be available anymore?

    Regards,

    Miguel Lopez

  • FDC2214EVM: Sensor design and optimization

    Part Number: FDC2214EVM
    Other Parts Discussed in Thread: FDC2214, FDC1004EVM, LDC1612EVM, FDC1004, LDC1312, FDC2112, FDC2212, LDC1612

    Tool/software:

    Hi everyone,
    I'm currently working with the FDC2214EVM – High Resolution L-C Sensing Evaluation …

  • PROCESSOR-SDK-AM62A: Issues with integrating the IMX 327 sensor

    Part Number: PROCESSOR-SDK-AM62A

    Tool/software:

    Hello,

    We are encountering issues with integrating the IMX 327 sensor with the TI SK-AM62A. We attempted to compile a new overlay using the repository at https://github.com/TexasInstruments/linux-kerne…

  • TMP75: I2c interfacing issue using NXP S32k3xx MBDT.

    Part Number: TMP75

    Tool/software:

    Hello,

    I am trying to interface TMP75 temperature sensor.

    I am using NXP S32k312 mcu using Model Based Design toolbox.

    From your forum,I saw following should be the waveform for continuous conversion

    But I am getting…

  • J784S4XEVM: Leopard AR0820 not working with Fusion Board 2

    Part Number: J784S4XEVM

    Tool/software:

    Hi TI,

    This ticket is in continuation with the linked ticket. I was not able to reply on that so I am raising this one.

    Env: QNX + SDK Version: 9_2_0_5

    Issue: The leopard AR0280 is not working with Fusion Board2…

  • HDC3022: Is the response of temperature reading of this sensor as fast as the response to humidity even with the PTFE hood?

    Part Number: HDC3022
    Other Parts Discussed in Thread: TMP117,

    Tool/software:

    in this discussion two years ago, there is some data that shows that the response time of the humidity reading in this sensor with the PTFE hood is only slightly slower than that…

  • HDC3022: DEJR

    Part Number: HDC3022

    Tool/software:

    Dear Texas Instrument Team,

    I'd like to ask you whether the p/n HDC3022DEJR complies with the California 65 preposition.

    Thanks in advance for the support.

  • [FAQ] SK-AM69: How to stream from CSI sensor and USB camera to display using GStreamer?

    Part Number: SK-AM69
    Other Parts Discussed in Thread: SK-AM68, AM67, SK-TDA4VM

    Tool/software:

    Hi,

    I have a Starter Kit (SK) Edge AI device with a CSI sensor connected and would like to stream to my display. I have enabled the sensor by following the…

  • LMP91000: I am having issue while configuring O2 3 lead sensor with LMP91000

    Part Number: LMP91000

    Tool/software:

    I am using LM91000EVM board and using O2 lead-free sensor which has -600mV bias and 100uA output at ambient air. Issue is that my bias is not being set and even after keeping it for an 2-3 Hour it does not respond…

  • LDC5071-Q1: What constitutes a "good" sensor design using the LDC5072 Sensor Designer tool?

    Part Number: LDC5071-Q1

    Tool/software:

    Hello, 

    I am hoping to use the LDC5071-Q1 with a custom linear inductive sensor to give me absolute position of a linear slide. 

    I have been playing around with the LDC5072 Sensor Designer Tool and looking at the generated…

  • TMP1826: Detailed Calibration Information

    Part Number: TMP1826

    Tool/software:

    I'm designing a new product using the TMP1826NGRR and have some questions about the NIST and Calibration process. Some of our clients require more information about the calibration of our devices.

    It sounds like…

  • AFE4960P: The driver sample code about AFE4960P

    Part Number: AFE4960P

    Tool/software:

    Hello,
    This is Emma from a Chinese JiangSu province wearable device company.

    Ourl company is developing an smart watch which is able to test users' ECG, and we chose to use the sensor AFE4960P.
    NOW in the driver…

  • TMAG6180-Q1: Off axis sin cos encoder

    Part Number: TMAG6180-Q1
    Other Parts Discussed in Thread: TMAG6180, TMAG5170-Q1, TMAG5253, TMAG5170, DRV5055, LDC5072-Q1

    Tool/software:

    Hello Team,

        we want to develop sin cos off axis encoder. your chip TMAG6180-Q1 suits to our application ,it matches…

  • MSP430FR2673: Send message via NFC with MSP430 and NFC IC

    Part Number: MSP430FR2673

    Tool/software:

    I want to send a message via NFC to a smartphone like "Hello world". I have MSP430FR2673 microcontroller and NT3H2111 NFC IC. In the next stage, I will try to transfer data obtained from a sensor via NFC. I'm…

  • LP-EM-CC1314R10: Using Frequency hopping mode in multiple sensor (sleepy devices) network.

    Part Number: LP-EM-CC1314R10

    Tool/software:

    Want to know how the the collector or sensors is hopping the channels and how much time it will stay in that channel especially if we use multiple sleepy sensor in a network.


    From the user guide I have listed…

  • MSP430FR5969: MSP430FR5969

    Part Number: MSP430FR5969

    Tool/software:

    Hello, we are interfacing the MSP430FR5969 with air quality sensors such as SGP30 and SEN55 via I2C Communication. Unfortunately, we have not been able to successfully read and write data to the registers of the…

  • TMAG6180-Q1: Support

    Part Number: TMAG6180-Q1
    Other Parts Discussed in Thread: TMAG6180

    Tool/software:

    Hi, 

    We have below requirement to read the position of control surfaces in aircraft which has possible deflection angle of +/-179 Deg. Can we use TMAG6180-Q1 for below application…

  • LP-EM-CC1314R10: orphan Sensor rejoin issue - orphan scan not triggered.

    Part Number: LP-EM-CC1314R10
    Other Parts Discussed in Thread: SYSCONFIG, CC1352P

    Tool/software:

    Hi, 

    We are using the TI-stack 15.4 sensor-collector example. We have issues with the orphaned sensor rejoining the network.

    As per the user guide, when the…

  • CC2650STK: More information about how to read the sensor data without using SimpleLink Ti App

    Part Number: CC2650STK
    Other Parts Discussed in Thread: BLE-STACK

    Tool/software:

    Hi,

    I am trying to read the sensor data using "python script and using Bleak library".

    Here is the link:

    https://github.com/hbldh/bleak

     

    For now I am interested…

  • TDA4VEN-Q1: How TDA4VEN distinguishes between different data types in vision_app.

    Part Number: TDA4VEN-Q1

    Tool/software:

    Hi ti,

    OS: Linux+RTOS(J722S)

    PSDK : ti-processor-sdk-rtos-j722s-evm-09_02_00_05

    Ser/Deserializer : max9295A/max96722B

    We have the demand for a sensor to output two kinds of data. The specific processing process is…

  • TDA4VEN-Q1: TDA4VEN An error occurs when executing run_app_multi_cam.sh

    Part Number: TDA4VEN-Q1

    Tool/software:

    Hi ti,

    OS: Linux+RTOS(J722S)

    PSDK : ti-processor-sdk-rtos-j722s-evm-09_02_00_05

    Ser/Deserializer : max96717F/max96722B

    After I successfully executed run_app_single_cam.sh, I tried to use run_app_multi_cam.sh to light…

  • MSP430FR2633: Entering determined Values via Software Side

    Part Number: MSP430FR2633

    Tool/software:

    Hello Everyone,

    i am currently working on a project to simulate the Captivate Microcontroller. Is there any known way to insert values for the microcontroller via Software and not via Sensors ?

    Thanks for your…

  • TDA4VEN-Q1: TDA4 had AE failure when adapting OX03F.

    Part Number: TDA4VEN-Q1

    Tool/software:

    Hi ti,

    OS: Linux+RTOS(J722S)

    PSDK : ti-processor-sdk-rtos-j722s-evm-09_02_00_05

    Ser/Deserializer : max96717F/max96722B

    During the adaptation process, I was able to capture the correct raw and yuv images using vision_app…

  • HDC3021: HDC3021: Offset Error Correction

    Part Number: HDC3021

    Tool/software:

    Hi there, 

    I refer to my original question here (I accidently hit resolve on that thread - however my question still remains and my problem is not resolved). 

    I refer to your technical document for the HDC3021 EVM, where…

1 2 3 4 5 »