Part Number: MCU-PLUS-SDK-AM243X Other Parts Discussed in Thread: DP83869
Tool/software:
Hi,
Can you help me with how to enable PRU Ethernet on the ICSSG0 instance on AM64x/AM243x?
Regards
Ashwani
Part Number: DS250DF230 Other Parts Discussed in Thread: DS250DF210 , DS250DF410 , DS250DF810 , , DS280DF810
Tool/software:
Across all 25-28G retimers (DS250DF210, DS250DF230, DS250DF410, DS250DF810, DS280DF810) there are 255 total CTLE boost settings. A…
Part Number: C2000WARE
Tool/software:
Situation example:
The CMPSS's compared voltage is set as 1.5V from internal DAC / external signal, once the sensed voltage on positive pin is higher than negative pin 1.5V, then trigger ONCE interrupt. Then…
Tool/software:
In the ADS129x family, a 4-bit DAC is used to set the lead-off detection threshold for the positive and negative channels inputs. The DAC settings are configured writing to COMP_TH[2:0] in the LOFF control register. The threshold voltages…
Part Number: TPS628502
Tool/software:
Hi Experts,
My customer is using TPS6285020MQDRLRQ1 to generate 1.8V fixed output from 3.3V input.
Help me understand how to connect the feedback - should this be left open.
Customer has connected the output to the…
Part Number: AM625 Other Parts Discussed in Thread: AM623 , AM6546 , AM6442 , AM2432 , TDA4VH-Q1 , TDA4VH
Tool/software:
HI TI experts,
I have queries related to the voltage monitoring capability of the SOC POK module types, accuracy., design recommendations…