Other Parts Discussed in Thread: TPS25751
Tool/software:
Hello everyone,
We're currently working on our engineering thesis project involving the TPS25751 and BQ25756 components. Project is a smart battery charger with bidirectional…
Tool/software:
Hello and thank you in advance!
We are planning on using the TPS25751 to implement a USB-C sourcing device port (UFP data role, Source power role, No DRP it will only act as a source).
We want to control and configure…
Tool/software:
Hello, I'm currently working on a project where I'm connecting a tablet to a card that must charge it at 5v and 3A (15W in power or 9V and 1.5A).…
Tool/software:
Hi, I'm using a TPS25830Q1EVM-040 in order to link a tablet to a monitor, in order to charge the tablet and send data to the monitor.
Except I'm currently…
Hello.
We are trying to use the TPS65988CERJTR as source. It is connected to a microcontroller, which can control the voltage output of the DC-DC boost. It works with 5V 3A, but we need more power.
I configured new PDOs with 9V/15V…
Customers are interested in configuring the TPS25751 to meet their application need, where can they access the Application Customization Tool mentioned in the TPS25751EVM User Guide (see below)?
I'm designing a docking station/hub that has one USB Type C port with 100W Power Delivery (PD) set up as a sink, and another Type C port with PD set up as a source…
Dear TI E2E,
I'm drafting a "Wireless USB-C Displayport Alt-Mode System" that is primarily intended for detethering 3rd-party USB-C DP Alt-Mode devices.
There are two distinct system scenarios, though…
Hello everyone,
I turn to you because I get some strange behavior from my USB-PD setup which basically is a copy of the USB-PD-CHG-EVM-01 (BQ25792 & TPS25750).
My circuit…
Hello,
I am looking to implement USB-C PD on my new board and I am running into an issue where every device requires an I2C or other communication interface to program…