Hi Adam.
It seems like you are doing everything correct here, I can share with you a configuration that can accomplish what you need. regarding your questions and observations
Adam Lock said: I am only able to get out a watt or so of power into a 4Ω dummy…
Hi James,
James May said: 1. On first connecting to the TAS2563EVM, I get this screen and wonder if it could account for some of my troubles?
this error wont affect the funcitonality of ppc3. the EVM has an eeprom IC on it which stores the boards hardware…
Hi Ning ,
Actually we are newbies to Battery charger .
I am not sure about firmware .
without firmware running firmware we measured the battery voltage ,battery current .
Please let us know where did we get the firmware ? please provide the steps how…
Hello Behnam,
I found this article on decoupling capacitors for high speed op-amps: How (Not (ti.com) . In general X7R and C0G capacitors are better for high speed applications, as ceramic capacitors tend to have a higher frequency 'self-resonance'.…
I just looked at this again, and I see that I was looking at a different digipot when I replied. The other one had one leg of the resistor tied to ground, but the one used in the EVM design has independent pins for both ends of the resistor plus one for…
Part Number: CIRCUIT060074 Other Parts Discussed in Thread: TLV1861 Hi BU team,
Hope you are doing well!
My customer is interested in using comparators to do OCP. Can you help design a current comparison circuit that meets my customer's requirements?…
Part Number: UCC28782EVM-030 Other Parts Discussed in Thread: UCC28782 Hello,
I would like to ask you a question about UCC28782EVM-030. Regarding the measurement conditions in Figure 8-9 on page 16 of this document, the Load Current is described as "1…
Part Number: TPS65130 We are trying to use the TPS65130 to provide +/- supply to two Op-Amps which are being used to drive two transducers which operate at 2MHz. Our current issue is that when running these amplifiers with a bench top DC supply we operate…
Part Number: MSP430F6736A Sir, we are working as E-meter project. MSP430F6736A, this TI ic is suited for my application.
your datasheet is mentioned, When CT or shunts are used, make sure the voltages across CUR2+ and CUR2- does not exceed 920 mV
my doubt…
Part Number: LMX1204EVM Other Parts Discussed in Thread: LMX1204 The EVM used two 1 amp regulators for the LMX1204. One for the VCC01/VCC23 pins and the other for the VCC_CLKIN/VCCLOGICLK pins. The datasheet gives the typical current draw as 1050mA with…