• TLV320ADC3101: output frequency is doubled and have noise

    Part Number: TLV320ADC3101

    Tool/software:

    Hi TI,

    I use TLV320ADC3101 develop project now, below is my schematic:

    I2S mode, MCLK=12.288M fs=48k BCLK=1.536M, 16 bits

    My register configuration is as follows:

    I2CWRITE(I2C_ADC31, 0, 0X0);
    I2CWRITE(I2C_ADC31…

  • TLV320ADC3101: Bandwidth for Input referred noise

    Part Number: TLV320ADC3101

    Tool/software:

    Figure 9 in the datasheet provides the input referred noise for the device.

    I am interested in the Vrms / √Hz value - so I am interested in what the bandwidth was for this measurement.

    I suspect this was…

  • TLV320ADC3001: Linux driver

    Part Number: TLV320ADC3001
    Other Parts Discussed in Thread: TLV320ADC3120, PCM3120-Q1, TLV320ADC3140, TLV320ADC3101, TLV320ADC3100, PCM1822

    Tool/software:

    We currently sruvery TI Stereo ADC IC "TLV320ADC3001", but we would like to first confirm with…

  • TLV320AIC3204: PGA input referred noise

    Part Number: TLV320AIC3204
    Other Parts Discussed in Thread: TLV320ADC3101

    Tool/software:

    Hi,

    I have a question about the input noise of the PGA.

    The datasheet mentions the following (page 11) about the input ferered noise of the PGA, when the AD converter…

  • TLV320ADC3101: TLV320ADC3101

    Part Number: TLV320ADC3101

    Tool/software:

    We want the ADCs to sample the left and right channels at the exact same time so there's no phase error in the data.  A 1kHz test signal shows there's a 0.21 radian (12 degree) phase error between left and…

  • [FAQ] PUREPATHCONSOLE: Software lookup table for audio devices

    Part Number: PUREPATHCONSOLE

    Tool/software:

    A table with links to all the software needed for audio devices and their EVMs. Find the device(s) of interest in the table and use the links to request access to the software you need.

    Product or Part …
  • TLV320ADC3101: Clipped ADC Data from TLV320ADC3101

    Part Number: TLV320ADC3101

    Tool/software:

    We're inputting a 1kHz sine wave to test code with the TLV320ADC3101.  We're getting data from the ADC that looks like the below image.  It appears to be clipping the sine wave and reducing the signal at…

  • TLV320ADC3101: What is the range of the ADC analog input differential for TLV320ADC3101?

    Part Number: TLV320ADC3101

    Tool/software:

    The analog voltage input range of the ADC for TLV320ADC3101 can be found in the manual, as shown in the following figure. The voltage ranges mentioned in the manual are all voltage input ranges under single terminal…

  • TLV320ADC3140: + TLV320ADC3101 5CH microphone array input

    Part Number: TLV320ADC3140
    Other Parts Discussed in Thread: TLV320ADC3101, , TLV320ADC3120

    Hi Team,

    My customer want to achieve 5 channels(4+1) microphone array input audio ADC.

    They are considering to use TLV320ADC3140+TLV320ADC3101 2chips solution, sharing…

  • TLV320ADC3101: Is analog pre-filtering needed for PWM line out from class-D DAC?

    Part Number: TLV320ADC3101
    Other Parts Discussed in Thread: TAS2505, TLV320ADC3120

    I need to digitize multiple analog consumer-level single-ended line-outs into one merged I2S stream. The DSP mode of TLV320ADC3101 and its configurable I2C address seems…

  • TLV320ADC3101: Help needed calculating sensitivity/resolution

    Part Number: TLV320ADC3101

    Good morning,

    we are using above mentioned ADC3101 for measuring very low-voltage analog signals. While it does indeed work very well, I'm struggling with the calculation of the overall sensitivity on a theoretical basis…

  • TLV320ADC3101:

    Part Number: TLV320ADC3101

    For I2S the DUTTLV320ADC3101 will generate with 1 bit offset, for the TDM, does it also transmit the I2S data protocol? Is there 1 bit offset for TDM?

    And are left justified mode with time-slot-based mode enabled and DSP mode…

  • TLV320ADC3101: Single ended vs Differential noise level

    Part Number: TLV320ADC3101
    Other Parts Discussed in Thread: DRV134, DRV135

    We previously have been using the TLV320ADC3101 to monitor differential signals. We now require the device to monitor a single ended signal.

    We did a measurement of the noise levels…

  • TLV320ADC3101: Mixing Audio Inputs

    Part Number: TLV320ADC3101

    Hi all,

    There is an information about mixing ADC inputs at pages 28 and 29 of the datasheet, but I've not found any aditional information or specific register for how to providing this feature.
    Nowadays I have a device configured…

  • [FAQ] Audio ADC FAQs

  • TLV320AIC3204: How to remove DC offsets at the output

    Part Number: TLV320AIC3204
    Other Parts Discussed in Thread: TLV320ADC3101, TLV320AIC3101

    Hi Team,

    My customer is using TLV320AIC3204 and connecting the IN1_R、IN1_L  as shown in the following diagram, and have noticed random DC offset at the output.

    They've…

  • [FAQ] Frequently Asked Questions: Audio Converters and Amplifiers

    Select this link to see answers to common questions, detailed use case implementations, and part recommendations for isolation devices.                                                                                                                                                       .     

    Top Audio FAQs - All-Time

    How to install…

  • TLV320ADC3101: About the MCLK pin.

    Part Number: TLV320ADC3101

    Hi, what should I do if the MCLK pins are not used? Can it be suspended or link to ground?

  • TAS2562: tas2562 design review

    Part Number: TAS2562
    Other Parts Discussed in Thread: CC8530, TLV320ADC3101, TAS2563

    I have designed a board using two TAS2562 amplifiers. If possible, I would like to have the audio portion of the design reviewed by an expert before ordering the boards…

  • TLV320ADC3101: Real time change of CODEC sampling rate under Linux system

    Part Number: TLV320ADC3101

    Hi team,

    One of our customer's issues, could you please give your comments?

    Can the sampling rate of TLV320ADC3101 be changed in real-time during device operation on Linux systems? What about resolution and gain ?

    Best Regards…

  • TLV320ADC3101: Two audio differential inputs, Linux drive porting

    Part Number: TLV320ADC3101

    Hi team,

    The customer now is configuring TLV320ADC3101 two audio differential inputs, they would like to know how to configure and port the driver for the audio under Linux? It's required to be ported to the i.MX 8M Mini platform…

  • TLV320ADC3001: Channel number cannot match

    Part Number: TLV320ADC3001
    Other Parts Discussed in Thread: TLV320ADC3101

    Hi team,

    Debug audio codec for audio recording verification via arrecord.

    1) A sine wave signal (analogue sound signal) is generated by the signal generator and is connected to the…

  • TLV320ADC3101EVM-K: TLV320ADC3101EVM-K

    Part Number: TLV320ADC3101EVM-K

    Hi,

    We are using TLV320ADC3101EVM-K, in our application. 

    As a initial testing, we have given  1V P-P as input to Analog input of Eval board (i.e. J6) and removed the W4 jumper. And we have connected the I2S output from J5…

  • TLV320ADC3101: TLV320ADC3101IRGER

    Part Number: TLV320ADC3101

    We find the TLV320ADC3101IRGER  has FFT Noise on 800HZ to 6KHZ @ Gain = Min , the setting is 48KHZ sample rate ,,  pls reference attach file , we debug the FW and  HW can't find  the Solutions , pls TI FAE help , thanks lot !

  • TLV320ADC3101: double package and footprint on datasheet

    Part Number: TLV320ADC3101

    Hi,

    in TLV320ADC3101 datasheet are provided 2 different packages for the same part number: RGE0024B and RGE0024F
    Which is the correct one?

    Best regards,
    Marco

1 2 3 4 5 »