Other Parts Discussed in Thread: LMX2492
Tool/software:
Hi TI team,
We're trying to implement a simple triangle frequency ramp using the LMX2492. The idea is:
Ramp0: 9400 MHz → 9485 MHz in 100 µs
Ramp1: 9485 MHz…
Tool/software:
Hi TI team,
We're trying to implement a simple triangle frequency ramp using the LMX2492. The idea is:
Ramp0: 9400 MHz → 9485 MHz in 100 µs
Ramp1: 9485 MHz…
Tool/software:
Hello,
We have recently purchased the LMX2492EVM and would like to clarify a few details regarding VCO replacement.
Our goal is to replace the onboard VCO on two separate…
Tool/software:
I would like to make sure that the component is compatible with my project.
in my project, I would like to apply a very fast sweeper across two channels:…
Tool/software:
I am doing a FMCW project and I would like to know if, to get a chirp at 10GHz and with a bandwidth of 1GHz, it is enough only with the LMX2594 EVM evaluation board…
Tool/software:
I am also using the LMX2492 for an FMCW radar and have found that undesirable spurs that are created from using the chirp feature.
Like the previous designer, I am also seeing…
Tool/software:
Hi Texas team,
I am using LMX2492EVM and LMX2594EVM board for our application where we need Ramp signal which bandwidth will be 1.5…
Tool/software:
Hi all
I use LMX2492 in my FMCW radar , i find that if i set LMX2492 to CW ,the spectrum after ADC sampled is clean . it just has some sub fraction spurs,the level of the…
Tool/software:
Hi,
I am using a TICSPro_1.7.7.5_23-Jul-2024.exe version of TICS Pro on a Windows 11 Enterprise, 10.0.22631 OS. I was able to use the software three days ago, until today…
Tool/software:
Hi Texas team,
We want to use LMX2594EVM board for our application. We have some enquiry about it which is given below,
1. Is it needed to buy separate…
Hi TI experts,
I'm looking for PLL chip featuring no internal VCO and minimun N divider value down to 1, and frequency range covers 2700MHz,do you have any suggestions?
thx!!
I have been using this part in a design for quite some time, there has always been an interesting relationship in the CP settings and how it affects the loop bandwidth. As you increase the CP settings it does move the loop corner…
Dear TI Team,
I'm currently making use of the LMX2492EVM for ramp generation within a low power FMCW radar system, but would like to make some changes to the VCO circuitry.
Is it possible to share the Altium project files?
…Dear TI teams,
I am using LMX2492EVM hardware for our application. We are using this hardware as a X-band LFM signal source. And we are mixing the same signal with some delay in Mixer. According…
Hi everyone!
Now i am testing the LMX2492 EVM. I downloaded and installed the current version of TICS Pro
I followed all the instructions on LMX2492EVM User's guide.
Then I tried the example…
Dear E2E support,
I am Located in the Netherlands' and wonder if there is a TI service center to repair the broken LMX2492evm.
I have two broken LMX2492evm, one caused by a power spike…
Iam testing the LMX2594 Evaluation module using TICS Pro software. It is required to test in automatic ramping mode with frequency from 12 to 12.4 GHz i.e. 400MHz in 100…
Hi Team,
For Chirp signal genenrated by LMX2492+CHC2442, frequency .vs. time Chirp Linearity is critical for our application. However, Suggested by some experience, the actul generated Chirp Linea…
Hi Team,
The frequency synthesizer configuration is LMX2492+CHC2442, generating a Chirp signal with a time interval of 204us and a bandwidth of 50MHz. Our concern is that within the 204us duration, we need to traverse the entire 50MHz bandwidth. Does the LMX2492 need
…