• TXB0304: Power consumption Calculation

    Part Number: TXB0304

    Tool/software:

    Hi Team,
     We are using this part in our design , need to know about the calculation of power consumption for this part 
    Please help us to calculate 

  • TXB0304: spec check

    Part Number: TXB0304
    Other Parts Discussed in Thread: TXB0104-Q1

    Tool/software:

    Hi

    Could you please help confirm whether there are any materials with the same specifications as the following materials and working temperature of -40~125°C that can be…

  • TXB0304: Unused ports

    Part Number: TXB0304

    Tool/software:

    Hello team,

    Should I tie the output of the unused ports to GND?

    My customer has tied the inputs to GND, but they have observed oscillation at the output.

    Best Regards,
    Kei Kuwahara

  • TXB0304: IBIS model

    Part Number: TXB0304

    Tool/software:

    Hello,

    Our customer has a question about if we can support 1.5V IBIS model for his circuit design.

    Best regards,

  • [FAQ] Which IBIS model should I choose for simulating Auto-Bidirectional Translators (LSF,TXB,TXS) ?

    Other Parts Discussed in Thread: LSF0101

    FAQ: Logic and Voltage Translation >  Auto-Bidirectional Level-Shifters > Current FAQ

    In most cases, it is recommended to test with the device EVM instead as it yields much more accurate results under specific…

  • TXB0304: QSPI translation - TXB0304 and propagation delay

    Part Number: TXB0304
    Other Parts Discussed in Thread: TXB0302, TXB0106

    Tool/software:

    Hello,

    In our design, we need to perform level translation on a QSPI signals between an FPGA (1.2V) and QSPI Nand Flash (1.8V).

    We would like to optimize the bandwidth…

  • TXB0304: USB2.0 Support

    Part Number: TXB0304

    Tool/software:

    Hello,

    Does the TXB0304 support USB2.0 level translation?

  • [FAQ] Auto-Bidirectional Level-Shifters

  • [FAQ] TXB0304 oscillates but TXB0104 works, why?

    Other Parts Discussed in Thread: TXB0304, TXB0104

    FAQ: Logic and Voltage Translation >  Auto-Bidirectional Level-Shifters  >> Current FAQ

    The most common reason is due to impedance mismatches. 

    TXB0304 specifies a stronger output impedance than TXB0104…

  • TXB0304: QSPI Trace limitation and evaluation of one short level-shift

    Part Number: TXB0304

    We use TXB0304 to transfer 33MHz and 16MHz CLK from 1V8 to 3V3.

    The topology list show as below:

    Topology 1: QSPI 16MHz trace length is 14" after level-shift, the waveform of CLK can't be recognized.

     Is there any solution…

  • TXB0304: The power consumption of TXB0304

    Part Number: TXB0304

    Hi,

    I encounter a issue about current, the schematic is as follows,

    Story:

    Step 1.  When the voltage of VDD_EXT changes from 1.8V to 0V, the current of TXBN0304 will be as high as 400uA(20pcs out of 100pcs chips will have this issue…

  • TXB0106: For SPI 1.8V to1.2V level shift ,Input 20M,output is 10M or some cycle lost.

    Part Number: TXB0106
    Other Parts Discussed in Thread: TXU0304, TXB0304, SN74AVC4T774

    Dear,

    I use TXB0106 for SPI level shift from 1.8V to 1.2V.When clock data rate is 20M,out waveform is incorrect 

    The out waveforms are as follow. 

    input is 20M,output…

  • TXB0304: eSPI redriver

    Hi team,

    Could you please recommend eSPI redriver(50MHz, 4channel)? If we have, what's the layout requirement for this device? Close to TX or close to RX? 

  • TXB0304: spec check

    Part Number: TXB0304
    Other Parts Discussed in Thread: TXU0102

    Hi

    Customer measurement found that U22 PIN8 has an abnormal waveform when USB is abnormal (USB_OC#_abnormal.png) U22 uses TXB0304RUTR

    Changing RA43 to a smaller size (1K for testing) can solve…

  • TXB0304: The internal circuit of the TXB0304 chip passes through a 1K resistor and then outputs it, causing an impedance mismatch in the high-speed circuit.

    Part Number: TXB0304
    Other Parts Discussed in Thread: TXU0304, TXU0104, TXU0204

    The internal circuit output of the TXB0304 chip needs to pass through a 1K resistor, which will cause a resistor-impedance mismatch during high-speed signal conversion, causing…

  • TXB0104: Application issues of chips

    Part Number: TXB0104
    Other Parts Discussed in Thread: TXB0304, SN74AXC4T774, TXU0304

    As communication with the phone, we use TXB0104 to level shift our controller‘s IOs to GDDR6 DRAMs’s JTAG, we found the JTAG link is not stable especially when the G6…

  • SN74AVC4T774: Starup Behaviour of AVX and AVC devices.

    Part Number: SN74AVC4T774
    Other Parts Discussed in Thread: SN74AXC4T774, TXU0304, TXU0104, TXU0204, TXB0304

    This is a question for both the AVX and the AVC parts.

    1. We are having the VCCA coming up first and the VCCB coming up after a few seconds. In the…
  • TXB0304: POWER SUPPLY RANGE

    Part Number: TXB0304
    Other Parts Discussed in Thread: TXU0304

    Hi,

    We are using TXB0304RUTR bidirectional level translator in our design for converting 3.3V to 1.8V. Can you please confirm the supply range for VCCA and VCCB.

    We need to establish connection…

  • Which Level Translator for application?

    Other Parts Discussed in Thread: TXV0108, TXU0304, SN74AXC4T774, TXB0304

    Hello,

    I am looking for a bi-directional level translator that has V_CCA of 1.8V and V_CCB of 3.3V OR 1.8V. 

    The IO voltage is 1.8V and some applications require 3.3V. I am looking…

  • TXB0108: QSPI 1.8V <> 3.3V

    Part Number: TXB0108
    Other Parts Discussed in Thread: TXB0304, TXB0106

    Hi expert,

    Customer is looking for level shift solution for 1.8V <> 3.3V with 31.25Mhz data frequency. I see TXB0108 only supports to 60Mbps(30Mhz). 

    Could you please advise proper…

  • TXB0304: Difference between TXB0304 and TXB0104

    Part Number: TXB0304
    Other Parts Discussed in Thread: TXB0104

    Hi team,  

    What's the difference between TXB0304 and TXB0104?

    Nison

  • TXB0304: level shifter with only one shot

    Part Number: TXB0304
    Other Parts Discussed in Thread: TXU0304, TXU0104, TXU0204

    Hi team,

    Do we have level shifter with only upper one shot?

    Nison

  • TXB0304: TXB0304 review schematic

    Part Number: TXB0304

    Hi, Support Team

    We will use TXB0304 as below chart, have any concern?

    if any suggestion, Please advise me.

    Thanks,

    Best regards,

    Lawrence

  • TXB0304: Recommended SPI buffer

    Part Number: TXB0304
    Other Parts Discussed in Thread: TXU0304, TXB0104

    Hello Team,

    We use the SPI trace length is about 20" on MB, we plan to add a SPI buffer on MB

    Can the TXB0304 be used as a buffer for SPI? or do you have any better suggestions…

  • LSF0108: Pull-up resistor value

    Part Number: LSF0108
    Other Parts Discussed in Thread: TXB0304

    Hi,

    I can find the calculated pull-up resistor value on "Table 9-3. Pull-Up Resistor Values".

    Is this Minimum value?  My customer wants to add a few k-ohm.  Is it OK to add a few k…

1 2 3 4 5 »