Other Parts Discussed in Thread: 2N7001T, TXU0202
Tool/software:
Hi there,
I'm struggling to get a UART port to an FTDI cable TTL-232R-3V3 up and running on a carrier board for an Ezurio SOM and I wonder if the issue isn't my level…
Tool/software:
Hi,
We are currently experiencing an issue where the +3.3V system is being damaged in a circuit utilizing the TXS0108E.
We would like to understand the possible causes and countermeasures for this issue, and we would…
Tool/software:
Hi Team,
The specs of tW, pulse duration(open-drain), have been downgraded due to PCN20241115003.0.
Please see attached for details.
The PCN document states the following as the reason for change.
To accurately reflect…
Tool/software:
Hi Team,
We are using the below attached circuit for driving our Bidirectional LED.
But the LED intensity is very low.
Looks like some drive issue.
Please suggest…
Tool/software:
I use the TXS0108EQPWRQ1 in our product for the CAN Transceiver - Microcontroller communication line to act as a level shifter from 3.3V to 5V. The device…
Tool/software:
Hello!
I'm using the TSX0108E in an I2C application and struggle to understand exactly how the behaviour is.
For my 400kHz I2C bus bus-pull-up calculations etc it is essential to know how the TXS0108E is helping…
Tool/software:
Can we use TXS0108E for MIPI clock & Data signals voltage translation of 1.8V to 3.3V with data rate of 2Gbps?? If not, Can you suggest any alternate part.
Tool/software:
Hello.
I am currently designing the timing for a circuit using the TXS0108E.
The circuit accesses MRAM from an FPGA via the TXS0108E.
The power supply voltage for the TXS0108E is VCCA=1.8V, VCCB=3.3V.
After checking…
Tool/software:
Hello, I am using the TXS0108E as a level shifter from 3.3V to 5V for my 5 MHz SPI. Unfortunately, I am experiencing unwanted ringing on the edges. To address this, I added…
Tool/software:
Hi team,
can you help to see why the VIL of TXS0108E is such low as 0.15V? while the TXB family can accept 0.35*VCCI?
the 0.15V is much difficult to cooperate with other TXP device like TCA9617's output. is there…
Tool/software:
Hi team,
Does TXS018 have an inverting output type? thansk
Tool/software:
Hello Sir,
In "www.ti.com/.../TXS0108E" product page High input voltage (min) (V) seems 1V.But in the product page:
İt seems 5V-0.4 = 4.6V High input voltage…
Tool/software:
Dear TI Team,
I have referred to the material data sheets TXS0108E - SCES642I to TXS0108E - SCES642L for comparison.
After discussing with QE, our customer requires your assistance in identifying and highlighting the…
Tool/software:
Hi
In the previous product, the following was used:
SN74LV244APWR, 5V -> 3.3V Level shift …
Tool/software:
Hi expert,
Customer used TXS0108ENMER and find a pulse one the B1 WL_REG_ON. Do you have any idea what might be the reasons?
Regards,
Allan
Tool/software:
Hi Team,
There is GPIO, SPI and UART Interface between IC1 and CPU.
Following are the IC1 IO Levels (Type I and II).
VOHmin=3V, VOHmax=3.3V
VOL max=0.4V
VIHmin…
Tool/software:
At present, our low-power doorbell products use TXS0108E (connected to WiFi module and main control SOC, communicating through SDIO, and the level shift enable pin OE pin controlled by low-power MCU). However, when…
Tool/software:
Hi team,
Using TXS0108E, MCU controls pin OE, and there is a voltage of around 0.42V in sleep mode, which has not fully entered the high impedance state.
Please help analyze the reason, thank you!