Quickly find solutions to common questions about voltage translation (level shifter) devices by clicking this link. This FAQ answers the most common questions asked about these devices …… ……… …
| Auto-Bidirectional Level-Shifters | Fixed DIR / DIR CNTRL Level-Shifters | Ground-Level Translators | SPI I/O Expander | IxC | Generic | Use Cases & Part Recommendations |
- [FAQ] If the OE pin is asserted to maintain Hi-Z at the IO, will it disconnect the internal pull-up resistors in TXS devices?
- [FAQ] Are there voltage level translation / level shifter device recommendations for the industry standard interfaces like GPIO, SPI, UART, I2C, MDIO, RGMII, I2S etc?
- [FAQ] What are the power sequencing requirements for the translation device?
- [FAQ] What should be done with unused I/O pins of the level translator devices?
- [FAQ] Is there a naming convention for Level Shifters?
Input Parameters:
- [FAQ] Is the reliability of a logic device affected by applying an input voltage larger than the supply (VCC)?
- [FAQ] What is the impedance of the device's input pin? Is it CMOS or bipolar device?
- [FAQ] Is it necessary to have pull-down( or pullup) resistor on the OE pin or can I connect it directly to TXS/ TXB supply?
- [FAQ] Can I connect the OE pin to Vccb supply pin instead of Vcca for TXS, TXB devices?
- [FAQ] What should be done with unused I/O pins of the level translator devices?
- [FAQ] Why does my device not switch at VIH or VIL?
- [FAQ] How do I size pull-up or pull-down resistors?
- [FAQ] How do I terminate any unused channels of a logic device?
- [FAQ] How does a slow or floating input affect a CMOS device?
- [FAQ] Can the input voltage (Vi) to my logic device be higher than the supply voltage (Vcc)?
- [FAQ] What is the TXS device internal resistor variation/ tolerance
- [FAQ] What is a floating input or floating node?
- [FAQ] What method is best used for estimating specification values between those given in the datasheet?
- [FAQ] What are the performance specifications of the HCS logic family at 3.3V operation?
- [FAQ] Do I still need pull-up/pull-down resistors with bus-hold circuitry?
Output Parameters:
- [FAQ] With Open-Drain outputs, can I ...use them to shift a logic voltage level? ...connect the outputs directly together? ...force a voltage node to zero?
- [FAQ] What should be done with unused I/O pins of the level translator devices?
- [FAQ] How do I determine the output voltage (VOH, VOL) or output current (IOH, IOL) of a CMOS logic device?
- [FAQ] What is the maximum trace length that a logic device can drive?
- [FAQ] What happens when I connect a logic device's output to a 50 ohm transmission line?
- [FAQ] Can I connect two outputs from a CMOS logic device together directly?
- [FAQ] How do I size pull-up or pull-down resistors?
- [FAQ] What is the output voltage (VOH or VOL) when the output current is X or the supply voltage is Y?
- [FAQ] How do I terminate any unused channels of a logic device?
- [FAQ] What is the default output of a latched device? (Flip-Flop, latch, register)
- [FAQ] What is the maximum capacitive load that a logic device can drive?
- [FAQ] What is the output transition rate for a logic device?
- [FAQ] What is the TXS device internal resistor variation/ tolerance
- [FAQ] Can you pull-up an open-drain output to a higher voltage than the device's supply (VCC) voltage?
- [FAQ] What is a floating input or floating node?
- [FAQ] What's the difference between logic output types (push-pull, open-drain, 3-state)?
- [FAQ] What method is best used for estimating specification values between those given in the datasheet?
- [FAQ] What are the performance specifications of the HCS logic family at 3.3V operation?
Timing Parameters
- [FAQ] What is the typical delay of a logic device in a particular logic family?
- [FAQ] What is the difference in timing between gates in the same device? How much skew is expected within a given logic device? What is the part-to-part skew?
- [FAQ] What is the maximum data rate (or operating frequency) for a logic gate or buffer?
- [FAQ] What method is best used for estimating specification values between those given in the datasheet?
- [FAQ] What is the output transition rate for a logic device?
Power and Thermals:
- [FAQ] How do I Calculate Power Consumption or Current Consumption for my CMOS Logic Device?
- [FAQ] What are the power sequencing requirements for the translation device?
- [FAQ] Where do I connect the thermal pad of the logic QFN devices?
- [FAQ] What is the maximum junction temperature (TJMAX) for a device?
- [FAQ] Where do I find maximum power dissipation for a device?
- [FAQ] How do I select a bypass capacitor for a CMOS logic device?
Quality and Manufacturing:
- [FAQ] Why does a logic device's part number have an E4/G4 suffix?
- [FAQ] When will TI End of Life (EOL) or Obsolete a certain logic device?
- [FAQ] Are there voltage level translation / level shifter device recommendations for the industry standard interfaces like GPIO, SPI, UART, I2C, MDIO, RGMII, I2S etc?
- [FAQ] Why do the leadframes look strongly oxidized or corroded?
- [FAQ] What do the underside markings on a part mean?
- [FAQ] What is the difference between TXS TXB and LSF devices?
- [FAQ] What are the RHA numbers, codes or radiation testing ratings for my high reliability part number?
- [FAQ] How do I find reliability data for a logic device?
- [FAQ] Is part number X pin to pin compatible with part number Y?
- [FAQ] How do I set up a TI.com device re-stock notification?
- [FAQ] Where can I get a CAD symbol, soldering footprint, or 3D model for my device?
- [FAQ] How will a logic device respond to a short or open circuit?
- [FAQ] Why do some SOT package parts from TI have a pin that is not in the mechanical drawing?
- [FAQ] What is the thickness of Gold (Au), Palladium (Pd), or Nickel (Ni) for TI's NiPdAu lead finish?
Simulation Models:
- [FAQ] An IBIS model returns the error "syntax error, unexpected IdentToken, expected $end" - what is wrong?
- [FAQ] How to import Logic SPICE models netlist into TINA-TI (Logic TINA-TI test benches)
Monostable Multivibrators:
- [FAQ] How does a monostable multivibrator (one shot) work?
- [FAQ] Why is there no PSpice model for a Monostable Multivibrator device?
- [FAQ] What is the maximum output pulse length for a monostable multivibrator?
- [FAQ] How stable is the output pulse length of a monostable multivibrator across changes in supply voltage?
- [FAQ] How stable is the output pulse length of a monostable multivibrator across temperature?
- [FAQ] How do I configure a monostable multivibrator's inputs for rising/falling edge triggering?
- [FAQ] Can I connect the Cext pin to ground on a monostable multivibrator?
- [FAQ] How do you determine the output pulse width and the 'K' value for a monostable multivibrator?
- [FAQ] How do I terminate an unused channel of a monostable multivibrator (one shot)?
Logic Technology:
- [FAQ] What's the difference between TTL and 5V CMOS logic?
- [FAQ] What is the difference between IOFF and VCC isolation? What are the conditions to guarantee it?
- [FAQ] Difference between Multiplexer/De-multiplexer and Analog Switch
- [FAQ] What does 'partial power down' or 'Ioff' mean in the datasheet?
- [FAQ] What is the difference between the SN74HCxx and the SN74HCxxA?
- [FAQ] What's the difference between a buffered and unbuffered CMOS device?