This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
when I try to connect the MSP-FET to program the MSP430F2617 chip, Uniflash shows me the message "No debug probes/devices detected", both in Auto and Manual setting.
I tried with different cables but the connection still doesn't work.
The drivers are updated, and I can also see 'MSP Application UART1' and "MSP Debug Interface" device in device manager.
Any suggestion o how to solve my issue?
Thank you.
Stefano
Hello Dennis,
thank you for your reply. Yes, I am able to connect the debugger to CCS and it works.
The version of Uniflash I am using is updated to the 6.4.
Here is a screenshot of what it shows me everytime I try to program with Uniflash.
Even if I try to add manually the .ccxml file I cannot flash the image during the second step and here is the message I see.
Yes, I am able to connect the debugger to CCS and it works.
What version of CCS did you use?
And what is the Host OS version (please specify if you are using 32 or 64 bit version also)
Thanks
ki
OS is win10 32 bit.
This is the issue.
CCS 8.1 is supported on Win32.
UniFlash 6.4 is not. It only supports 64-bit Windows.
The last version of UniFlash to support 32-bit Windows is UniFlash 4.6:
http://software-dl.ti.com/ccs/esd/uniflash/docs/release_archive.html#uniflash-v4-releases
Thanks
ki
Thank you,
I installed the older version 4.6 and now Uniflash correctly identify the FET.
**Attention** This is a public forum