[FAQ] AM625 / AM623 / AM620-Q1 / AM625-Q1 / AM625SIP Design Recommendations / Custom board hardware design – Common queries for PMIC TPS65219 and PDN

Part Number: AM625
Other Parts Discussed in Thread: TPS65219, TPS65219-Q1, TPS6521905, TPS65215, AM2434, TPS65220, AM6421, TPS22918, , TPS6522005-EP, , AM6548, TPS22965, AM623

Tool/software:

HI Board designers, 

I am designing my board using TPS65219.

Are there some common recommendation or observations that i should be aware?

Note: Learn about TI's automotive PMIC portfolio and TPS65219-Q1 for powering Sitara AM62x-Q1

https://www.ti.com/video/6326829023112

  • HI Board designers, 

    Refer below, common queries and replies

    Q.1

    Our customer has a question about TPS65219. Customer thinks to use TPS6521901 for supplying AM64x power. Is the TPS6521901 programmable device? Or, Is TPS6521901 not programmable device and customer cannot change anything of the output voltage and power sequence? If customer wants to change the power sequence, does customer needs to use TPS6521905? Customer worries about the unintentional change of power sequence. So, customer is happy if TPS6521901

     The TPS6521901 and TPS6521905 both have NVM that can be reprogrammed. It is not easy to accidentally reprogram the NVM, so I do not think the customer needs to worry about accidentally modifying the power sequence. 

    The TPS6521905 comes with default setting with all outputs disabled, so it is helpful if a customer wants to program the device on the PCB while keeping all of the outputs in a safe state. 

      Q.2

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1407703/am625-pmic_lpm_en0-connection

    Connecting the PMIC_LPM_EN0 to the PMIC MODE/STBY pin is optional. The TPS6521904 NVM has the MODE/STBY pin configured to select the Bucks switching mode with the following polarity:

    • MODE/STBY High, Bucks operate in forced-PWM
    • MODE/STBY Low, Bucks operate in auto-PFM. 

    If you are planning to use an AM62x low power mode where internal processor domains are turned-OFF while all the PMIC rails stay ON, then driving the MODE/STBY pin low with the PMIC_LPM_EN0 will allow to increase efficiency at light load. 

     Q.3

    (+) AM625: How to set correct VDD_CORE & VDDA_DDR_PLL0 for LPDDR4 - Processors forum - Processors - TI E2E support forums

    TPS6521908 is another option for customers who want to supply VDD_CORE with 0.85V instead of 0.75V. As noted in the processor datasheet, VDD_CORE and VDDR_CORE are expected to be powered by the same source so they ramp together when VDD_CORE is operating at 0.85V. In this scenario, we don't need to configure an LDO in the PMIC to supply 0.85 because Buck1 can supply both. This is why LDO2 is disabled. 

    Q.4

    (+) TPS65219: 3.3V no output - Power management forum - Power management - TI E2E support forums

    The TPS65219 PMIC executes two residual voltage checks; the first one occurs before the power-up sequence is executed and a second occurs during the power-up sequence (right before each rail is turned ON).

    The first check can be disabled by changing register field "Register field "BYPASS_RAILS_DISCHA RGED_CHECK" but the second one cannot be disabled. Please note that changing any register field would require to turn-ON the PMIC first and get the device in Active state to enable I2C communication. 

    we found out where the residual voltage is coming from. This is come from E-PHY 

    - Residual voltage VLDO4 , 2.5V line : 4~500mV /  VDDIO, 3.3V line : 50mV. 

    If the backfeeding issue on VLDO4 exist before the PMIC executes the power-up sequence, then none of the rails will turn-ON. The reason is because as I mentioned in my previous message, the PMIC performs the first residual voltage check before executing the power-up sequence.  

    Do you see a voltage on VLDO4 before Buck2 is turned ON?

    TPS65219: Residual Voltage checks during start-up

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1434550/faq-am625-am623-am625sip-am620-q1-am625-q1-design-recommendations-ustom-board-hardware-design-common-queries-for-pmic-tps65219

    Regards,

    Sreenivasa

  • HI Board designers, 

    Refer additional inputs

    Q.5

    TPS6521905: NVM programing procedure

    https://www.ti.com/lit/ug/slvucm5/slvucm5.pdf

     Q.6

    (+) TPS65219: Can the maximum load capacitance of the channels be exceeded? - Power management forum - Power management - TI E2E support forums

    If the maximum output capacitance on the PMIC rails is exceeded, the phase margin starts to drop and stability gets affected.

    Just for reference, the TPS65219 PMIC has an option for "multi-PMIC operation" that allows to fully synchronize the sequencing between multiple TPS65219 devices. This feature might help to split the load/POL capacitance across the PMIC rails. Is this a non-automotive application? The TPS65215 has a 4x4mm package option that helps to keep the overall power solution small even when using 2x TPS65219 devices.  

     

    https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1204248/tps65219-reprogramming-the-tps65219

     This is a great feature in the TPS65219 PMIC that allows synchronizing multiple devices to power processors and SoCs that require multiple rails! Here is some information for the multi-PMIC operation, feel free to let us know if you have any questions and we will be happy to help.

    • GPIO (pin#16) is used to synchronize the two PMICs. 
    • To configure the GPIO pin for multi-PMIC, register field "MULTI_DEVICE_ENABLE" must be changed to 1.
    • The GPIOs on both PMICs should be tied together sharing the same pull-up resistor.  
    • The I2C address for the 2nd PMIC must be changed on register field "I2C_ADDRESS" so they can both be connected to the same I2C bus without conflict. 

     Q.7 TPS65219: Share 3.3V rail for 2pcs AM2434 and peripherals

     If the customer wants to use a single 3.3V rail to supply both MCUs and peripherals, then I would recommend using the TPS6521904 NVM instead.

    Here are the two options when using TPS6521904:

    • Using 3.3V pre-regulator to supply the 2x TPS6521904 PMICs and an external 3.3V power-switch. The power-switch can be enabled by the PMIC GPO2. The output of the power-switch can supply the MCU 3.3V IO and peripherals.
    • Using a 5V pre-regulator to supply the 2x TPS6521904 PMICs and an external 3.3V BUCK. The external Buck can be enabled by the PMIC GPO2. The output of the external 3.3V buck can be used to supply the PMIC LDO1, MCU 3.3V IO and peripherals. 

    Regards,

    Sreenivasa

  • HI Board designers, 

    Refer additional inputs

    Checklist and guidelines for PMIC

    https://www.ti.com/lit/zip/slvafe2

    Regards,

    Sreenivasa

  • HI Board designers, 

    Refer below additional inputs: 

    TPS65219: Residual Voltage checks during start-up

    ttps://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1229202/tps65219-residual-voltage-checks-during-start-up

    The TPS65219 PMIC performs a voltage check and discharge on each of its power rails to make sure they are all under the SCG threshold before executing the power-up sequence. 

    Although not recommended, this safety feature could be bypass by changing the register field "BYPASS_RAILS_DISCHARGED_CHECK" on address 0x1E. Since there is no I2C communication in Initialize state, PMIC would have to be programmed from factory to bypass the discharge check during power-up/power-down sequence. Any custom NVM configuration requires a new orderable part number and approval from our marketing team. 

    TPS65219: Programming NVM using the processor itself

    (23) TPS65219: Programming NVM using the processor itself - Power management forum - Power management - TI E2E support forums

    TPS65219: Difference between TPS65219 and TPS65220

    (23) TPS65219: Difference between TPS65219 and TPS65220 - Power management forum - Power management - TI E2E support forums

    TPS65220 is designed to operate over extended temperature range.

    Regards,

    Sreenivasa

  • Hi Board designers

    Input regarding selection of PMIC:

    The recommend PMIC(s) on the product folder or used on the SK or EVM schematics has been designed considering the power sequencing, supply rail output slew, nRSTOUT (reset output) delay output from PMIC connected to MCU_PORz after all the supplies ramp for clock to be stable and the sizing of the supply rails based on the processor worst case current draw.

    When choosing an alternate non-TI PMIC, the recommendation for custom board designers is to review the relevant collaterals including the data sheet and Maximum Current Ratings document and follow the requirements/recommendations. The recommendation is to review the slew rate requirements, Power-up and power-down sequence sections of the data sheet and confirm the non-TI PMIC based power architecture follows the recommendation.

    An important point to note is the processor does not support dynamic scaling of the core voltage or the analog supplies.

    Inputs regarding supply decay

    Refer below FAQ

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1485094/faq-am62a7-power-rails-decay-note-in-latest-datasheet/5703704#5703704

    I have placed the note in both sections because it applies to both power-up and power-down. The power-up sequence should not begin until all power rails are below 300mV, and the power-down sequence is not complete until all power rails are below 300mV.

    Regards,

    Sreenivasa

  • HI Board designers, 

    Inputs on power supply sizing:

    Using Maximum Current Ratings application note vs Power Estimation Tool PET 

    The max current app note is representing the current draw for a group of rails. Please note that it is not expected for this current to necessarily be replicated in the power estimation tool. The PET will tend to show more average use case power while the max current app note is intended to be used for power supply sizing as it will allow for the max transient on these groups with some margin. The PET should not be used for power supply sizing.

    Power Estimation Tool (PET) and the max current rating apps note serve two different purposes. The PET is used to estimate active power consumption for a specific use case/application. The max current rating apps note can be used for supply sizing when designing a custom power solution

    Regards,

    Sreenivasa

  • HI Board designers, 

    Note:

    How were these pdn specs derived? Is it based on worst case analysis?

    Yes it is based on worst case load transient estimates for a given SoC design.

    The Target impedance for AM62x and AM62xSiP will be identical as the same worst case load transients exist on both designs since they share the same die.

    Via sharing recommendations in the escape application note are only made to help guide a customer to escape the design with fewer vias in the VCA regions. The number of vias used for escaping signals will ultimately depend on the specific customer use-case, the number of interfaces that need to be implemented and the layer count. If the specific use case allows the customer to use more vias for VDD_CORE in the VCA regions, that is definitely a valid approach. Per-pin loop inductance guidelines are more applicable for single-pin supplies that are connected to a decap. In case of multi-pin supplies like VDD_CORE where there are a number of parallel connections to multiple pins/decap thru multiple vias, it is hard to tie it back in to a per-pin requirement. The most important target to meet is the impedance target specified in Table 7-6 of the PDN Applications note. This table is the same for AM62x and AM62x SiP.

    We do not include Buck output inductance in PDN simulations.

    For VDDS_DDR: we do not recommend using target impedance as the signoff for DDR.
    Refer to the AM62x, AM62Lx DDR Board Design and Layout Guidelines which outlines all details of power aware SI/PI simulations
    that need to be run. The eye mask checks from these power aware simulations are the signoff.

    Power Distribution Networks: Implementation and Analysis

    Sitara Processor Power Distribution Networks: Implementation and Analysis

    https://www.ti.com/lit/pdf/sprac76

    Note: The decoupling capacitor numbers and type on the SK/EVM are only intended to serve as a guideline for customers. The true pass/fail criteria is the target impedance published in the PDN app note.

    High Speed Board design and Signal integrity simulation 

    https://www.ti.com/lit/pdf/spraar7

    https://www.ti.com/lit/pdf/spracn9

    https://www.ti.com/lit/pdf/sprabi1

    Inputs on PDN 

    (+) [FAQ] AM62A3-Q1: AM62A3-Q1 PDN Power SI SIMULATION Questions - Processors forum - Processors - TI E2E support forums

    Please refer below inputs i received:

    Please note these are only recommendations and they need to contact their EDA vendor on what works best for their specific simulation environment.
    1、Do I need to separate VDD_CORE-1 to 17 for simulation, or use VDD_CORE as a Port?
    TI>> You can lump all VDD_CORE BGAs together as a single terminal for the port
    2、Do I need to include the PMIC FB loop in the simulation?
    TI>> If you are simulating only for AC impedance (target impedance checks) this is not required. The board layout from the inductor onwards (inductor not included) can be modeled and PMIC FB loop can be studied separately.
    3、 Is the simulation starting frequency from 1Hz or from a minimum of 100kHz for the capacitor S2P?
    TI>> There should be some DC frequency points added. Please check with your EDA vendor on the exact setup and simulation points needed to generate causal models.

    I added additional inputs related to PDN and decoupling capacitors for reference.

    The voltage at the device ball must never be below the MIN voltage or above the MAX voltage for any amount of time. This requirement includes dynamic voltage events such as AC ripple, voltage transients, voltage dips, and so forth

    PCB design & Dcap scheme combine to form your board's Power Distribution Network (PDN) that should meet recommended SoC PI performance targets for robust processor operations. Each PCB design has a "unique finger-print" based upon component placements, power & Gnd routing, layer assignments, via qtys & locations, Dcap mounting & loop inductance, Dcap parameters, etc. As a result, an optimized Dcap scheme will vary from one PCB design to another but should provide a system PDN that meets PI performance targets when combined together. Similarly, the PI simulation tools can impact the estimated ZvsF response values, especially above 3.0MHz where non-3D extraction tools can return better Z values (10-15% less than more accurate 3D tools). This ican be due to a non-3D tool is only extracting a PCB's X & Y design elements & assuming a power & Gnd via inductances.  Due to the 3D nature of current flow across & through a PCB from power & Gnd planes on different PCB layers, a 3D extraction gives a more accurate series inductance estimate needed to more accurately model power & Gnd vias which leads to a more accurate power rail impedance (ZvsF) response

    it would be difficult to comment on reducing the amount of decoupling caps without going through the exercise ourselves.  That said, you can likely prioritize the high-current and sensitive analog rails, then look to share bypass caps when you hit space constraints.  Having decap as close to the BGA as possible will reduce inductance and improve their efficacy (two supply vias with a shared decap would be better than a decap located far away in most circumstances). 

    Please be aware that each PCB design is unique and may need different Dcap scheme to meet recommended PI parameter targets

    Regarding decoupling capacitors, the recommendation is to start with the EVMs decoupling and then optimize (if needed) based on your power simulation results.

    For the placement of the Caps and values, we would still recommend using the EVM as a reference along with the PDN document.

    SK uses an EMI Filter at 1uF, can I replace it with a general ceramic capacitor?

    The SK performance has been tested with 3-T terminal caps.

    You may have to add multiple 2-T caps for each cap and perform simulations to finalize the values.

    (50) [DRA829] SOM Schematic has "NFM15HC105D0G" and "NFM18HC106D0G" - Processors forum - Processors - TI E2E support forums

    (49) TDA4VH-Q1: TDA4VH Power 3T filter capacitor questions - Processors forum - Processors - TI E2E support forums

    PDN application note

    https://www.ti.com/lit/an/sprac76g/sprac76g.pdf

    Regards,

    Sreenivasa

  • Hi Board designers, 

    PMIC capacitor and feedback recommendations

    PMIC - feed back and jumper or 0R provisioning 

    PMIC input capacitor connection recommendation:

    Application note TPS65219 Schematic, Layout Checklist

    Regards,

    Sreenivasa

  • Hi Board designers,

    Refer below inputs for PMIC power sequencing.

    AM6421: Sudden Loss of Power Impact on Power Down Sequence

    (+) AM6421: Sudden Loss of Power Impact on Power Down Sequence - Processors forum - Processors - TI E2E support forums

     As stated in the AM64x datasheet, "The potential applied to VDDR_CORE must never be greater than the potential applied to VDD_CORE + 0.18V during power-up or power-down. This requires VDD_CORE to ramp up before and ramp down after VDDR_CORE when VDD_CORE is operating at 0.75V". AM64 was characterized under operating conditions so we cannot guarantee the expected operation beyond the conditions specified in the datasheet. PCB designers are responsible for validating and characterizing the SoC under specific use case conditions to confirm it meets the application system level requirements. 

    Handling uncontrolled power-down requires additional considerations in the design like adding additional input capacitance or a discrete supervisor to monitor voltage at the power source and trigger an OFF request before PMIC loses power. Here is an example FAQ for reference: https://e2e.ti.com/blogs_/b/powerhouse/posts/how-to-meet-power-sequencing-requirements-with-a-pmic.

    Another option to consider to mitigate the sequencing concerns during uncontrolled power-down is running the main CORE at 0.85V which allows to combine VDD_CORE and VDDR_CORE together. In this scenario both rails are supplied by the same PMIC DCDC regulator.

    Regards,

    Sreenivasa

  • Hi Board designers,

    Information related to open drain GPO

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Inputs related to user programmable PMIC 

    In case User-programmable power management IC (PMIC) is required, TPS6521905 with three step-down DC/DC converters and four LDOs can be considered.
    Dynamic scaling of supplies is not allowed for the processor family.

    https://www.ti.com/product/TPS6521905

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Refer below input related to eFuse caps and pinout

    TPS22918 5.5-V, 2-A, 52-mΩ On-Resistance Load Switch

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Refer below input related to PMIC selection

    (+) AM625: AM625 compatible PMIC options - Processors forum - Processors - TI E2E support forums

    AM625: AM625 compatible PMIC options

    1. As stated in the datasheet, unfortunately TPS6521903 is only qualified for -40°C lower limit storage temperature. This will not meet the -55°C requirement. 

    2. TPS6522005-EP is the extended performance device within the same family, this is qualified for -65°C lower limit.

    Yes, this device can be compatible with AM625. TPS6522005-EP is a user-programmable device, so the settings come as a blank configuration.
    The configuration can mirror that of the TPS6521903 configurations to be compatible with AM625.
    NVM programming details can be found in this document: https://www.ti.com/lit/pdf/SLVUCM5

    Regards,

    Sreenivasa 

  • Hi Board designers. 

    Application noted for using PMIC with AM62x family of processors

    Powering the AM625SIP With the TPS65219 PMIC app note 

    https://www.ti.com/lit/an/slvafp8/slvafp8.pdf

    Powering the AM62x with the TPS65219 PMIC

    https://www.ti.com/lit/an/slvafd0c/slvafd0c.pdf

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Inputs related to power supply slew

    (9) AM6548: Confirmation on slew rate - Processors forum - Processors - TI E2E support forums

    Per the datasheet for the AM6548, the maximum slew rate is recommended to be less than 100 mV/µs for supplies in general, and less than 40 mV/µs for the VDDA_1P8_SERDES0 supplies. Alternatively, the slew time must be greater than the supply value x 10µs, and greater than supply value x 25µs, respectively.

    image.png

    Just to confirm, this slew rate does apply for both rise and fall times?

    The max power supply slew rates requirement defined in the datasheet only applies when the power rails are ramping up. The ESD circuits implemented on the power rails may false trigger, clamping the power rails to VSS if the power rails ramp too fast.

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Inputs related to load switch slew rate control, QOD and output cap.

    https://www.ti.com/lit/ds/symlink/tps22918.pdf

    9.2.2.1 Input Capacitor (CIN)
    To limit the voltage drop on the input supply caused by transient in-rush currents when the switch turns on into a
    discharged load capacitor or short-circuit, a capacitor needs to be placed between VIN and GND. A 1 µF ceramic
    capacitor, CIN, placed close to the pins, is usually sufficient. Higher values of CIN can be used to further reduce
    the voltage drop during high-current application. When switching heavy loads, it is recommended to have an
    input capacitor about 10 times higher than the output capacitor to avoid excessive voltage drop.

    9.2.2.2 Output Capacitor (CL) (Optional)
    Becuase of the integrated body diode in the MOSFET, a CIN greater than CL
    is highly recommended. A CL
    greater than CIN can cause VOUT to exceed VIN when the system supply is removed. This could result in current
    flow through the body diode from VOUT to VIN. A CIN to CL
    ratio of 10 to 1 is recommended for minimizing VIN
    dip caused by inrush currents during startup.

    8.3.2 Quick Output Discharge (QOD)

    https://www.ti.com/lit/ds/symlink/tps22965.pdf

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Inputs related to load switch implementation using FET

    FET based switch implementation for peripheral supply control

    General implementation 

    Can cause reverse voltage to be applied during power cycle 

    Recommended implementation 

    Note: Verify the slew rate requirement for the connected peripherals 

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Inputs related to load switch implementation

    https://www.ti.com/lit/ds/symlink/tps22965.pdf

    10.1.2 Input Capacitor (Optional)
    To limit the voltage drop on the input supply caused by transient inrush currents when the switch turns on into a
    discharged load capacitor or short-circuit, a capacitor needs to be placed between VIN and GND. A 1-µF ceramic
    capacitor, CIN, placed close to the pins, is usually sufficient. Higher values of CIN can be used to further reduce
    the voltage drop during high current applications. When switching heavy loads, it is recommended to have an
    input capacitor about 10 times higher than the output capacitor to avoid excessive voltage drop.

    10.1.3 Output Capacitor (Optional)
    Becuase of the integrated body diode in the NMOS switch, a CIN greater than CL is highly recommended. A CL
    greater than CIN can cause VOUT to exceed VIN when the system supply is removed. This could result in current
    flow through the body diode from VOUT to VIN. A CIN to CL ratio of 10 to 1 is recommended for minimizing VIN dip
    caused by inrush currents during startup; however, a 10 to 1 ratio for capacitance is not required for proper
    functionality of the device. A ratio smaller than 10 to 1 (such as 1 to 1) could cause slightly more VIN dip upon
    turn-on due to inrush currents. This can be mitigated by increasing the capacitance on the CT pin for a longer
    rise time (see the Adjustable Rise Time section).

    Regards,

    Sreenivasa

  • Hi Board Designers, 

    Inputs related to LDO selection and transient response

    (+) TLV757P: Load transient response for 400mA load transient - Power management forum - Power management - TI E2E support forums

     see the below load transient response 

    image.png

    The load transient expected is 400mA

    Would the voltage transient for 400mA be less than 1A (meaning lesser voltage variation)

    Reference LDO - TLV75518.

    The use case is to program eFuse array for Sitara AM62x family.

    The starting current can almost assumed to be near to zero.

    In this use case you can expect the maximum voltage dip during the transient to be lower. I have attached a measurement simulating this use case.

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Inputs related to PMIC use case 

    have a question about PDN design for processor. Is it possible not to use  PMIC? Can I use a bunch of simple DCDCs instead? I just could like to simplify my design.

    That is possible but not recommended.  The processor has been tested with the PMIC, and thus has validated its load step response, noise levels, power rail sequence control, etc. with the processor.  I'm not sure using a bunch of discrete supplies and sequencer would be simplified. 

    You need to ensure the discrete power architecture follows the power sequence as per processor-specific data sheet, provides the required delay before asserting the processor warm reset input after the supplies ramp, sizing of the supply as per max current application note,  follow the slew rate requirements, supports residual voltage detection and allows powering the PMIC after the power supplies ramp down to <300mv

    Regards,

    Sreenivasa

  • Hi Board Designers,

    PMIC LDO input or output connection when not used 

    Regards,

    Sreenivasa 

  • Hi Board Designers,

    Information related to delay between supplies:

    (+) [FAQ] AM625: what is the specific delay time requirement between the different power rail? - Processors forum - Processors - TI E2E support forums

    [FAQ] AM625: what is the specific delay time requirement between the different power rail?

    We do not have any time specified between 2 supplies except that the previous supply needs to be ramped and stable before the start of the next supply ramp.
    No specific timing requirements. The sequence is required only to prevent potential differences.

    The delay between these two power rails ramping down is not important. The device has a power-up and power-down sequence requirement to ensure potential differences between power rails.

    The primary concern is the potential difference between VDD_CORE and VDDR_CORE, where VDDR_CORE must never be greater than the potential applied to VDD_CORE + 0.18V during power-up or power-down.

    (+) AM6422: Power up / Down sequencing - Processors forum - Processors - TI E2E support forums

    There is only one firm requirement for AM64x power-down. See note 5 associated with the power-down sequence. 

    The potential applied to VDDR_CORE must never be greater than the potential applied to VDD_CORE + 0.18V during power-up or power-down. This requires VDD_CORE to ramp up before and ramp down after VDDR_CORE when VDD_CORE is operating at 0.75V. VDD_CORE does not have any ramp requirements beyond the one defined for VDDR_CORE. VDD_CORE and VDDR_CORE are expected to be powered by the same source so they ramp together when VDD_CORE is operating at 0.85V.

    (+) AM6548: Confirmation on slew rate - Processors forum - Processors - TI E2E support forums

    The max power supply slew rates requirement defined in the datasheet only applies when the power rails are ramping up. The ESD circuits implemented on the power rails may false trigger, clamping the power rails to VSS if the power rails ramp too fast.

    Are there any requirements on the slew rate for fall times?

    No.

    We are basically allowing the IO supply to delay their turn-off until the last core supply is turned off. The previous power-down diagram showed the IO supplies being turned off by the time VDD_CORE was turned off. This is still the preferred sequence, if possible, to help prevent the IOs from doing unpredictable things during power-down since logic in the core domain controls the IO functions. However, we found this was difficult to implement and decided the internal circuits that force the IOs to a known state until VDD_CORE ramps-up should perform a similar task during power down when VDD_CORE is lost before the IO supply. We do not want customers leaving IO supplies powered for long periods of time after the VDD_CORE is turned off, so we decided to extend each IO supply turn off until the last core rail is turned off as way to limit the time IO are turned on after VDD_CORE is turned off.    

    It appears you are showing an uncontrolled power-down sequence where all supplies are turned off at the same time, which is consistent with the new power-down diagram as long as you ensure the potential applied to VDDR_CORE is never greater than the potential applied to VDD_CORE + 0.18V during power-up or power-down. This is the only absolute voltage difference that must be managed during power-down.

    All power rails must be turned off and decay below 300mV before initiating a new power-up sequence anytime a power rail drops below the minimum value defined in Recommended Operating Conditions. The only exception is when entering/exiting Partial IO low power mode with VDDSHV_CANUART and VDD_CANUART sourced from an always on power source. For this use case the VDDSHV_CANUART and VDD_CANUART power rails are allowed to remain on.

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Information related to supply sequence:

    (+) AM623: Reference Design Questions - Processors forum - Processors - TI E2E support forums

    In this power up sequence, the first power supply to come up is the 3.3V from the power switch on top (TPS22965). In the reference design, this 3.3V is used to power peripherals on the dev board which may apply a signal or pull-up GPIO pins on the AM623 before the rest of the power supplies are up. would this cause an issue? should we separate the 3.3V power supply to a 3.3v switched to power peripherals (including the Ethernet PHYs) after VDD_CORE is stable?

    Most of the processor IOs are not fail-safe. As noted in our design collateral, we recommend using the same regulator for the IO supply of the SoC (i.e VDDSHVx) and the IO supply of the external peripheral. This will help prevent having a voltage on a digital pin while its corresponding IO supply is not powered. Regarding your question about the clock buffer, please follow our EVM implementation. 

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Information related to voltage feed.

    (+) AM623: TPS6521901RHBR Power Management IC (PMIC) is not working properly. - Power management forum - Power management - TI E2E support forums

    AM623: TPS6521901RHBR Power Management IC (PMIC) is not working properly.

    Depending on the specific voltage domains affected by the backfeeding, the issue could violate the SoC sequence requirements, stress IOs that are not fail-safe, affect internal ESD diodes, etc etc. It is challenging to guarantee all the specific consequences when the SoC has not been fully tested and validated for that kind of spec violation faults.  

    (+) SK-AM62B-P1: TPS6521904 – No BUCK outputs after power-up on custom board - Processors forum - Processors - TI E2E support forums

    I am sharing the captured sequences here:
    Yellow-VSYS
    Green-EN
    Blue-GPO2

    (+) AM625: VDD_Core Changing Voltage using TPS65219 - Processors forum - Processors - TI E2E support forums

    Dynamically changing the VDD_CORE or any other fixed SOC supply voltages after the reset is released is not allowed or recommended.

    Please refer below FAQ:

    [FAQ] AM625 / AM623 / AM620-Q1 / AM62Ax / AM62Px / AM62D-Q1 / AM62L / AM64x / AM243x Design Recommendations / Custom board hardware design – Dynamic Voltage Scaling for SOC core (VDD_CORE), Peripheral Core and Analog supplies - Processors forum - Processors - TI E2E support forums

    Regards,

    Sreenivasa