Browse By Tags

  • OPA2626: opa2626

    Part Number: OPA2626
    Other Parts Discussed in Thread: OPA2376

    Tool/software:

    Does TI use a new logo to replace the original logo? It seems the original map is not used.

      

  • PCM2903C: PCM2903C Low Pass Filter on Line in / out

    Part Number: PCM2903C
    Other Parts Discussed in Thread: OPA2353, , OPA1662, OPA2376

    Tool/software:

    PCM2903C EVM schematic shows OPA2353 Op Amp for low pass filters.

    Could we use OPA1662 instead since the price is much lower?

  • OPA2376: How much current can the OPA2376 source and sink?

    Part Number: OPA2376
    Other Parts Discussed in Thread: OPA376

    Tool/software:

    Hello, I am planning on using the OPA2376 and would like to know where in the datasheet it specs out output current?

    Could I use the Short-circuit current Isc spec found on page…

  • OPA2387: Internal circuit Diagram of the component

    Part Number: OPA2387
    Other Parts Discussed in Thread: OPA387, ADS1299, OPA397, OPA2392, OPA2376, OPA2391, TLV2376

    Tool/software:

    Hello,

    we are designing a EEG Device ,where the device is suitable for EEG device as pre amplifier in AFE. And also please…

  • OPA2376: When there is no input, the output voltage is abnormal

    Part Number: OPA2376

    Tool/software:

    Dears,

    The schematic diagram is as follows:

    when the differential input is 0, there is an output voltage of 1-2mV (the output voltage has been subtracted by 0.55V-B voltage), with a significant deviation. Assistance…

  • OPA2376-Q1: Vos range of TA = –40°C to +125°C

    Part Number: OPA2376-Q1
    Other Parts Discussed in Thread: OPA192, OPA2376, OPA388-Q1, OPA387

    Hi Expert,

    Do we have a Vos range of TA = –40°C to +125°C?

    BR,

    Link

  • OPA2376: Need a Dual source Amp

    Part Number: OPA2376
    Other Parts Discussed in Thread: OPA2392, OPA2325, OPA2397

    I need to replace the OPA2376AIYZDR for a dual source amplifier with similar parameters (Noise, offset, rail to rail, drift, etc). My main request is the size. Would you have…

  • OPA2376: Searching for 6 channels device

    Part Number: OPA2376
    Other Parts Discussed in Thread: OPA4376

    Hi Team,

    Do we have such device like OPA2376 but have 6 channels? Or do you have other suggestions to achieve such function?

    BRs,

    Francis

  • OPA2376: Application issues of chips

    Part Number: OPA2376

    May I ask if I use the OPA2376 operational amplifier and connect it to a follower for use, and expect to output 1V? Why does the voltage value measured when the output terminal is connected to a 0 ohm resistor cause oscillation? Switching…

  • OPA2376: I need spice model to execute in the LTspice software.

    Part Number: OPA2376

    Hi Team,
    Greetings!

    Kindly share us the LTspice model this OPA2376AIDR.

    Regards!
    Poornima D

  • OPA2376: Minimum Short Circuit current

    Part Number: OPA2376

    Hi Folks,

    Do we have an idea on what the minimum short circuit output current would be?

    Thanks,

  • LMC6482: Device alternative

    Part Number: LMC6482
    Other Parts Discussed in Thread: OPA2191, OPA2196, OPA2376, OPA2186, OPA2990

    Hi Team,

    Good day. 

    I am looking for a pin for pin alternative for LMC6482. The closest device that I found was OPA2196 and OPA2191. However, these devices are…

  • OPA2180: recommended alternative product

    Part Number: OPA2180
    Other Parts Discussed in Thread: OPA2377, OPA2376, OPA2188, , OPA2325, OPA2397, OPA2392, OPA2387, OPA2182, OPA2187, OPA180, OPA188

    Hi experts, 

    Q1. Could you please tell me your recommended devices that is alternative to OPA2377AIDGKR…

  • OPA2376: Is this the best replacement for LMV821

    Part Number: OPA2376
    Other Parts Discussed in Thread: OPA1611, OPA1612, OPA397, OPA376

    Hello, I am currently using the LMV821 as a microphone Preamp but it has a noisy output. I was looking into a fully differential opamp or a low noise opamp as potential…

  • TIDA-00445: Input common mode

    Part Number: TIDA-00445
    Other Parts Discussed in Thread: OPA2376, AMC1200

    Hi,

    I went for the TIDA-00445 after these specs caught my eyes:

    So I thought it would provide some sort of shunt based AC mains measurement.

    But after reading the document, I found…

  • OPA2376-Q1: measured offset voltage is larger than calculated.

    Part Number: OPA2376-Q1
    Other Parts Discussed in Thread: OPA2376,

    Dear Specialists,

    My customer is evaluated OPA2376 in the customer's circuit, offset voltage is larger than the calculated value.

    I would be grateful if you could advise and make a friendship…

  • TIDA-01525: Max Current Limit in the current mirror

    Part Number: TIDA-01525
    Other Parts Discussed in Thread: OPA2376, OPA2189, OPA2192, CSD22206W, CSD23285F5

    Hi team,


    The figure is the voltage controlled current mirror circuit diagram of TIDA-01525.

    I want to configure Rload be about 3.5V LED within 1…

  • ADS1278-EP: Can I use I resistor divider as a voltage reference input

    Part Number: ADS1278-EP
    Other Parts Discussed in Thread: REF5025, ADS1278, OPA2376, OPA2320, OPA2350, , INA129-EP, INA129

    My analog signal is from a Wheatstone bridge supplied by 10V. I use instrument amplifier to enlarge the signal and set the common voltage…

  • TLV9064: When will TI release any more quad op amps in X2QFN 14-pin packages

    Part Number: TLV9064
    Other Parts Discussed in Thread: OPA4375, OPA4376, TLV6744, TLV6742, , OPA2376, OPA4392, OPA4325, OPA4192, OPA2392

    I am looking for low-noise quad op amps in the smallest packages. Data sheets exist for OPA4375 and TLV6744 but no chips…

  • OPA2376: Does OPA2376 offset voltage become bigger than typical offset voltage spec when input pin (+IN,-IN)voltage is very low?

    Part Number: OPA2376

    Hello guys,

    One of my customers is evaluating OPA2376 with low pass filter circuit like the follow.(But +IN=+100mV, V+=+5V, V-=0V)

    https://www.avrfreaks.net/forum/why-simple-op-amp-low-pass-filter-does-not-work

    The customer parameters…

  • OPA2376: What is the maximum capacitor value can be driven by OPA2376 for low pass filter circuit?

    Part Number: OPA2376

    Hello guys,

    One of my customers is evaluating OPA2376 with low pass filter circuit like the follow.

    https://www.avrfreaks.net/forum/why-simple-op-amp-low-pass-filter-does-not-work

    The customer parameters are the follow.
    R1 = 1k ohm…

  • OPA2376: Supply Missing with Input

    Part Number: OPA2376

    Hi,

    I would like to have a question: What could happen, if the 3.3V supply of OPA2376 is missing, but input is supplied by some 10k Ohm to some volt?

    I am looking forward to your answer!

    Thank you and best regards,

    Ziming

  • OPA2376: Device failure mode and limitation.

    Part Number: OPA2376

    Hello

    According to the data sheet, the absolute rating of the input current to OUT pin is defined as up to 40mA.
    How long can be tolerated if a current about 50mA flows through the OUT pin?

    This is a question for circuit protection…

  • OPA2376: Detail of abnormal behavior concerned with power supply failure

    Part Number: OPA2376

    Hi team!

    Could you please let me know the behavior of your product in following cases?

    Case1:
    The IN+ and IN- pins are entered the signal with Voltage from 0.5V to 5.0V, without power supply. (V+ = V- = GND))
    If the device will be…

  • OPA2376: OPA2376 ESD Rating

    Part Number: OPA2376

    Hello,

    where can I find the ESD rating for HBM and CDM?

    I didn't find anything in the datasheet.

    Best regards

    Basti

1 2 3 4 5 »