Browse By Tags

  • TPS7A84: Alternatives for TPS7A8400 with 0.5/0.6V FB voltage

    Part Number: TPS7A84
    Other Parts Discussed in Thread: TPS7A53B,

    Tool/software:

    Hi team,

    My customer is looking for an alternatives to replace with TPS7A8400.

    And the LDO should have the similar Vin range, and 3A output current capability.

    But the FB voltage…

  • TPS7A84: how to set to 0.8Vout if not using any-out function

    Part Number: TPS7A84

    Tool/software:

    Hi Team, 

    just want to check how to set Vout to 0.8V if not using any-out function? Thanks. 

    BRs

    Given 

  • TPS7A84: TPS7A8400RGRT CTE value for VQFN

    Part Number: TPS7A84

    Tool/software:

    Hello,

    Can someone please provide the CTE for this component package? 

    thank you

  • TPS7A84: Except the output voltage range, is there any characteristics differences between ANY-OUTPUT and resister programming

    Part Number: TPS7A84

    Tool/software:

    Dear team,

    Except the output voltage range, is there any characteristics differences between ANY-OUTPUT and resister programming.

    Like the transient response, power dissipation....etc

    Best regards,

    Hank Lin

  • TPS7A84: parallel to achieve 5A

    Part Number: TPS7A84
    Other Parts Discussed in Thread: TPS7A57, , TPS7A85A

    Dear BU friends,

    Could we support TPS7A84 parallel to achieve 5A application. Customer prefer TPS7A84 due to the setting voltage is convenient for customer.

     

  • TPS7A84: TPS7A8400 ENpin max voltage

    Part Number: TPS7A84

    Hi team, 

    I found that in datasheet, EN should be lower than VIN? What's the consideration here? Can custoemr pull up VIN to 1.8V and pull up EN to 3.3V?

    Nison

  • TPS7A84: Do we have low iq LDO with SNS?

    Part Number: TPS7A84

    Hi Teams,

    My customer is using TPS7A84 which has Remote sns for ATE application. But the Iq of TPS7A84 is 2.8mA, which is too large for the system. Do we have low iq LDO parts to meet this requirement?

    BRs,

    Marsh

  • TPS7A84: TPS7A84 --- feedback resistors

    Part Number: TPS7A84

    Hello Experts,

    Refer Table 8.5 for feedback resistor values for setting the output voltage.

    Can R1 be 6800 ohm and R2 vary from 30k ohm to 130 kohm (using a I2C potentiometer)? The resultant output voltage can change between 0.84V…

  • TPS7A84: Wrong output voltage

    Part Number: TPS7A84

    I would like to know what, if anything, I need to check to correct the output voltage of this regulator.

    Vin is 5.1V

    Vout = Vin = 5.1V .  ANY-OUT is configured for 3.3V.

    The IC is configured identically to Figure 8-2 in the datash…

  • TPS7A84: Overload protection

    Part Number: TPS7A84

    Hi team, 

    may I know the operation of TPS7A84 when it’s output current exceeds the limitation? How TPS7A84 operates to protect the device from damage? And the protection is auto-retry or latchup? What the kind of overcurrent protection…

  • TPS7A84: 40mA reverse sink current

    Part Number: TPS7A84

    Hi Team,

    ZTE uses TPS7A8401A, and they have some question when using this part.

    Test condition: Vin=3.3V, Vout=2.5V, Iout=0.5A; RFB_up=30.1k, RFB_bottom=7.44k, cff=0.01uF

    After the LDO normally outputs 2.5V, the load will have a reverse…

  • 低ノイズと低リップルを重視した設計手法を活用し、パワー インテグリティ (電力品質) とシグナル インテグリティを強化する方法

    Other Parts Discussed in Post: TPSM82912, TPS7A94, TPSM82913, TPS62913, TPS62912

    医療用アプリケーション、試験 / 測定、ワイヤレス インフラなどの分野には、クロック、データ コンバータ、アンプを使用し、ノイズの影響を受けやすいシステムが多く存在します。それらのシステム向けの電源を設計するエンジニアは、精度の向上や、システム ノイズの最小化という共通の課題に直面します。「ノイズ」という用語は人によって意味が異なりますが…

  • 如何以低雜訊和低漣波設計技術強化電源與訊號完整性

    Other Parts Discussed in Post: TPSM82912, TPS7A94, TPSM82913, TPS62913, TPS62912

    德州儀器作者: Steve Schnier

    在為醫療應用、測試與量測及無線架構等使用時脈、資料轉換器或放大器的雜訊敏感系統設計電源供應器時,提升準確度和精密度及減少系統雜訊是工程師的共同挑戰。雖然每個人對「雜訊」一詞的定義不盡相同,但本文中我會將雜訊定義成由電路中電阻器和電晶體所產生的低頻率熱雜訊。  您可透過頻譜雜訊密度曲線 (單位為微伏特…

  • 저잡음 및 저리플 설계 기술로 전력 및 신호 무결성을 향상시키는 방법

    Other Parts Discussed in Post: TPSM82912, TPS7A94, TPSM82913, TPS62913, TPS62912

    정확도와 정밀도를 높이고 시스템 잡음을 최소화하는 것은 클록, 데이터 컨버터 또는 증폭기를 사용하는 의료 애플리케이션, 테스트 및 측정, 무선 인프라를 위한 잡음에 민감한 시스템을 위한 전원 공급 장치를 설계하는 엔지니어들이 흔히 마주하는 과제다. "잡음"이라는 용어는 사람마다 다른 의미를 가질 수 있지만…

  • TPS7A84: VFB accuracy

    Part Number: TPS7A84
    Other Parts Discussed in Thread: TLV767

    Hi,

    Could you help share the accuracy of the feedback voltage? Thanks.

    Zach

  • TPS7A84: TPS7A84: FB have a overshoot and undershoot when VIN power off

    Part Number: TPS7A84
    Other Parts Discussed in Thread: TEST2

    Hi team,

    This is FAE Jayden, my customer use TPS7A8401, there is a fault that needs help to confirm:

    Application: 3.6Vin~3.3Vout, Vout adjusted by using external FB resistors; When Vin power off…

  • TPS7A8300: The difference between TPS7A8300 and TPS7A8400

    Part Number: TPS7A8300
    Other Parts Discussed in Thread: TPS7A84

    Hi BU team,

    What's the difference between TPS7A8300 and TPS7A8400? Which one do you recommend for powering the clock chip? Thanks.

    Regards,

    Charlie

  • TPS7A84: TPS7A8400ARGRT charge pump

    Part Number: TPS7A84

    Hi team,

    The application I'm designing now is EMI demanding, so I'd like to reduce the noise as much as possible.

    Question 1. Does charge pump noise appear on the VIN side as well?
    Question 2. Is it better to use a ferrite…

  • TPS7A53: is there comparison between TPS7A53 and TPS7A57 and TPS7A84?

    Part Number: TPS7A53
    Other Parts Discussed in Thread: TPS7A57, TPS7A84,

    Hi Team, 

    Is there comparison between TPS7A53 and TPS7A57 and TPS7A84?  Thanks. 

    BRs

    Given 

  • TPS7A84: SCH review

    Part Number: TPS7A84

    Hi team

     

    this is my customer SCH  could you help me to review it ?

     

    because I will LOA next week 

     

    can you reply this week?

     

    there are

     

    one TPS7A8401 in page3

     

    total 3 

    in attached files 

     

    BRs

     

    brian

    3240.New_schematic_Power_20230309_B…

  • TPS7A84: will 1.3V voltage backflow at the output port affect the chip function?

    Part Number: TPS7A84

    Hi team,

    I am Jayden, the customer I support used TPS7A8400RGRR. There is one thing need to be confirmed with team in application.

    • When the TPS7A8400RGRR (3.6V to 3.3V ) is not working, there is a 1.3V voltage backflow at the output…
  • TPS7A84: TPS7A84

    Part Number: TPS7A84

    we buy the part#TPS7A8400ARGRR with date code year21 week05 ( 2105) & MSL LEVEL 2. But the MSL level is level1 showed in date sheet published in Sept 2021, and the it showed level 2 in data sheet published in Feb 2017, so could you…

  • TPS7A8300: Voltage Leak At Output Before LDO is ON

    Part Number: TPS7A8300
    Other Parts Discussed in Thread: TPS7A85, TPS7A84

    Hi TI Team,

    I have a question on TPS7A8300

    We have power supply rail as above.

    First of all the 1.5V is output from buck converter, and then ANALOG_0.9V is enabled before ANALOG_1…

  • TPS7A8300: Difference between TPS7A8300RGRT and TPS7A8400RGRT

    Part Number: TPS7A8300
    Other Parts Discussed in Thread: TPS7A84

    Hi,

    We are considering replacing TPS7A8300RGRT with TPS7A8400RGRT.

    ○ Output current… TPS7A8300 2A [Max], TPS7A84 3A [Max]

    I think these two parts are pin compatible, but are they…

  • TPS7A84: LDO current rating

    Part Number: TPS7A84
    Other Parts Discussed in Thread: TL1963A-Q1, TPS74301, LM1086, LM317

    Hi Experts,

    When looking at the LDO thermal resistance, they are the same between TPS7A83/84/85. Then how do i choose the LDO based on input/output voltage and current…

1 2 3 4 5 »