Browse By Tags

  • RE: RE: two XTR116 with non isolated power supply

    Hi Shrikant,

    1. Please attach a schematic.

    2. The error in output current could be because of the ohmic tolerence of the resistor in series with pin 2 (Iin) of the XTR116.

    3. Using two diodes in series might not be a good idea to drop voltage from 5V…

  • RE: XTR116 PIC18F46K22 DAC

    Hello User,

    We'll need to read through the PIC datasheet to understand if it will properly interact with the XTR116. 

    While we're reviewing the MCU, please provide a more complete schematic of the PIC that shows how you intend to power the VCC/GND…

  • RE: 3 way isolation for field interface modules

    Dear Collin,

    Thanks for the quick and valuable reply.

    I will go through these datasheets and try to build a schematic which will satisfy my requirements. I will get back to you with upadate on this.

    Also I forgot to update you on our last discussion regarding…

  • RE: XTR116 and PIC16F877 PWM Connection

    Hi Collin,
    Thank u so much for answer.

    1) I feed system from a single source (Vloop). I did circuit isolation. But I'm using the ground of Vloop sources. So I'm using as of the system GND. Does theproblem ? Or how I'm gonna use ?

    2) What is…
  • Interfacing XTR116 with DAC0808

    Other Parts Discussed in Thread: DAC0800, DAC0808, XTR116, ISO7641FC, DAC7311, ISO1541, DAC7571

    I have an application which need to convert a binary value 0-255 to a 4-20 mA signal. I would like to do this using a XTR116 and DAC0808 or DAC0800 d/a converter…

  • RE: EMI XTR116

    Hello Magne,

    Please take a look at one of our "CerTIfied" precision reference design, TIPD126, that provides radiated immunity testing data using the XTR117 current loop transmitter.  The XTR117 is very similar to the XTR116 but without the internal…

  • XTR116 and PIC16F877 PWM Connection

    Other Parts Discussed in Thread: XTR117, XTR116, XTR111

    Hi Everyone,

    I did the conversion 0-5V 4-20ma convert with XTR 116. Circuit schema like in the photo. I want to use PIC16F877 instead of potentiometers. Using PWM want to get to 4-20. But I don't…

  • XTR116 PIC18F46K22 DAC

    Other Parts Discussed in Thread: XTR116, XTR111, XTR115

    Hi everyone,

    XTR116 integrate , I would like to include in my circuit. My processor is 18f46k22. I'm gonna use the DAC pin of the processor. I made a connection like that in the picture. Is this…

  • How to convert linear resistance to 4-20mA using XTR115 ?

    Other Parts Discussed in Thread: XTR116, XTR115

    I'd like to hear from anybody familiar with XTR115 or XTR116 on their recommendations how to convert 0-1000 Ohm linear resistance to 4-20mA...

    Any circuit ideas or schematic examples other than going…

  • Current Transformer to 4-20 mA

    Other Parts Discussed in Thread: XTR116, XTR115

    Hello,

    I am trying to convert CT (Current transformer) output AC current to 4-20mA loop powered output. I have to convert CT's output AC current to AC voltage (using a shunt resistor). Does the XTR115 or…

  • Re: 4-20mA variable output

    Hello Alan,

    Thank you for your question, and welcome to the TI E2E forums!

    The simplest way to achieve 4-20mA out with a resistance pot at the input would be by using the XTR115 or XTR116, since both parts have an internal voltage reference that could be…

  • RE: xtr116 performance below 1mA

    Hello Kris,

    This is an interesting application, could you provide some information about what type of sensor it interacts with as well as what type of control equipment the 250uA - 450uA output is connected to?  We can start a private conversation if you…

  • RE: xtr116 performance below 1mA

    Hello,

    We reviewed the product datasheet and agree that there doesn't appear to be any limiting factors for operating the device in this limited low output current range.  However, to be sure we setup the circuit in the lab and configured it for a…

  • RE: XTR116 ESD Rating

    The ESD ratings of the XTR116 are:

    Human Body Model: 2000V

    Machine Model: 300V. 

  • xtr116 performance below 1mA

    Other Parts Discussed in Thread: XTR116

    I'm looking to implement a low-power 2-wire current loop where my signal current will range about 250uA to 450uA (not 4-20mA) using the XTR116. 

    The data sheet seems to say the xtr116 can do this under these conditions…

  • RE: xtr116 performance below 1mA

    Hello Kris,

    Yes, the blue trace uses the transistor internal to the XTR116.  

    Perhaps the discrepancy with/without the transistor is simply due to the polarity of the bias currents and/or offset voltage in the circuit and depending on the device one may…

  • XTR116 ESD Rating

    Other Parts Discussed in Thread: XTR116

    Hi,

    What is the ESD rating of the XTR116 current loop transmitter?

    Thanks!

  • XTR116 TINA Simulation Model

    Other Parts Discussed in Thread: XTR116, XTR115, TINA-TI

    Hi Dear TI and Other Forum Members,

    I am new to TINA.I could not find a model for XTR116 or XTR115 which I wanted to simulate.

    I am also worried about why is this component model not put in

    "…