Other Parts Discussed in Thread: XTR116, ADS1232
Tool/software:
I'm using a PGA308/XTR116 to convert a strain gauge output into 4-20mA.
Measuring the bridge voltage directly and calculating my offsets and gains seems to work well…
Tool/software:
Hello All,
Please refer below link for the last communication for the same issue.
xtr116-dac-out-to-4-to-20ma-conversion
Now simulation is working fine with the given voltages of Vin: 0.1752V - 3.0998V ---- Iout: 4…
Tool/software:
Hi,
The partially filled failure analysis report is herewith attached. Please go through the document for the problem.
Look forward to hearing from you.
Best Regards…
Tool/software:
Hello,
I am going to use XTR116 this IC and I am procuring RDL 4-20mA Current Loop Transmitter XTR116U with Analog Input from Amazon Web, for prototype.
My application is I want to convert STM32L151C8T6A DAC out voltage…
Regarding output Vref
spec sheet describes parameters (under test condition column) where Iref = 0 to 2.5mA
I wish to source current up to 3.8mA to increase my bridge circuit sensitivity.
is this recommended and what are my limitations…
How will this component do if someone shorts the 24v wire with the current return wire, during operation? Will the component be damaged? And lets say that the reference design has been implemented.
Will there be damage to the device…
Hi,
As I looked through the latest datasheet of XTR116 (SBOS124B – JANUARY 2000 – REVISED JUNE 2023) , the minimum operating temperature has been changed from -55C to -40C. I'm pleased to know if the construction of the IC has been…