Browse By Tags

  • XTR117: XTR117 , 4-20mA current

    Part Number: XTR117
    Other Parts Discussed in Thread: INA333, XTR111, XTR300, XTR116, DAC8551

    Hi all,

     The plan is to read a digital sensor and send out 4-20mA signal out.

    So I'm using the DAC to convert the digital signal to analogue and trying to use…

  • XTR116: What additional components are absolutely necessary & any project advice :)

    Part Number: XTR116
    Other Parts Discussed in Thread: XTR115, XTR111

    Hello!

    I made the silly mistake of ordering a XTR116 without properly reading the datasheet and now i have no external transistor which i definitely need.

    Im struggling to understand…

  • OPA551: opa551 VS opa552

    Part Number: OPA551
    Other Parts Discussed in Thread: OPA552, OPA454, OPA2991

    Hi,

    The OPA551 and OPA552 are two high voltage amplifier but one is unity-gain stable and the second is optimized for gains of 5 or greater.

    What's the difference between unity…

  • XTR117: DAC16 channel XTR117 or XTR116 signal connections.

    Part Number: XTR117

    Dear XTR and DAC Team,

    Can you help me with the identification of the Iret pin isolation component for the below details.

    Regards

    Wasim

  • XTR116: The TINA TI design model of XTR116 (4 to 20 mA loop Analyzer) is not working as espected from library of TINA software

    Part Number: XTR116
    Other Parts Discussed in Thread: XTR115

    Hello,

    Is it possible to get the TINA TI spice model for XTR116. I have tried with below 4-20 mA Loop Analyzer but it is not working as expected. I tried with 500mv and 800mV input voltage…

  • XTR115: About the case of connecting without RL

    Part Number: XTR115
    Other Parts Discussed in Thread: XTR116

    Hello,

    If the customer supplies 24V and connects without RL, does it output 4-20mA without breaking?
    (The customer wants to know what happens if both ends of the RL are shorted due to a mistake…

  • XTR116: XTR116 limited output

    Part Number: XTR116

    XTR116

    Problem 1. Can't get full range output only 4-12mA. Input PT1000. Supply 12 to 24 Vdc.
    Problem 2. Can't get relay to operate or adjust relay setpoint.

    I can send layout, but it can't be public available.

  • RE: XTR115: Inquiry about New product and ESD

    Hello Michael,

    Currently, we do not have another product with equivalent functionality to the XTR115/XTR116/XTR117 family of 2-wire current transmitters.

    Figure 4 of the datasheet has a basic protection circuit.

    A protection scheme for the XTR115/XTR116…

  • RE: XTR105: Support on understanding possible ground loop with XTR105 + Arduino Dues

    Hello,

    The XTR105 is a 2-wire 4mA to 20mA current transmitter incorporating current sources, analog front-end instrumentation amplifier (providing gain) and linearization circuitry intended to interface directly with RTD temperature sensors (without a…

  • RE: XTR117: 4-20mA to 0-3.3V converter

    Hello Neel,

    -What type of current transmitter is required? 2-wire or 3-wire?

    -What type of temperature transducer are you using (RTD, thermistor, thermocouple)?

    -Are you referring to an ADC with I2C or SPI interface on the receiver side? 

    The XTR115, XTR116…

  • RE: WEBENCH® Tools/XTR116: XTR116

    Hello Sumit,

    You can add a trimpot to R1+R3 and R4+R5. The R4+R5 resistors divides the voltage output of the DAC into the input current, and the R1+R3 resistors add a 40uA offset to the input current. Both The Vout range of the DAC in the TIPD190 example…

  • WEBENCH® Tools/XTR116: XTR116

    Part Number: XTR116
    Other Parts Discussed in Thread: TIPD190

    Tool/software: WEBENCH® Design Tools

    I am using XTR116U/2K5 device for getting 4 - 20mA output current.

    I have seen the reference design TIPD190.

    I would like to know - Which resistor we can…

  • RE: XTR106: Iret pins tied together if Loop - pins are isolated?

    Hi Katlynne,

    I tried writing some equations, but when I went back and read your analysis again, it really helped that it was just first-principles of opamps! I agree, the negative feedback will try to drive the voltage difference between the inverting…

  • RE: XTR106: Iret pins tied together if Loop - pins are isolated?

    Hi Paul,

    Can you draw a schematic with what you are proposing. Using this block diagram of the XTR116 as an example (no load connected), the voltage across R1 is seen at the non inverting input of the op amp, and the voltage across R2 is seen at the…

  • RE: XTR115: TXR115 5V voltage ripple and loop current ripple

    Hi Frank,

    The 5V Regulator can only source current approx. 2.5mA or so. What is the output current at 3.3V output? One possibility is that the circuit's load current on Vreg pin exceeds the current limit. 

    XTR115/XTR116/XTR117 are all 2-wire transmitters…

  • [FAQ] What types of applications or end equipment are 4-20mA transmitters used in?

    In what applications are 4-20mA transmitters used? What types of end equipment are 4-20mA transmitters a part of? 

  • RE: [FAQ] How do I choose a 4-20mA transmitter?

    Choosing a 2, 3, or 4-wire transmitter depends on how accessible a power supply is to the transmitter, and what type of signal your source is. You can choose to build a discrete 4-20mA transmitter, or use a partially or fully integrated 2-wire or 3-wire…

  • RE: [FAQ] Are there reference designs that can help me build a 4-20mA transmitter?

    To find reference designs leveraging the best in TI technology – from analog and power management to embedded processors, visit https://www.ti.com/reference-designs/index.html. All designs include a schematic, test data and design files.

    I will…

  • [FAQ] Designing with 4-20mA current loop transmitters (XTRs): FAQ links

    This post serves as a landing pad for frequently asked questions that arise when designing with 4-20mA current loop transmitters. Keep in mind that there are other common output current ranges such as 0-20mA or 0-24mA, and the ideas presented in the following…

  • [FAQ] How do I choose a 4-20mA transmitter?

    How do I choose a 4-20mA transmitter? What is the difference between a 2, 3, or 4-wire transmitter and when should I use each?

  • RE: [FAQ] What is a 2-wire 4-20mA current transmitter?

    2-wire transmitters are loop powered devices most commonly used to monitor a remote process with no access to a local supply. Two analog signal wires carry both the analog output signal, and power for the sensor/monitoring circuitry and transmitter. The…

  • [FAQ] What is a 2-wire 4-20mA current transmitter?

    Other Parts Discussed in Thread: XTR117, XTR106, XTR101, XTR112, XTR108, XTR116, XTR115, XTR105, DAC161P997, DAC161S997

    What is a 2-wire 4-20mA current transmitter? How do I use one?

  • [FAQ] What is a 4-20mA current transmitter?

    What is a 4-20mA current transmitter? 

  • [FAQ] Can I use multiple XTR devices if I have multiple DAC outputs or multiple sensors that share a supply and ground?

    Other Parts Discussed in Thread: ISO7340C, ISO7310C

    I have multiple sensors going into a DAC with multiple output channels. Can I use multiple XTR devices to transmit the 4-20mA current signals for each sensor?

  • [FAQ] Are there reference designs that can help me build a 4-20mA transmitter?

    Other Parts Discussed in Thread: XTR105, XTR112, XTR116, XTR117, XTR111, XTR300, XTR305, DAC8771, DAC8775, DAC8760

    Are there reference designs that can help me build a 4-20mA transmitter? Where can I find them?

    How do I incorporate IEC protection into…

1 2 3 4 5 »