Tool/software:
I am MURALI SELVAM from India, Currently I working Audio Project I need reference for below given part number, If you have kindly give me. Thank you.
Tool/software:
I am MURALI SELVAM from India, Currently I working Audio Project I need reference for below given part number, If you have kindly give me. Thank you.
Dear All,
I designed a new Audio Pre-amplifier PCB board in which I use PGA2320 in order to control the volume by a Microcontroller. To test the sound performance, after analyzing the THD+N, frequency response, Slew rate etc ... At…
Hy dear people,
I have again a silly question to which I cannot find an Answer.
How can I dynamically control the output volume on a TLV320DAC3203 (HPL HPR) with digital mics as input?
The datasheet says:
"The level of the…
I intend to use the TLV320ADC5120 with the CC8530 without a host processor in something similar to a PA system. The only issue here is both devices require digital volume control. Does…
Hello - I'm looking for a speaker amplifier with fine volume support, as low as 0.125dB steps or lower. The TAS5717 would be perfect but my application requires an analog audio input…
We were looking to DSP Processor with one Digital audio input, two analog inputs (differential) and one digital output. Aslo MCU inside the chip to drive LCD, Some IOs for Input selection and volume control etc., We found from TI…
Part Number: PCM2707C
hi,
Does PCM2707C support Audio Control from master volume control of windows10 over I2S line? We have a PCM2707 IC on an Evaluation board from MAXIM Integrated but it can't control the volume from Windows.
also what is difference…
Hello,
When doing volume control with the SRC4193 how many bits does it use internally for volume control 32, 64? This is not mentioned in the datasheet.
Thanks;
Leo
grazie.
cerco qualunque cosa mi permetta di comandare da remoto un pga2311 oppure un altro chip di qualità superiore, e per farlo mi serve lo schema elettrico completo, oppure una vostra realizzazione, non mi serve altro in quanto come ho già detto amo…
Hi,
Are you describing a case with single ended input and single ended output?
I plan on using this with differential output from the PCM1794A (monaural mode), in this case the (+) side would be gain controlled from one input and the (-) side would be…
Tool/software: Code Composer Studio
Need it to Interface it with MSP430G2955 with PINS connected as follows:
Frame -> P2.2
SCLK -> P3.3/UCB0CLK/UCA0STE
RST/LBM -> P4.1/TB0.1/CA1…
Tool/software: Code Composer Studio
Need it to Interface it with MSP430G2955 with PINS connected as follows:
Frame -> P2.2
SCLK -> P3.3/UCB0CLK/UCA0STE
RST/LBM -> P4.1/TB0.1/CA1…
Hi,
I plan to add volume control using a digipot in feedback path of LM4819. Is this a good option or is there a better alternative?
The amplifier gain would be less than 10 so as per datasheet Cf is not required across the digipot…
Hi,
I have the TAS5766M successfully running on a custom board. I'm quite confused, however, by the volume control options and registers; there seems to be a lot of missing and conflicting information.
To start with, the main…
Have you ever tried to use a linear potentiometer (pot) as a volume control? Yikes! The volume jumps up much too rapidly. It requires a safe-cracker’s touch to adjust the volume to quiet listening levels. Thus the logarithmic potentiometer.
Our…
Hi,
I´m interested in the evaluation module TAS5706EVM. I´m student of electronic engineering, I´m studying how it works because I´m making a replicate in order to interact with various electronic issues such as…