Hong,
Is it possible to boot from USB (using a USB to micro SD adapter)? The TI data sheets seem to indicate that it's an option. If so, can you verify the dip switch settings. I'm not sure it's supported on the dev board but I might have a use…
Hello Chris,
We have to use "TPS65987 Application Customization Tool" to design the USB Type-C PD controller.
Based on the method you described, We understood that if using the TPS65987 Application Customization Tool, only the third-party Aardvark…
I have replaced it with a brand new Cheetah USB to SPI adapter, but the problem remains the same as before - the computer software cannot connect to the EVM.
Hi JT,
So we don't have any specific boards for our quad RS-422 devices.
For the 7 RS-422 outputs the AM26LV31E (2x of them) would be good for the outputs - we don't have a specific board to test this. In the past when we test these or other quad…
Hi Simon,
The reason why your LMK04906EVM is not responding is because the board is a relatively old part - so old that it does not use SPI. Instead, it uses the Microwire protocol. I do not believe Texas Instruments sells the Microwire-SPI adapter board…
Hello Nick, Thank you for your response.
I’m using a general USB Bluetooth adapter, similar to the one in this link [ click here ]. It’s a generic V5.0 adapter available in the local market. Do you think this might be causing the issue, or should I…
Hey Chris,
We are looking into this. I will respond here once I find the document. In the meantime we do have alternatives with the documents available online below.
https://www.ti.com/tool/DUAL-DIYAMP-EVM
https://www.ti.com/tool/DIYAMP-EVM
https://www…
Hi Jack,
I would recommend the antenna type used by the customer has a maximum gain of what is listed in our WL18xx Module Hardware Integration Guide
The WL1835MODCOM8B EVM does come with an on board antenna (a ANT016008LCD2442MA chip antenna), you can…
Hi Aya,
the exact voltage is 14.97V, I tried to use a second board (the same circuit used to source wich work right with a commercial adapter) and a PD analyzer STM32CubeMOnitor USB Type-C PD.
When I use the same voltage on the EVM and almost the same…
Mahalakshmi C
We confirmed FUSION release 7.10.1 supports the TPSM846C23 module
Please make sure:
1) The TPSM846C23 EVM is powered with VIN at at least 4.5V. The TPSM846C23 does not derive power from the USB-TO-GPIO adapter and needs a minimum of 4…