Tool/software:
Hi Team,
Customer uses VCC=1.8V, and uses A=3.3V, B=1.8V, would like to double check with you whether there is any risk for this design? Or need A=B=1.8V or 3.3V. Thanks.
BRs,
Francis
Tool/software:
Hi Team,
Customer uses VCC=1.8V, and uses A=3.3V, B=1.8V, would like to double check with you whether there is any risk for this design? Or need A=B=1.8V or 3.3V. Thanks.
BRs,
Francis
Tool/software:
Hi TI Experts,
my question is rather simple.
The IC is supplied by 1.8V.
Input A is feed by 3.3V logic.
Input B is feed by 1.8V logic.
Is this "mixed" as well as "above supply" input voltage allowed…
Tool/software:
HI Team,
datasheet specifies the following,
Ioff Supports Live Insertion, Partial-Power-Down Mode, and Back Drive Protection
Can inputs be applied before VCC?
Regards,
Vidhya
Tool/software:
When we use the chip SN74LVC1G08DBV, its VCC=1.8V, the input of one channel is continuously low, and the input of the other channel is a high level signal…
Tool/software:
Hi team,
My customer had a question about how to tell the output logic when there is a mechanical dither. When the power is 3.3V, the high level threshold is 2V. So if the input fluctuates up and down 2V, how to…
Tool/software:
Hi,
I purchased the part of SN74LVC1G08DBVRG4, and its marking is "C08F", which is inconsistency with that showing in data sheet.
Pls check the reason for this.
Thanks,
Suri
Tool/software:
Hi Team,
In our application, we use GPIO control 1T126 enable/ disable. But this GPIO connect to many of signal.
May I know the driving current requirement of OE pin…
Tool/software:
Hello Team,
I would have a follow up question to already closed question from this thread: https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1404713/sn74lvc1g32…
Tool/software:
Hi Team,
Could you please advise do we have open drain output ANG gate supports VCC(min)<1.8V?
I just found SN74AHC1G09, but VCC min is 2V.
Thanks and best regards…
Tool/software:
Once VCC is above the 5.5V - 6.5V (out of Recommended voltage), what about the behavior of the AND gate? is behavior normally?
Customer is estimated if this logic is ok in MD with FuSa application? Very thanks…
Tool/software:
Hello guys,
One of my customers is considering using SN74AHC1G08 or SN74AHCT1G08 for their new products.
At this…
Tool/software:
Hi,
Customer would like to enquire on the stain found on the leads for part SN74LVC1G08DRLR.(see photo)
Please help to verify and advise whether this is considered reject.
Thanks
Regards
Hi TI support teams,
Please help confirm the two parameters,
1. Input transition rise or fall rate spec for min value in max temperature. spec only max value
2. Is the effect of temperature on slew rate (rise/fall time) directly…
Please tell me about the marking of SN74LVC1G08DBVRE4 as I could not find it in the data sheet. Is it consistent with "C08F"?
Hello engineers,
i can't find in SN74LVC1G08 datasheet difference between SN74LVC1G08DCKTE4 and SN74LVC1G08DCKTG4 part numbers.
footprint, surface finish, packing, all looks the same.
is silicon version different or manufacturing…
Could you please share the EMC Characterizations report for the SN74LVC1G08Q IC
Hi,
Could you please provide the max/min sink current capability of below input pins? Thanks.
Since a Schmitt trigger is now required, we are considering changing from SN74LVC1G08 to SN74LVC1G17 by replacing parts.
If you replace it as is without changing the circuit, you will…
Hi,
Could someone please help me with part number SN74LVC1G08DCKR? I don't want to discuss this in a public forum so could you please discuss over email? Thank you so much.
Hello Logic Team,
can you provide a Spice model of SN74LVC1G08? Preferred unencrypted model.
Thanks and best regards,
Michael
Dear Sir or Madam,
Could you inform me about terminal finish of the parts SN74LVC1G08DBVT & SN74LVC1G08DBVR. Could you tell me the thickness of Au in case the terminal finish is NiPdAu or NiAu or Au.
Thanks.
Best Regards…
Hi team,
My customer is using our SN74HCS08.
And they find in the datasheet the spec Δt/Δv is unlimited.
Could you please kindly help check why is it unlimited…
Hi Expert,
The customer is asking the max current (Icc) of Vcc.
They are simulating the power loss for whole system.
Thanks
Eric
Hello.
Good day.
We are contacting from HCL Technologies Ltd., We are currently serving the client of Medical Domain.
We are in need of RoHS3 Certificate of Compliance (COC) for the parts SN74AHC1G08DRLR, SN74LVC1G08DRLR and…
Hi TI Team,
Thank you for your support.
The customer purchased SN74LVC1G08DBVRE4.
But he thinks he got wrong item.
Reason is marking information on Datasheet is different.
But Label is TI manufacture label stated SN74LVC1G08DBVRE4…