Tool/software:
Dear TI experts,
General-purpose logic ICs
Specifically
SN74LVC244APWR
SN74LVT244BPW
Are there any documents on input voltage relaxation conditions?
I would like to know the input allowable voltage for overshoot/undershoot…
Tool/software:
Dear TI experts,
General-purpose logic ICs
Specifically
SN74LVC244APWR
SN74LVT244BPW
Are there any documents on input voltage relaxation conditions?
I would like to know the input allowable voltage for overshoot/undershoot…
Tool/software:
Hi TI team,
We have an application that a pull-up high 3V3 with 10k at input side of SN74LVTH244ADWR as below diagram.
But we found the voltage level of input side is…
Tool/software:
Hi Team,
There is GPIO, SPI and UART Interface between IC1 and CPU.
Following are the IC1 IO Levels (Type I and II).
VOHmin=3V, VOHmax=3.3V
VOL max=0.4V
VIHmin…
Tool/software:
Hello,
Requesting a response to my query.
Background:
I'm using a SN74LVC244A octal buffer on a daughter board connected to a unidirectional parallel data…
Tool/software:
Hello,
I am experiencing an unexpected delay variation issue with the SN74LVC244A IC and would appreciate your support in diagnosing the potential causes.
Issue Description:
I am using the SN74LVC244A in two identical…
Tool/software:
Hello team,
Does this device require pull up/down resistor for each in/out?
If so, what is the recommended value?
Best Regards,
Kei Kuwahara
Tool/software:
Hi Sirs
When OE pull high, the impedance of output (Y side) is high, how about the input side?
We want to know in this condition, impedance of A side is high impedance or low impedance, or floating?
Thank you
Tool/software:
Hi,
I'm using the buffer SN74ALVC244 to drive some other IC input pins on an existing PCB.
The IC is already active before the…
Tool/software:
Hello,
Should I connect GND to the Thermal Pad of SN74LVC244ARGY?
This is not mentioned in the datasheet, so please let me know.
Hi,
I need to use SPI master/slave configuration, have one STM32 as master uC as SPI master & 6 STM32 are slaves, i was trying on one prototype which involved external wiring…
Hi TI Team.
Is there any problem if voltage is applied to Vin (A side) before voltage is applied to VCC in this IC?
Best regards.
Hello expert,
Are we able to enhance output driving capability in SN74LVC244APWR IBIS model? Based on datasheet, output driving capability is related to VCC. Could we adjust VCC in IBIS model? If no, do we have other method to…
Hi,
Please see below queries and request you to suggest
Query1: Regarding 8 Bit Buffer IC SN74LVC244ARGYR…
Hi,
RnD currently used SN74LVC244A for the signal 50MHz. The output signal is distortion.
Is there solution for high speed (tpd < 5.9ns)?
Thanks and Best regards,
Hello,
I didn't find information about the connection of thermal pad (21).
Is the pad isolated from GND ?
Package X1QFN (RWP)
Thanks.
Hello E2ETeams
Ask a question.
Do you use barrier metal for your SN74LVC244APWR?
Hi team,
I would like to use SN74LVC244A to divide the output of one oscillator into four outputs as shown below.
In this condition, do you have any information about the output jitter characteristics of SN74LVC244A?
If there…
Hi Team,
Do we have recommendations for a Buffer IC that is shorter in height than the SN74LVC541's VQFN (H=1.0mm) package?
Best regards,
Scott
Hi,
Will this dip/step at the edge be concern? I think the time is short and should not cause an additional pulse and influence the following device.
Could you help confirm?
I got the Ibis model for SN74LVC244A, but in that package I couldn't see SN74LVC244ARWPR (Which is having X1QFN Package)
Hello,
What is the difference between SN74LVCH244APWR and SN74LVC244APWR? I only see an additional package of the SN74LVC244APWR, but don't see differences otherwise. Could you please share any other differences?
Thank you,
…Hello team,
(I see tw on datasheet, but doesn't specify any numbers.)
Best Regards,
Kei Kuwahara
Hello TI Experts,
We have a faulty design (which have already been mass shipped out in field ….), we want to evaluate the risk of the design and consider next step
Conditions:
1. SN74LVC244APWR
I want to generate a pulse that always falls between 20ns and 50ns over the entire temperature range of an industrial device. Is 20ns a feasible lower bound for this device? I have…
Hi Team,
When I look the Vo spec in the datasheet of SN74AHCT244 & SN74LVC244A, I found something different. In the DS of SN74LVC244A, the Vo max has different description in power…