• TXB0102: Pspice model requirement

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXB-EVM

    Tool/software:

    I would like to simulate the TXB0102DCUR  which is bidirectional voltage level shifter it is not available in Pspice for simulation. It only has IBIS model can you able to provide…

  • TXB0102: Output Voltage Not driven to complete 0V

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXS0102, TXU0102,

    Tool/software:

    Hi Team,

    I am using the TXB010 in my design for reset signal level conversion between 1.5V and 3.3V. I have placed a 10kΩ pull-up resistor on both the input and output…

  • TXB0102: Level shifter issue

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXU0202

    Tool/software:

    Dear [Recipient],

    We are working on a project where we need to convert a 3.3V signal to 5V using your IC, part number TXB0102DCUR. This is being used for UART communication

  • TXB0102: Level shifter issue

    Part Number: TXB0102

    Tool/software:

    Dear Texas,

    We are working on a project where we need to convert a 3.3V signal to 5V using your IC, part number TXB0102DCUR. This is being used for UART communication at a baud rate of 9600.

    We are facing issues with…

  • TXB0104: Seeing unusual behavior

    Part Number: TXB0104
    Other Parts Discussed in Thread: TS3DDR3812, TXS0104E

    Tool/software:

    Hey Team,

    In the circuit we utilized for one of our industrial sensor read kits, we incorporated a TXB device as a bidirectional buffer. According to the datasheet…

  • [FAQ] Which IBIS model should I choose for simulating Auto-Bidirectional Translators (LSF,TXB,TXS) ?

    Other Parts Discussed in Thread: LSF0101

    FAQ: Logic and Voltage Translation >  Auto-Bidirectional Level-Shifters > Current FAQ

    In most cases, it is recommended to test with the device EVM instead as it yields much more accurate results under specific…

  • LSF0102-Q1: Looking for the voltage level shifter for MIPI3.0 RFFE application

    Part Number: LSF0102-Q1
    Other Parts Discussed in Thread: TXS0102, TXS02326A, TXS02612, TXB0102, TXB0302

    Tool/software:

    Hi. I am looking for voltage level shifter for MIPI RFFE application.

    The product should operate up to 52MHz. (MIPI3.0 standard requires…

  • TXB0102: Controller in B and system in A

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXU0202

    Tool/software:

    I recently added  TXB0102 to make the UART level translation from an MCU at +3.3 V (PIC18F47J13) to send AT Commands to a Modem at +1.8 V (Quectel BG600L-M3), however, in my design…

  • TXB0102: TXB

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXU0102

    Tool/software:

    In the datasheet of TXB0102, why should the VCCA<=VCCB? The architecture of TXB is symmetrical.

  • TXB0102: TXS0104E for sim card

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXB0104, TXS0104E

    Hi team,

    would you help check if TXB0104 or TXS0104E are more suitable can support below CLK and DATA from SIM card?

  • TXB0102: SIM card buffer

    Part Number: TXB0102
    Other Parts Discussed in Thread: SN74AVC2T245, TXS4555, TCA9617B

    Hi team,

    would you help check if TXB0102 can support below CLK and DATA from SIM card?

    I also see someone mentioned SN74AVC2T245 in the forum, which one is more suitable…

  • TXB0102: TXB0102DCUR

    Part Number: TXB0102

    Hi Team, I am using TXB0102DCUR level shifter in our project but it is not working beyond 100Kbps, beyond 100kbps its rise and fall time increase and at 2.5Mbps we get Vcc voltage level output side, not a pulses. our direction is 5VccB…

  • TXB0102: Looking for suggestions and guidance of serial ring and level shifting design?

    Part Number: TXB0102
    Other Parts Discussed in Thread: SN74AHCT1G14, TCAN330, SN74LVC1G07, SN74LVC1G17

    Hello, 

    An actuator vendor provided schematics to interface circuitry between an MCU (on our end) and the actuator serial interface on (their end). The…

  • LSF0102: MDC MDIO Level Translator

    Part Number: LSF0102
    Other Parts Discussed in Thread: TXB0102, , TXS0102

    Dear Team,

    which device is recommended for MDC and MDIO level translation?

    MAC side is 3.3V , PHY side is 1.8V

    LSF0102, TXS0102 or TXB0102 

    Best Regards,

    d.

  • TXB0102: Level Translation for MDC,MDIO, Ethernet MDC,MDIO

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXS0102

    Hi,

    We Have used TXB0102DCUR for Level Translation for MDC/MDIO for Ethernet Interface, from 1.8V (VCCA) to 3.3V (VCCB).

    attaching schematic for reference. We have tried adding 100k Pull-up on…

  • TXB0102: Abnormal low voltage

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXU0202

    Hi team,

    my customer is using TXB0102 and they found that the low voltage can't be pulled down to 0V and stays at 1.5V .

    Could u kindly help to analyze the problem? thanks~

    blue---A2 input…

  • TXB0102: Problem with level translation using TXB0102DCUR

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXU0102, , SN74LVC2G126

    In the attached schematic, I am sending in a 42MHz clock signal. 

    At TP6 and TP7, the clock signal looks very good. (A nice square wave 0 to 3.3V at 42MHz)
    After the TXB0102DCUR…

  • TXB0102: Iq Supply Verification

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXB0108

    Hey team,

    I have a customer trying to verify quiescent supply currents against the datasheet and confused on observed high current. Full question below

    "We are trying to verify the quiescent…

  • TXB0102: Is there any level shift with shift register function?

    Part Number: TXB0102
    Other Parts Discussed in Thread: TPIC6C595, TXU0104

    Hi Team, 

    May I ask if you have a shift register with level shifting. My customer SOC GPIO outputs is 1.8V. Is there a shift register that supports input 1.8V to 3.3V output or a shift…

  • TXB0102: TXB0102DCUR

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXU0102, TXU0202

    为什么TXB0102DCUR这个料,3.3V这边的波形正常,5V这边的波形波异常,低电平不会到0V,这是什么情况,麻烦帮忙解答一下,谢谢。

  • TXB0102: OUTPUT Buffer

    Part Number: TXB0102

    Hi

    I received a question from a customer following this thread.

    https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1207722/txb0102-open-output/4555295#4555295

    Customer Question
    =============================================…

  • TXB0102: voltage level converter for UART data lines

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXU0202

    Hello,

    My name is Amith. I am using your component TXB0102 in my circuit as a voltage level converter for UART data lines from 3.3V to 1.8V and opposite directions.

    My connection configuration…

  • TXB0102: Open Output

    Part Number: TXB0102
    Other Parts Discussed in Thread: TXU0102, TXU0202

    Hi,

    Please confirm the inquiry from the customer.

    Q1 If the B port is open while a signal is being input to the A port, will there be any effect on the A port?
          Also, could the device…

  • SN74LXC2T45-Q1: Output rise and fall times

    Part Number: SN74LXC2T45-Q1
    Other Parts Discussed in Thread: SN74AXC2T45, TXB0102, TXB0304

    Can I know what is the output rise and fall time or slew rate of the device at 1.8V supplies and 50pF cap load.

    I am also looking for a buffer/ level shifter with…

  • TXB0102: Output noise prevents high-speed translation

    Part Number: TXB0102
    Other Parts Discussed in Thread: MSP430FR2433

    I'm using the TXB0102 and seeing noise that prevents using it above ~1MHz, but the datasheet claims 60 MHz (60 Mbps) for my VDD setup.

    In the attached scopeshots, a 2MHz square wave…

1 2 3 4 5 »