Other Parts Discussed in Thread: INA253-Q1, , INA745B, TPS7A47, TPS7A85A, TPS7A84A, TPS7A57, TPS7A54, TPS7A52, TPS7A53
Tool/software:
I am reaching out regarding a design challenge in my application and would appreciate your assistance…
Tool/software:
We use TPS7A5401QRGRRQ in our current design.
Could we use TPS7A8500ARGRR instead of TPS7A5401QRGRRQ1 without any change schematic/layout?
Thanks,
Jimmy Huang
Hi Team,
Customer report the vout waveform is abnormal when pull the enable low. Pls check the waveform and schematic below. As double check with customer the test method is good. Do you have any comments for this case?
Regards…
I am testing the achievable accuracy of this regulator for powering sensitive parallel optical transceivers. The regulator datasheet states multiple accuracies
Hi Experts
datasheet tell us. bias can improve dc and ac performance
I wonder how does bias work to improve it.
Best
Regards
Brian
Hi team
this is my customer SCH could you help me to review it ?
because I will LOA next week
can you reply this week?
there are
TPS7A5401 in page2
TPS7A5401 *3 in page3
TPS7A5401 *2 in page5
total 6
in attached files
BRs
b…
Hi team,
I am using the TPS7A54 and with the 5V power supply on the bias pins. I find in data sheet section 7.3.2.2. There is a description that bias is better not change when VIN>1.4V. Does that means the bias voltage should be ready…
Hi,
I noticed that the TPS7A5401RPST is a VQFN package. But what is the material of the Bond Wire of TPS7A5401RPST? Thanks.
Regards,
Charlie
Hi team!
I see TPS7A54 parallel method on the link( https://e2e.ti.com/support/power-management-group/power-management---internal/f/power-management---internal-forum/1052479/tps7a54…
Dear team,
We would like to calculate device output accuracy for system design. But cannot find min/max value of VFB.
Does Vout accuracy in datasheet exclude feedback…
Hi team,
My customer is considering TPS7A54 to generate 2.3V/15A from 2.5V rail by current sharing configuration.
The available rail is limited, so I think they will go without BIAS.
Just for reference, if BIAS is used, is clean power…
Hi all,
Customer was wondering how ferrite beads on the bias input affect Vout noise and PSRR? Does it impact it at all?
Thanks,
Lauren