Part Number: OPA818
Other Parts Discussed in Thread: OPA858, OPA857
I am currently working on designing a TIA module for an APD using the OPA818, based on the design steps provided in the datasheet:

I want to design a 40MHz, 22k gain TIA, and have used to TIA calculator and Capacitor T-network to realise the small feedback capacitance required. I have followed the layout guidelines provided along with an isolation resistor of 10R at the inverting input with (+5/-5V) supply.
The output waveform looks like this, giving a very low bandwidth of 18MHz instead of 40MHz and if zoomed, some ripples can be seen:

Instead of grounding the In+ node of the OPA818, if I connect it to a potential divider between the positive and negative supplies (+5V/-5V) with the potential divider providing 0V, I see this waveform (offset is 0.14V instead of 0), and a slightly improved bandwidth:

I tried to vary the supply to the TIA to note its effect and I saw that when I supplied (+3/-3V) I am very close to the required bandwidth and the offset is 0V, with much lower overshoot and undershoot:

My questions are:
1) Why do I get a much lower bandwidth and ripple output when the input+ node is grounded?
2) Why does the offset and overshoot/undershoot vary with change in supply voltage which is supplying the potential divider providing 0V to the input+ node?
Any advice/input would be highly appreciated!